Transport Layer Control
The Transport Layer control provides the following information:
Gev IEEE 1588 - Enables IEEE 1588 Precision Time Protocol (PTP) to control the timestamp register.
Gev IEEE 1588 Clock Accuracy - The expected accuracy of the device clock when it is the grandmaster or when it becomes the grandmaster.
Gev IEEE 1588 Status - The status of the IEEE 1588 clock.
Gev IEEE 1588 Mode - The mode of the IEEE 1588 clock.
Summary Table
| Name | Interface | Access | Visibility | Description |
|---|---|---|---|---|
| Payload Size | IInteger | Expert | Provides the number of bytes transferred for each image or chunk on the stream channel. | |
| GigE Vision | ICategory | RO | Beginner | Category that contains the features pertaining to the GigE Vision transport layer of the device. |
| Link Error Count | IInteger | RO | Expert | Counts the number of error on the link. |
| Packet Resend Request Count | IInteger | RO | Expert | Counts the number of resend requests received from the host. |
Transport Layer Control Features
Payload Size
Provides the number of bytes transferred for each image or chunk on the stream channel.
| Property | Value |
|---|---|
| Name | PayloadSize |
| Interface | IInteger |
| Access | |
| Unit | |
| Visibility | Expert |
GigE Vision
Category that contains the features pertaining to the GigE Vision transport layer of device, including IEEE 1588.
| Property | Value |
|---|---|
| Name | GigEVision |
| Interface | ICategory |
| Access | RO |
| Visibility | Beginner |
Link Error Count
Counts the number of error on the link.
| Property | Value |
|---|---|
| Name | LinkErrorCount |
| Interface | IInteger |
| Access | RO |
| Unit | |
| Visibility | Expert |
Packet Resend Request Count
Counts the number of resend requests received from the host.
| Property | Value |
|---|---|
| Name | PacketResendRequestCount |
| Interface | IInteger |
| Access | RO |
| Unit | |
| Visibility | Expert |