Chunk Data Control

Chunk Data allows you the ability to send additional information with the image data. This can be helpful when debugging issues or looking at what settings have been applied to the acquired image.

Use ChunkModeActive to enable chunk data for images.

The following information is enabled by default as chunk data:

Image - enabled by default and cannot be disabled.

Image CRC - enabled by default and cannot be disabled.

Image properties available for chunk data depend on the camera's sensor, but could include image size, image format settings (gain, exposure, pixel format), timestamp, and others.

Use ChunkSelector to select a chunk then use ChunkEnable to enable or disable it. Image and ImageCRC cannot be disabled.

Once acquisition has started Chunk data can not be altered. To enable or disable chunks acquisition must be stopped.

Lossless Compression

Lossless compression is a feature that uses a lossless compression algorithm to reduce the amount of data transmitted from the camera. This can be used to either lower bandwidth or increase frame rate.

Lossless compression adds the following information in Chunk Data:

Summary Table

Name Interface Access Visibility Description
Chunk Mode Active IBoolean RW Expert Activates the inclusion of Chunk data in the payload of the image.
Chunk Selector IEnumeration RW Expert Selects which chunk data to enable or disable.
Chunk Enable [Chunk Selector] IBoolean RW Expert Enables the inclusion of the selected Chunk data in the payload of the image.
Chunk Image IInteger RO Expert Returns the image payload.
Image CRC IInteger RO Expert Returns the CRC of the image payload.
Chunk Frame ID IInteger RO Expert Returns the image frame ID.
Chunk Offset X IInteger RO Expert Returns the Offset X of the image included in the payload.
Chunk Offset Y IInteger RO Expert Returns the Offset Y of the image included in the payload.
Chunk Width IInteger RO Expert Returns the width of the image included in the payload.
Chunk Height IInteger RO Expert Returns the height of the image included in the payload.
Chunk Pixel Format IEnumeration Expert Format of the pixel provided by the camera
Chunk Exposure Time IFloat RO Expert Returns the exposure time used to capture the image.
Chunk Gain IFloat RO Expert Returns the gain used to capture the image.
Chunk Black Level IFloat RO Expert Returns the black level used to capture the image.
Chunk Timestamp IInteger RO Expert Returns the Timestamp of the image.
Chunk Sequencer Set Active IInteger RO Expert Returns the index of the active set of the running sequencer included in the payload.
Chunk Exposure End Line Status All IInteger RO Expert Returns the status of all the I/O lines at the end of exposure event.
Chunk Compression Mode IInteger RO Expert Returns the compression mode of the last image payload.
Chunk Current Datarate IInteger RO Expert Returns the current datarate of the last image payload.
Chunk Compression Ratio IFloat RO Expert Returns the compression ratio of the last image payload.
Chunk Serial Data Length IInteger RO Expert Returns the length of the received serial data that was included in the payload.
Chunk Serial Data IStringReg Expert Returns the serial data that was received.
Chunk Serial Receive Overflow IBoolean RO Expert Returns the status of the chunk serial receive overflow.

Chunk Data Control Features


Chunk Mode Active

Activates the inclusion of Chunk data in the payload of the image.

Property Value
Name ChunkModeActive
Interface IBoolean
Access RW
Visibility Expert

Chunk Selector

Selects which chunk data to enable or disable.

Property Value
Name ChunkSelector
Interface IEnumeration
Access RW
Visibility Expert

Enumeration Values
Image
CRC
FrameID
OffsetX
OffsetY
Width
Height
ExposureTime
Gain
BlackLevel
PixelFormat
Timestamp
SequencerSetActive
SerialData
ExposureEndLineStatusAll
CompressionMode
CompressionRatio
CurrentDatarate

Chunk Enable

Enables the inclusion of the selected Chunk data in the payload of the image.

Property Value
Name ChunkEnable [Chunk Selector]
Interface IBoolean
Access RW
Visibility Expert

Chunk Image

Returns the image payload.

Property Value
Name ChunkImage
Interface IInteger
Access RO
Unit
Visibility Expert

Image CRC

Returns the CRC of the image payload.

Property Value
Name ChunkCRC
Interface IInteger
Access RO
Unit
Visibility Expert

Chunk Frame ID

Returns the image frame ID.

Property Value
Name ChunkFrameID
Interface IInteger
Access RO
Unit
Visibility Expert

Chunk Offset X

Returns the Offset X of the image included in the payload.

Property Value
Name ChunkOffsetX
Interface IInteger
Access RO
Unit
Visibility Expert

Chunk Offset Y

Returns the Offset Y of the image included in the payload.

Property Value
Name ChunkOffsetY
Interface IInteger
Access RO
Unit
Visibility Expert

Chunk Width

Returns the width of the image included in the payload.

Property Value
Name ChunkWidth
Interface IInteger
Access RO
Unit
Visibility Expert

Chunk Height

Returns the height of the image included in the payload.

Property Value
Name ChunkHeight
Interface IInteger
Access RO
Unit
Visibility Expert

Chunk Pixel Format

Format of the pixel provided by the camera

Property Value
Name ChunkPixelFormat
Interface IEnumeration
Access
Visibility Expert

Enumeration Values
Mono8
Mono12Packed
Mono16
RGB8Packed
YUV422Packed
BayerGR8
BayerRG8
BayerGB8
BayerBG8
YCbCr601_422_8_CbYCrY

Chunk Exposure Time

Returns the exposure time used to capture the image.

Property Value
Name ChunkExposureTime
Interface IFloat
Access RO
Unit us
Visibility Expert

Chunk Gain

Returns the gain used to capture the image.

Property Value
Name ChunkGain
Interface IFloat
Access RO
Unit
Visibility Expert

Chunk Black Level

Returns the black level used to capture the image.

Property Value
Name ChunkBlackLevel
Interface IFloat
Access RO
Unit
Visibility Expert

Chunk Timestamp

Returns the Timestamp of the image.

Property Value
Name ChunkTimestamp
Interface IInteger
Access RO
Unit
Visibility Expert

Chunk Sequencer Set Active

Returns the index of the active set of the running sequencer included in the payload.

Property Value
Name ChunkSequencerSetActive
Interface IInteger
Access RO
Unit
Visibility Expert

Chunk Exposure End Line Status All

Returns the status of all the I/O lines at the end of exposure event.

Property Value
Name ChunkExposureEndLineStatusAll
Interface IInteger
Access RO
Unit
Visibility Expert

Chunk Compression Mode

Returns the compression mode of the last image payload.

Property Value
Name ChunkCompressionMode
Interface IInteger
Access RO
Unit
Visibility Expert

Chunk Current Datarate

Returns the current datarate of the last image payload.

Property Value
Name ChunkCurrentDatarate
Interface IInteger
Access RO
Unit
Visibility Expert

Chunk Compression Ratio

Returns the compression ratio of the last image payload.

Property Value
Name ChunkCompressionRatio
Interface IFloat
Access RO
Unit
Visibility Expert

Chunk Serial Data Length

Returns the length of the received serial data that was included in the payload.

Property Value
Name ChunkSerialDataLength
Interface IInteger
Access RO
Unit
Visibility Expert

Chunk Serial Data

Returns the serial data that was received.

Property Value
Name ChunkSerialData
Interface IStringReg
Access
Visibility Expert

Chunk Serial Receive Overflow

Returns the status of the chunk serial receive overflow.

Property Value
Name ChunkSerialReceiveOverflow
Interface IBoolean
Access RO
Visibility Expert