Configuring the Camera Driver
The driver is installed automatically by the Spinnaker SDK installer for Camera Evaluation or for Application Development if the Drivers checkbox is selected (default). A restart is required.
Note: For optimal driver performance, install Spinnaker version 4.0 or later.
Alternatively, you can manually install the driver. The driver files are located in:
To manage and update drivers use the SpinView application:
- Start SpinView:
- From the Devices list, select the camera and click the Switch Driver button.
- Select the driver from the drop-down list.
- Click Install Driver.