Spinnaker SDK C++
4.2.0.83
 
 

 
Loading...
Searching...
No Matches
CMainFrame Class Reference

#include <MainFrm.h>

Inheritance diagram for CMainFrame:

Public Member Functions

void ResizeToFit ()
 
void UpdateStatusBar ()
 
virtual BOOL PreCreateWindow (CREATESTRUCT &cs)
 
virtual ~CMainFrame ()
 
afx_msg void OnTimer (UINT_PTR idEvent)
 
afx_msg void OnDestroy ()
 

Protected Member Functions

 CMainFrame ()
 
afx_msg int OnCreate (LPCREATESTRUCT lpCreateStruct)
 

Protected Attributes

CStatusBar m_wndStatusBar
 
CToolBar m_wndToolBar
 
UINT_PTR m_timer
 
RECT m_rectStatus
 

Constructor & Destructor Documentation

◆ CMainFrame()

CMainFrame ( )
protected

◆ ~CMainFrame()

~CMainFrame ( )
virtual

Member Function Documentation

◆ OnCreate()

int OnCreate ( LPCREATESTRUCT  lpCreateStruct)
protected

◆ OnDestroy()

void OnDestroy ( )

◆ OnTimer()

void OnTimer ( UINT_PTR  idEvent)

◆ PreCreateWindow()

BOOL PreCreateWindow ( CREATESTRUCT &  cs)
virtual

◆ ResizeToFit()

void ResizeToFit ( )

◆ UpdateStatusBar()

void UpdateStatusBar ( )

Member Data Documentation

◆ m_rectStatus

RECT m_rectStatus
protected

◆ m_timer

UINT_PTR m_timer
protected

◆ m_wndStatusBar

CStatusBar m_wndStatusBar
protected

◆ m_wndToolBar

CToolBar m_wndToolBar
protected

The documentation for this class was generated from the following files: