Spinnaker SDK C++
4.2.0.83
 
 

 
Loading...
Searching...
No Matches
CSpinnakerMFCView Class Reference

#include <SpinnakerMFCView.h>

Inheritance diagram for CSpinnakerMFCView:

Public Member Functions

CSpinnakerMFCDocGetDocument () const
 
double GetDisplayedFrameRate ()
 
virtual void OnDraw (CDC *pDC)
 
virtual BOOL PreCreateWindow (CREATESTRUCT &cs)
 
virtual ~CSpinnakerMFCView ()
 
virtual void OnInitialUpdate ()
 
afx_msg int OnCreate (LPCREATESTRUCT lpCreateStruct)
 
afx_msg void OnDestroy ()
 
afx_msg void OnSize (UINT nType, int cx, int cy)
 
afx_msg BOOL OnEraseBkgnd (CDC *pDC)
 

Static Public Member Functions

static CSpinnakerMFCViewGetView ()
 

Protected Member Functions

 CSpinnakerMFCView ()
 

Protected Attributes

FrameRateCounter m_displayedFrameRate
 
CDC * m_pDC
 Device context for drawing.
 

Constructor & Destructor Documentation

◆ ~CSpinnakerMFCView()

~CSpinnakerMFCView ( )
virtual

◆ CSpinnakerMFCView()

CSpinnakerMFCView ( )
protected

Member Function Documentation

◆ GetDisplayedFrameRate()

double GetDisplayedFrameRate ( )

◆ GetDocument()

CSpinnakerMFCDoc * GetDocument ( ) const
inline

◆ GetView()

CSpinnakerMFCView * GetView ( )
static

◆ OnCreate()

int OnCreate ( LPCREATESTRUCT  lpCreateStruct)

◆ OnDestroy()

void OnDestroy ( )

◆ OnDraw()

void OnDraw ( CDC *  pDC)
virtual

◆ OnEraseBkgnd()

BOOL OnEraseBkgnd ( CDC *  pDC)

◆ OnInitialUpdate()

void OnInitialUpdate ( )
virtual

◆ OnSize()

void OnSize ( UINT  nType,
int  cx,
int  cy 
)

◆ PreCreateWindow()

BOOL PreCreateWindow ( CREATESTRUCT &  cs)
virtual

Member Data Documentation

◆ m_displayedFrameRate

FrameRateCounter m_displayedFrameRate
protected

◆ m_pDC

CDC* m_pDC
protected

Device context for drawing.


The documentation for this class was generated from the following files: