Spinnaker SDK C++
4.2.0.83
 
 

 
Loading...
Searching...
No Matches
ISpinDevice Interface Referenceabstract

#include <SpinnakerDirectShow.h>

Public Member Functions

Spinnaker Interface and Camera Functions

These functions deal with querying/setting generic interface and camera info.

virtual HRESULT GetNumCameras (unsigned int *numCameras)=0
 Retrieves the number of cameras available for this Spinnaker DirectShow interface.
 
virtual HRESULT GetSelectedCameraIndex (unsigned int *selectedIndex)=0
 Retrieves an integer index to the currently selected camera.
 
virtual HRESULT SetSelectedCameraIndex (unsigned int index, bool needsRelease=true)=0
 Sets the currently selected camera to the index specified.
 
virtual HRESULT GetCameraInfo (unsigned int index, char *model, char *type, char *serial, size_t bufferSize)=0
 Retrieves general information about the camera at the specified index.
 
virtual HRESULT IsStreaming (bool *isStreaming)=0
 Checks if the selected camera is currently streaming.
 
virtual HRESULT BeginAcquisition ()=0
 Starts the image acquisition engine for the currently selected camera.
 
virtual HRESULT EndAcquisition ()=0
 Stops the image acquisition engine for the currently selected camera.
 
Spinnaker GenAPI Generic Functions

These functions deal with Spinnaker GenAPI NodeMap and Node Accesses for setting camera properties.

virtual HRESULT NodeMapGetNumNodes (size_t *numNodes)=0
 Retrieves the number of nodes available in the node map for the currently selected camera.
 
virtual HRESULT NodeMapGetNodeAtIndex (size_t index, char *nodeName, size_t bufferSize)=0
 Retrieves the string representation of the node at the specified index.
 
virtual HRESULT NodeIsImplemented (const char *nodeName, bool *isImplemented)=0
 Checks if a node is implemented.
 
virtual HRESULT NodeIsAvailable (const char *nodeName, bool *isAvailable)=0
 Checks if a node is available.
 
virtual HRESULT NodeIsReadable (const char *nodeName, bool *isReadable)=0
 Checks if a node is readable.
 
virtual HRESULT NodeIsWritable (const char *nodeName, bool *isWritable)=0
 Checks if a node is writable.
 
virtual HRESULT NodeGetType (const char *nodeName, char *typeName, size_t bufferSize)=0
 Gets the type of the node.
 
virtual HRESULT NodeToString (const char *nodeName, char *valueAsString, size_t bufferSize)=0
 Gets content of the node as string.
 
virtual HRESULT NodeGetDisplayName (const char *nodeName, char *displayName, size_t bufferSize)=0
 Gets a name string for display.
 
Spinnaker GenAPI Integer Node Functions

These functions deal with Spinnaker GenAPI Integer Node Accesses

virtual HRESULT IntegerGetValue (const char *nodeName, int64_t *value)=0
 Gets integer node value for the specified feature.
 
virtual HRESULT IntegerSetValue (const char *nodeName, int64_t value)=0
 Sets integer node value for the specified feature.
 
virtual HRESULT IntegerGetMax (const char *nodeName, int64_t *maxValue)=0
 Gets maximum integer value allowed for the specified feature.
 
virtual HRESULT IntegerGetMin (const char *nodeName, int64_t *minValue)=0
 Gets minimum integer value allowed for the specified feature.
 
virtual HRESULT IntegerGetIncMode (const char *nodeName, Spinnaker::GenApi::EIncMode *incMode)=0
 Gets integer increment mode for the specified feature.
 
virtual HRESULT IntegerGetInc (const char *nodeName, int64_t *increment)=0
 Gets integer step increment for the specified feature.
 
Spinnaker GenAPI Float Node Functions

These functions deal with Spinnaker GenAPI Float Node Accesses

virtual HRESULT FloatGetValue (const char *nodeName, double *value)=0
 Gets float node value for the specified feature.
 
virtual HRESULT FloatSetValue (const char *nodeName, double value)=0
 Sets float node value for the specified feature.
 
virtual HRESULT FloatGetMax (const char *nodeName, double *floatMax)=0
 Gets maximum float value allowed for the specified feature.
 
virtual HRESULT FloatGetMin (const char *nodeName, double *floatMin)=0
 Gets minimum float value allowed for the specified feature.
 
virtual HRESULT FloatGetIncMode (const char *nodeName, Spinnaker::GenApi::EIncMode *incMode)=0
 Gets float increment mode for the specified feature.
 
virtual HRESULT FloatGetInc (const char *nodeName, double *increment)=0
 Gets float step increment for the specified feature.
 
Spinnaker GenAPI Boolean Node Functions

These functions deal with Spinnaker GenAPI Boolean Node Accesses

virtual HRESULT BooleanGetValue (const char *nodeName, bool *value)=0
 Gets boolean node value for the specified feature.
 
virtual HRESULT BooleanSetValue (const char *nodeName, bool value)=0
 Sets boolean node value for the specified feature.
 
Spinnaker GenAPI String Node Functions

These functions deal with Spinnaker GenAPI String Node Accesses

virtual HRESULT StringGetValue (const char *nodeName, char *value, size_t bufferSize)=0
 Gets string node value for the specified feature.
 
virtual HRESULT StringSetValue (const char *nodeName, const char *value)=0
 Sets string node value for the specified feature.
 
Spinnaker GenAPI Enumeration Node Functions

These functions deal with Spinnaker GenAPI Enumeration and EnumeratEntry Node Accesses

virtual HRESULT EnumerationGetEntry (const char *nodeName, char *value, size_t bufferSize)=0
 Gets enumeration entry string for the specified enumeration feature.
 
virtual HRESULT EnumerationSetEntry (const char *nodeName, const char *value)=0
 Sets enumeration entry for the specified enumeration feature.
 
virtual HRESULT EnumerationEntryExists (const char *enumerationName, const char *enumerationEntryName, bool *entryExist)=0
 Checks if an enumeration entry exists for the specified enumeration feature.
 
virtual HRESULT EnumerationGetNumEntries (const char *enumerationName, size_t *numEntries)=0
 Retrieves the number of enumeration entry nodes available for the specified enumeration feature.
 
virtual HRESULT EnumerationGetEntryAtIndex (const char *enumerationName, unsigned int entryIndex, char *enumerationEntryName, size_t bufferSize)=0
 Gets enumeration entry string for the specified enumeration feature at the specified index.
 
Spinnaker GenAPI Command Node Functions

These functions deal with Spinnaker GenAPI Command Node Accesses

virtual HRESULT CommandExecute (const char *nodeName)=0
 Executes the command for the specified feature.
 

Detailed Description

Member Function Documentation

◆ BeginAcquisition()

virtual HRESULT BeginAcquisition ( )
pure virtual

Starts the image acquisition engine for the currently selected camera.

Nothing occurs if the camera is already streaming.

Returns
An HRESULT indicating the success or failure of the function.

◆ BooleanGetValue()

virtual HRESULT BooleanGetValue ( const char *  nodeName,
bool *  value 
)
pure virtual

Gets boolean node value for the specified feature.

Parameters
nodeNameGenICam device feature name
valueThe value read from the device
Returns
An HRESULT indicating the success or failure of the function.

◆ BooleanSetValue()

virtual HRESULT BooleanSetValue ( const char *  nodeName,
bool  value 
)
pure virtual

Sets boolean node value for the specified feature.

Parameters
nodeNameGenICam device feature name
valueThe value to set to device
Returns
An HRESULT indicating the success or failure of the function.

◆ CommandExecute()

virtual HRESULT CommandExecute ( const char *  nodeName)
pure virtual

Executes the command for the specified feature.

Parameters
nodeNameGenICam device feature name
Returns
An HRESULT error code indicating the success or failure of the function.

◆ EndAcquisition()

virtual HRESULT EndAcquisition ( )
pure virtual

Stops the image acquisition engine for the currently selected camera.

Nothing occurs if there were no prior call to BeginAcquisition(). Note that EndAcquisition() needs to be called before selecting a new camera.

Returns
An HRESULT indicating the success or failure of the function.

◆ EnumerationEntryExists()

virtual HRESULT EnumerationEntryExists ( const char *  enumerationName,
const char *  enumerationEntryName,
bool *  entryExist 
)
pure virtual

Checks if an enumeration entry exists for the specified enumeration feature.

Parameters
enumerationNameGenICam device enumeration feature name
enumerationEntryNameGenICam device enumeration entry name to check
entryExistFlag indicating whether the specified entry node exists for the enumeration node
Returns
An HRESULT indicating the success or failure of the function.
Examples
SpinSimpleGUI_DirectShow.cpp.

◆ EnumerationGetEntry()

virtual HRESULT EnumerationGetEntry ( const char *  nodeName,
char *  value,
size_t  bufferSize 
)
pure virtual

Gets enumeration entry string for the specified enumeration feature.

Parameters
nodeNameGenICam device feature name
valueThe enumeration entry string read from the device
bufferSizeSize of the provided value buffer in bytes
Returns
An HRESULT indicating the success or failure of the function.
Examples
SpinSimpleGUI_DirectShow.cpp.

◆ EnumerationGetEntryAtIndex()

virtual HRESULT EnumerationGetEntryAtIndex ( const char *  enumerationName,
unsigned int  entryIndex,
char *  enumerationEntryName,
size_t  bufferSize 
)
pure virtual

Gets enumeration entry string for the specified enumeration feature at the specified index.

Parameters
enumerationNameGenICam device enumeration feature name
entryIndexEnumeration entry index
enumerationEntryNameGenICam device enumeration entry name at specified entryIndex to be populated
bufferSizeSize of the provided enumerationEntryName buffer in bytes
Returns
An HRESULT indicating the success or failure of the function.
Examples
SpinSimpleGUI_DirectShow.cpp.

◆ EnumerationGetNumEntries()

virtual HRESULT EnumerationGetNumEntries ( const char *  enumerationName,
size_t *  numEntries 
)
pure virtual

Retrieves the number of enumeration entry nodes available for the specified enumeration feature.

Parameters
enumerationNameGenICam device enumeration feature name
numEntriesNumber of nodes available for the specified enumeration feature
Returns
An HRESULT indicating the success or failure of the function.
Examples
SpinSimpleGUI_DirectShow.cpp.

◆ EnumerationSetEntry()

virtual HRESULT EnumerationSetEntry ( const char *  nodeName,
const char *  value 
)
pure virtual

Sets enumeration entry for the specified enumeration feature.

Parameters
nodeNameGenICam device feature name
valueThe enumeration entry string to set to device
Returns
An HRESULT indicating the success or failure of the function.
Examples
SpinSimpleGUI_DirectShow.cpp.

◆ FloatGetInc()

virtual HRESULT FloatGetInc ( const char *  nodeName,
double *  increment 
)
pure virtual

Gets float step increment for the specified feature.

Parameters
nodeNameGenICam device feature name
incrementThe step increment value read from the device
Returns
An HRESULT indicating the success or failure of the function.

◆ FloatGetIncMode()

virtual HRESULT FloatGetIncMode ( const char *  nodeName,
Spinnaker::GenApi::EIncMode incMode 
)
pure virtual

Gets float increment mode for the specified feature.

Parameters
nodeNameGenICam device feature name
incModeSpinnaker GenAPI increment mode for the specified feature
Returns
An HRESULT indicating the success or failure of the function.

◆ FloatGetMax()

virtual HRESULT FloatGetMax ( const char *  nodeName,
double *  floatMax 
)
pure virtual

Gets maximum float value allowed for the specified feature.

Parameters
nodeNameGenICam device feature name
floatMaxThe maximum allowed value read from the device
Returns
An HRESULT indicating the success or failure of the function.

◆ FloatGetMin()

virtual HRESULT FloatGetMin ( const char *  nodeName,
double *  floatMin 
)
pure virtual

Gets minimum float value allowed for the specified feature.

Parameters
nodeNameGenICam device feature name
floatMinThe minimum allowed value read from the device
Returns
An HRESULT indicating the success or failure of the function.

◆ FloatGetValue()

virtual HRESULT FloatGetValue ( const char *  nodeName,
double *  value 
)
pure virtual

Gets float node value for the specified feature.

Parameters
nodeNameGenICam device feature name
valueThe value read from the device
Returns
An HRESULT indicating the success or failure of the function.

◆ FloatSetValue()

virtual HRESULT FloatSetValue ( const char *  nodeName,
double  value 
)
pure virtual

Sets float node value for the specified feature.

Parameters
nodeNameGenICam device feature name
valueThe value to set to device
Returns
An HRESULT indicating the success or failure of the function.

◆ GetCameraInfo()

virtual HRESULT GetCameraInfo ( unsigned int  index,
char *  model,
char *  type,
char *  serial,
size_t  bufferSize 
)
pure virtual

Retrieves general information about the camera at the specified index.

Parameters
indexThe index at which to retrieve the camera information
modelModel description of the camera
typeTransport layer description of the camera
serialSerial number of the camera
bufferSizeSize of the individual provided model, sensor, serial buffer in bytes
Returns
An HRESULT indicating the success or failure of the function.
Examples
SpinSimpleGUI_DirectShow.cpp.

◆ GetNumCameras()

virtual HRESULT GetNumCameras ( unsigned int *  numCameras)
pure virtual

Retrieves the number of cameras available for this Spinnaker DirectShow interface.

Parameters
numCamerasAn integer that represents the number of cameras discovered
Returns
An HRESULT indicating the success or failure of the function.
Examples
SpinSimpleGUI_DirectShow.cpp.

◆ GetSelectedCameraIndex()

virtual HRESULT GetSelectedCameraIndex ( unsigned int *  selectedIndex)
pure virtual

Retrieves an integer index to the currently selected camera.

Parameters
selectedIndexAn integer that represents the index of the selected camera
Returns
An HRESULT indicating the success or failure of the function.
Examples
SpinSimpleGUI_DirectShow.cpp.

◆ IntegerGetInc()

virtual HRESULT IntegerGetInc ( const char *  nodeName,
int64_t *  increment 
)
pure virtual

Gets integer step increment for the specified feature.

Parameters
nodeNameGenICam device feature name
incrementThe step increment value read from the device
Returns
An HRESULT indicating the success or failure of the function.

◆ IntegerGetIncMode()

virtual HRESULT IntegerGetIncMode ( const char *  nodeName,
Spinnaker::GenApi::EIncMode incMode 
)
pure virtual

Gets integer increment mode for the specified feature.

Parameters
nodeNameGenICam device feature name
incModeSpinnaker GenAPI increment mode for the specified feature
Returns
An HRESULT indicating the success or failure of the function.

◆ IntegerGetMax()

virtual HRESULT IntegerGetMax ( const char *  nodeName,
int64_t *  maxValue 
)
pure virtual

Gets maximum integer value allowed for the specified feature.

Parameters
nodeNameGenICam device feature name
maxValueThe maximum allowed value read from the device
Returns
An HRESULT indicating the success or failure of the function.

◆ IntegerGetMin()

virtual HRESULT IntegerGetMin ( const char *  nodeName,
int64_t *  minValue 
)
pure virtual

Gets minimum integer value allowed for the specified feature.

Parameters
nodeNameGenICam device feature name
minValueThe minimum allowed value read from the device
Returns
An HRESULT indicating the success or failure of the function.

◆ IntegerGetValue()

virtual HRESULT IntegerGetValue ( const char *  nodeName,
int64_t *  value 
)
pure virtual

Gets integer node value for the specified feature.

Parameters
nodeNameGenICam device feature name
valueThe value read from the device
Returns
An HRESULT indicating the success or failure of the function.
Examples
SpinSimpleGUI_DirectShow.cpp.

◆ IntegerSetValue()

virtual HRESULT IntegerSetValue ( const char *  nodeName,
int64_t  value 
)
pure virtual

Sets integer node value for the specified feature.

Parameters
nodeNameGenICam device feature name
valueThe value to set to device
Returns
An HRESULT indicating the success or failure of the function.

◆ IsStreaming()

virtual HRESULT IsStreaming ( bool *  isStreaming)
pure virtual

Checks if the selected camera is currently streaming.

Parameters
isStreamingFlag indicating whether camera is streaming or not
Returns
An HRESULT indicating the success or failure of the function.

◆ NodeGetDisplayName()

virtual HRESULT NodeGetDisplayName ( const char *  nodeName,
char *  displayName,
size_t  bufferSize 
)
pure virtual

Gets a name string for display.

Parameters
nodeNameGenICam device feature name
displayNameDisplay name of the device feature
bufferSizeSize of the provided displayName buffer in bytes
Returns
An HRESULT indicating the success or failure of the function.

◆ NodeGetType()

virtual HRESULT NodeGetType ( const char *  nodeName,
char *  typeName,
size_t  bufferSize 
)
pure virtual

Gets the type of the node.

Parameters
nodeNameGenICam device feature name
typeNameThe type of the node. Available type names are: Integer, Float, Boolean, String, Enumeration, Entry, Command and Other
bufferSizeSize of the provided typeName buffer in bytes
Returns
An HRESULT indicating the success or failure of the function.

◆ NodeIsAvailable()

virtual HRESULT NodeIsAvailable ( const char *  nodeName,
bool *  isAvailable 
)
pure virtual

Checks if a node is available.

Parameters
nodeNameGenICam device feature name
isAvailableFlag indicating whether node is available or not
Returns
An HRESULT indicating the success or failure of the function.
Examples
SpinSimpleGUI_DirectShow.cpp.

◆ NodeIsImplemented()

virtual HRESULT NodeIsImplemented ( const char *  nodeName,
bool *  isImplemented 
)
pure virtual

Checks if a node is implemented.

Parameters
nodeNameGenICam device feature name
isImplementedFlag indicating whether node is implemented or not
Returns
An HRESULT indicating the success or failure of the function.

◆ NodeIsReadable()

virtual HRESULT NodeIsReadable ( const char *  nodeName,
bool *  isReadable 
)
pure virtual

Checks if a node is readable.

Parameters
nodeNameGenICam device feature name
isReadableFlag indicating whether node is readable or not
Returns
An HRESULT indicating the success or failure of the function.
Examples
SpinSimpleGUI_DirectShow.cpp.

◆ NodeIsWritable()

virtual HRESULT NodeIsWritable ( const char *  nodeName,
bool *  isWritable 
)
pure virtual

Checks if a node is writable.

Parameters
nodeNameGenICam device feature name
isWritableFlag indicating whether node is writable or not
Returns
An HRESULT indicating the success or failure of the function.
Examples
SpinSimpleGUI_DirectShow.cpp.

◆ NodeMapGetNodeAtIndex()

virtual HRESULT NodeMapGetNodeAtIndex ( size_t  index,
char *  nodeName,
size_t  bufferSize 
)
pure virtual

Retrieves the string representation of the node at the specified index.

Parameters
indexNode index in the NodeMap
nodeNameGenICam node name at specified index to be populated
bufferSizeSize of the provided nodeName buffer in bytes
Returns
An HRESULT indicating the success or failure of the function.
Examples
SpinSimpleGUI_DirectShow.cpp.

◆ NodeMapGetNumNodes()

virtual HRESULT NodeMapGetNumNodes ( size_t *  numNodes)
pure virtual

Retrieves the number of nodes available in the node map for the currently selected camera.

Parameters
numNodesNumber of nodes available for the currently selected device
Returns
An HRESULT indicating the success or failure of the function.
Examples
SpinSimpleGUI_DirectShow.cpp.

◆ NodeToString()

virtual HRESULT NodeToString ( const char *  nodeName,
char *  valueAsString,
size_t  bufferSize 
)
pure virtual

Gets content of the node as string.

Parameters
nodeNameGenICam device feature name
valueAsStringString representation of the node value
bufferSizeSize of the provided valueAsString buffer in bytes
Returns
An HRESULT indicating the success or failure of the function.

◆ SetSelectedCameraIndex()

virtual HRESULT SetSelectedCameraIndex ( unsigned int  index,
bool  needsRelease = true 
)
pure virtual

Sets the currently selected camera to the index specified.

This function will do nothing if the selected index is out of range.

Parameters
indexThe index at which to retrieve the camera object
needsReleaseSpecifies whether to release the previously selected camera object
Returns
An HRESULT indicating the success or failure of the function.

◆ StringGetValue()

virtual HRESULT StringGetValue ( const char *  nodeName,
char *  value,
size_t  bufferSize 
)
pure virtual

Gets string node value for the specified feature.

Parameters
nodeNameGenICam device feature name
valueThe value read from the device
bufferSizeSize of the provided value buffer in bytes
Returns
An HRESULT indicating the success or failure of the function.

◆ StringSetValue()

virtual HRESULT StringSetValue ( const char *  nodeName,
const char *  value 
)
pure virtual

Sets string node value for the specified feature.

Parameters
nodeNameGenICam device feature name
valueThe value to set to device
Returns
An HRESULT indicating the success or failure of the function.

The documentation for this interface was generated from the following file: