Spinnaker SDK C++
4.2.0.88
 
 

 
Loading...
Searching...
No Matches
ImageEventHandlerImpl Class Reference
Inheritance diagram for ImageEventHandlerImpl:
ImageEventHandler IImageEventHandler EventHandler

Public Member Functions

 ImageEventHandlerImpl (string deviceSerial)
 
 ~ImageEventHandlerImpl ()
 
void OnImageEvent (ImagePtr image)
 Image event callback.
 
 ImageEventHandlerImpl (CameraPtr pCam)
 
 ~ImageEventHandlerImpl ()
 
void OnImageEvent (ImagePtr image)
 Image event callback.
 
int getImageCount ()
 
int getMaxImages ()
 
- Public Member Functions inherited from ImageEventHandler
 ImageEventHandler ()
 Default image handler constructor.
 
virtual ~ImageEventHandler ()
 Virtual Destructor.
 
- Public Member Functions inherited from IImageEventHandler
virtual ~IImageEventHandler ()
 
- Public Member Functions inherited from EventHandler
virtual ~EventHandler ()
 Virtual Destructor.
 
void SetEventType (EventType eventType)
 Sets the event type.
 
EventType GetEventType ()
 Gets the event type.
 
const uint8_t * GetEventPayloadData ()
 Gets the event payload data.
 
const size_t GetEventPayloadDataSize ()
 Gets the event payload data size.
 

Additional Inherited Members

- Protected Member Functions inherited from ImageEventHandler
ImageEventHandleroperator= (const ImageEventHandler &)
 Assignment operator.
 
virtual void OnImageEvent (ImagePtr image)=0
 Image event callback.
 
- Protected Member Functions inherited from IImageEventHandler
 IImageEventHandler ()
 
 IImageEventHandler (const IImageEventHandler &)
 
IImageEventHandleroperator= (const IImageEventHandler &)
 
virtual void OnImageEvent (ImagePtr image)=0
 
- Protected Member Functions inherited from EventHandler
 EventHandler ()
 
EventHandleroperator= (const EventHandler &)
 
void SetEventPayload (uint8_t *offset, size_t length)
 
- Protected Attributes inherited from EventHandler
EventData * m_pEventData
 

Detailed Description

Constructor & Destructor Documentation

◆ ImageEventHandlerImpl() [1/2]

ImageEventHandlerImpl ( string  deviceSerial)
inline

◆ ~ImageEventHandlerImpl() [1/2]

◆ ImageEventHandlerImpl() [2/2]

ImageEventHandlerImpl ( CameraPtr  pCam)
inline

◆ ~ImageEventHandlerImpl() [2/2]

~ImageEventHandlerImpl ( )
inline

Member Function Documentation

◆ getImageCount()

int getImageCount ( )
inline

◆ getMaxImages()

int getMaxImages ( )
inline

◆ OnImageEvent() [1/2]

void OnImageEvent ( ImagePtr  image)
virtual

Image event callback.

Parameters
imageThe ImagePtr object

Implements ImageEventHandler.

Examples
AcquisitionMultipleCameraRecovery.cpp.

◆ OnImageEvent() [2/2]

void OnImageEvent ( ImagePtr  image)
inlinevirtual

Image event callback.

Parameters
imageThe ImagePtr object

Implements ImageEventHandler.


The documentation for this class was generated from the following files: