Spinnaker SDK C++
4.3.0.190
 
 

 
Loading...
Searching...
No Matches
NodeMapFactory Class

Classes

class  CNodeMapFactory
 The node map factory is used for creating node maps from camera description files. See the following for some examples.
More...
 

Enumerations

enum  ECacheUsage_t { CacheUsage_Automatic , CacheUsage_ForceWrite , CacheUsage_ForceRead , CacheUsage_Ignore }
 Lists the cache usage strategies. More...
 
enum  EContentType_t { ContentType_Xml , ContentType_ZippedXml }
 Lists the processable file types. More...
 

Detailed Description

Enumeration Type Documentation

◆ ECacheUsage_t

Lists the cache usage strategies.

The cache stores preprocessed camera description xml files providing faster access or smaller footprint. note The environment variable GENICAM_CACHE_VERSION, e.g. GENICAM_CACHE_V3_0, must contain the path to cache directory for using the cache.

Enumerator
CacheUsage_Automatic 

The use of cache files is determined automatically.

CacheUsage_ForceWrite 

Forces the loading and preprocessing of the camera description xml file.

If a cache directory is available the result of preprocessing is written to the cache.

CacheUsage_ForceRead 

Suppresses loading and preprocessing of the camera description xml file and.

forces reading a cache file from cache directory. Fails if no matching cache file is available.

CacheUsage_Ignore 

Forces the loading and preprocessing of the camera description xml file.

No cache file is written.

◆ EContentType_t

Lists the processable file types.

Enumerator
ContentType_Xml 

XML camera description file text.

ContentType_ZippedXml 

Zipped XML camera description file text.