Classes | |
| struct | DeviceInformationStruct |
| Return type for ShowModal() method in CameraSelectionWindow. More... | |
| class | CameraSelectionWindow |
| The CameraSelectionWindow object represents a dialog that provides a graphical interface that lists number of cameras and interfaces available to the library. More... | |
| class | PropertyGridWindow |
| The PropertyGridWindow object represents a dialog that provides a graphical interface to view and control features on a camera object. More... | |
| class | ImageDrawingWindow |
| The ImageDrawingWindow object represents a dialog that displays live images from a connected camera object. More... | |
| class | GUIFactory |
| The GUIFactory object represents a C++ object that provides access to GUI objects such as CameraSelectionWindow, PropertyGridWindow and dialogs defined in GUI XML. More... | |
Typedefs | |
| typedef void(* | ClickedEventCallback) (bool isCamera, Spinnaker::CameraPtr *pCamera, Spinnaker::InterfacePtr *pInterface, Spinnaker::SystemPtr *pSystem, bool isSystem) |
| Device clicked event callback function prototype. | |
| typedef void(* | FirmwareUpdateEventCallback) (bool isStarting, bool isFinished, bool isSuccessful, const char *pErrorMessage, Spinnaker::CameraPtr *pCamera) |
| Device firmware update event callback function prototype. | |
| typedef void(* | IPConfigEventCallback) (bool isStarting, bool isFinished, Spinnaker::CameraPtr *pCamera) |
| IP configuration event callback function prototype. | |
| typedef void(* ClickedEventCallback) (bool isCamera, Spinnaker::CameraPtr *pCamera, Spinnaker::InterfacePtr *pInterface, Spinnaker::SystemPtr *pSystem, bool isSystem) |
Device clicked event callback function prototype.
Defines the syntax of the clicked callback function that is passed into RegisterDoubleClickedCallback() and RegisterSingleClickedCallback().
| isCamera | boolean indicating whether the object clicked is a camera. |
| pCamera | pointer to clicked camera object. |
| pInterface | pointer to clicked interface object. |
| pSystem | pointer to clicked system object. |
| isSystem | boolean indicating whether the system object is clicked. |
| typedef void(* FirmwareUpdateEventCallback) (bool isStarting, bool isFinished, bool isSuccessful, const char *pErrorMessage, Spinnaker::CameraPtr *pCamera) |
Device firmware update event callback function prototype.
Defines the syntax of the firmware update callback function that is passed into RegisterFirmwareUpdateStartingCallback() and RegisterFirmwareUpdateFinishedCallback().
| boolean | indicating whether firmware update is starting. |
| boolean | indicating whether firmware update is finished. |
| boolean | indicating whether firmware update is successful. |
| char* | containing error message returned from firmware update. |
| pointer | to camera object being updated. |
| typedef void(* IPConfigEventCallback) (bool isStarting, bool isFinished, Spinnaker::CameraPtr *pCamera) |
IP configuration event callback function prototype.
Defines the syntax of the IP configuration callback function that is passed into RegisterIPConfigStartingCallback() and RegisterIPConfigFinishedCallback().
| boolean | indicating whether firmware update is starting. |
| boolean | indicating whether firmware update is finished. |
| pointer | to camera object being updated. |