FG-PGE-13S3S-U Release Notes
Product Information
Product: FG-PGE-13S3S-U
Firmware Version: 2406.0001.014.000
Bugs Fixed
| Bug | Description |
|---|---|
| F-12388 | The MFG test DefectPixelScripts failed with error: 'ChunkExposureTime' is not readable. |
Changes
| Change | Description |
|---|---|
| FG-PGE-13S3S-U-C (IMX990): initial release |
Known Issues
| Issue | Description |
|---|---|
| F-12260 | The serial port testing failed at baud rate is 300. |
| F-12278 | The TestBulbTriggerSpin failed with error that the chunk exposure time was out of range. |
| F-12279 | The TestHighFrameRateChunkSpin failed to run completely. |