Skip to content

FlyCapture2 Feature Comparison with Spinnaker

Spinnaker re-engineered the way camera features are accessed compared to FlyCapture2. Camera features and properties are now named according to the standard GenICam Feature Naming Convention (SFNC). For programmers not familiar with GenICam, see EMVA's GenICam Standard introduction.

IIDC register read and write is no longer available. Instead, camera properties are accessed through the GenICam node map.

Feature Comparison

FlyCapture2 Feature Spinnaker Equivalent Notes
IIDC register read and write (AsyncTriggerEx) GenICam node map get/set values (Acquisition) Typically used to access camera settings or control camera state
Embedded image info (MultipleCameraWriteToDiskEx) Chunk data (ChunkData) Allows the camera to add image metadata to the transmission
ImageEvents (ImageEventEx) GenICam message or event channel (DeviceEvents) Signals the user when events such as image arrival occur
FC2Config struct (grab mode, num_buffer) (RecordingDialog) Stream node map (NodeMapInfo) Used to set buffer mode and number of buffers
Error return code (FlyCapture2Test) Exceptions (Acquisition) New error handling uses exceptions instead of error codes
Format7 packet size for bandwidth control (GigEGrabEx) DeviceLinkLayerThroughputLimit Defines total available bandwidth for the camera
Imaging mode (e.g., Format7 mode 1) (CustomImageEx) Binning controls in GenICam Reduces resolution to achieve faster frame rate or brighter images
Events callback (BusEventEx_CSharp) Register event class with overloaded functions (EnumerationEvents) Bus event callbacks such as camera arrival and removal
GUID to identify and track cameras (FlyCapture2Test) Unique camera class (Acquisition) Used to access camera features in the SDK

Terminology Changes

FlyCapture2 Spinnaker Notes
Brightness Black Level Output of the camera when not illuminated
Exposure Exposure and Gain Combination of the camera's shutter and gain; also known as average intensity
Shutter Exposure Amount of time the electronic shutter stays open
Packet Size GevSCPSPacketSize Size of packets, in bytes, to send on the selected channel for a GVSP transmitter or receiver
Packet Delay GevSCPD Delay to insert between each packet for this stream channel
Trigger Mode 0 TriggerSelector → FrameStart, AcquisitionMode → Continuous Camera starts integration of light from external trigger source; exposure time controlled by Exposure setting
Trigger Mode 1 TriggerSelector → ExposureActive, AcquisitionMode → Continuous Same as Trigger Mode 0 except sensor exposure time is controlled by the external trigger source
Trigger Mode X Logic Block (Blackfly S only) All other trigger modes. Logic Block allows you to define any internal logic, including custom trigger modes. See Using Logic Blocks
Memory Channel User Set Storing camera settings onto non-volatile memory
High Dynamic Range (HDR) Sequencer (Blackfly S) / HDR (USB3 Vision cameras) Cycling of frames with different settings (gain, exposure) to capture the dynamic range of the scene. See Using the Sequencer Feature
Frame Buffer Transfer Control Transferring of image data to the host
Video Mode Image Format Control Controls that define binning/decimation and image size
Mirror / Flip Reverse X / Reverse Y Flipping the image horizontally or vertically
Grab Acquisition Process of capturing images
Property Feature / Node Camera parameter accessible via GenICam node map