Skip to content

Struct _spinJPEGOption

ClassList > _spinJPEGOption

More...

  • #include <SpinnakerDefsC.h>

Public Attributes

Type Name
bool8_t progressive
unsigned int quality
unsigned int reserved

Detailed Description

Options for saving JPEG images. Used in saving PPM images with a call to spinImageSaveJpeg().

Public Attributes Documentation

variable progressive

bool8_t _spinJPEGOption::progressive;

Whether to save as a progressive JPEG file.


variable quality

unsigned int _spinJPEGOption::quality;

JPEG image quality in range (0-100). * 100 - Superb quality. * 75 - Good quality. * 50 - Normal quality. * 10 - Poor quality.


variable reserved

unsigned int _spinJPEGOption::reserved[16];

Reserved for future use.



The documentation for this class was generated from the following file /workspace/include/spinc/SpinnakerDefsC.h