Skip to content

Struct _spinLibraryVersion

ClassList > _spinLibraryVersion

More...

  • #include <SpinnakerDefsC.h>

Public Attributes

Type Name
unsigned int build
unsigned int major
unsigned int minor
unsigned int type

Detailed Description

Provides easier access to the current version of Spinnaker.

Public Attributes Documentation

variable build

unsigned int _spinLibraryVersion::build;

Build number of the library


variable major

unsigned int _spinLibraryVersion::major;

Major version of the library


variable minor

unsigned int _spinLibraryVersion::minor;

Minor version of the library


variable type

unsigned int _spinLibraryVersion::type;

Version type of the library



The documentation for this class was generated from the following file /workspace/include/spinc/SpinnakerDefsC.h