Namespace SpinnakerNET¶
Namespaces¶
| Type | Name |
|---|---|
| namespace | Base |
| namespace | GenApi |
Classes¶
| Type | Name |
|---|---|
| struct | ActionCommandResult |
| struct | AviOption |
| struct | BmpOption |
| struct | CCMSettings |
| class | DeviceEventRedirector |
| struct | H264Option |
| interface | IManagedCamera The managed camera interface object class. |
| interface | IManagedCameraBase |
| interface | IManagedCameraList |
| interface | IManagedImage |
| interface | IManagedInterface |
| interface | IManagedInterfaceList |
| interface | IManagedSystem |
| class | ImageEventRedirector |
| struct | ImagePixel |
| class | InterfaceEventRedirector |
| struct | JpegOption |
| struct | Jpg2Option |
| struct | LibraryVersion |
| class | LoggingEventRedirector |
| struct | MJPGOption |
| class | ManagedCamera The managed camera object class. |
| class | ManagedCameraBase |
| class | ManagedCameraList |
| class | ManagedChunkData The managed chunk data which contains additional information about an image. |
| class | ManagedImage The managed image object class. |
| class | ManagedImageStatistics |
| class | ManagedImageUtility Helper functions for managed image objects. |
| class | ManagedImageUtilityPolarization Helper functions for managed image objects of pixel format Polarized8 and BayerRGPolarized8. |
| class | ManagedImageUtilityStereo Helper functions for managed image objects. |
| struct | ManagedInferenceBoundingBox A single managed inference bounding box. |
| class | ManagedInferenceBoundingBoxResult The managed inference bounding box result. |
| class | ManagedInterface |
| class | ManagedInterfaceList |
| class | ManagedLogger |
| class | ManagedLoggingEventData |
| class | ManagedPointCloud |
| class | ManagedSystem |
| class | ManagedTransportLayerDevice Part of the Managed QuickSpin API to provide access to camera information without having to first initialize the camera. |
| class | ManagedTransportLayerInterface Part of the Managed QuickSpin API to provide access to camera information without having to first initialize the camera. |
| class | ManagedTransportLayerStream Part of the Managed QuickSpin API to provide access to camera information without having to first initialize the camera. |
| class | ManagedTransportLayerSystem Part of the Managed QuickSpin API to provide access to camera information without having to first initialize the camera. |
| struct | PgmOption |
| struct | PngOption |
| struct | PointCloudParameters |
| struct | PpmOption |
| class | SpinnakerException |
| struct | Stereo3DPoint |
| struct | StereoCameraParameters |
| class | SystemEventRedirector |
| struct | TiffOption |
| class | abstract |
Public Types¶
| Type | Name |
|---|---|
| enum | ActionCommandStatus |
| enum | BufferOwnership |
| enum | CCMApplication |
| enum | CCMColorSpace |
| enum | CCMColorTemperature |
| enum | CCMSensor |
| enum | CCMType |
| enum | ColorProcessingAlgorithm |
| enum | DisparityProcessingMethod |
| enum | Error |
| enum | HeatmapColor |
| enum | ImageFileFormat |
| enum | ImagePayloadType |
| enum | ImageStatus |
| enum | InferenceBoundingBoxType |
| enum | ManagedLogType |
| enum | ManagedLoggingLevel |
| typedef void(__stdcall * | OnDeviceArrivalNative |
| typedef void(__stdcall * | OnDeviceEventNative |
| typedef void(__stdcall * | OnDeviceRemovalNative |
| typedef void(__stdcall * | OnImageEventNative |
| typedef void(__stdcall * | OnInterfaceArrivalNative |
| typedef void(__stdcall * | OnInterfaceRemovalNative |
| typedef void(__stdcall * | OnLoggingEventNative |
| enum | PolarizationQuadrant |
| enum | StatisticsChannel |
| enum | TIFFCompressionMethod |
| enum | TLPayloadType |
| enum | TLPixelFormatNamespace |
Public Functions¶
| Type | Name |
|---|---|
| delegate void | ManagedLogEventCallback (SpinnakerNET::ManagedLoggingEventData^ logEvent) |
| delegate void | OnDeviceArrivalDelegate (Spinnaker::CameraPtr) |
| delegate void | OnDeviceEventDelegate (Spinnaker::GenICam::gcstring eventName) |
| delegate void | OnDeviceRemovalDelegate (Spinnaker::CameraPtr) |
| delegate void | OnImageEventDelegate (Spinnaker::ImagePtr image) |
| delegate void | OnInterfaceArrivalDelegate (Spinnaker::InterfacePtr) |
| delegate void | OnInterfaceRemovalDelegate (Spinnaker::InterfacePtr) |
| delegate void | OnLoggingEventDelegate (Spinnaker::LoggingEventDataPtr loggingEvent) |
| inline ::System::String | ToManaged (const char * str) |
| inline ::System::String | ToManaged (const char * str, size_t len) |
| inline ::System::String | ToManaged (const Spinnaker::GenICam::gcstring & str) |
| Spinnaker::GenICam::gcstring | ToNative (::System::String ^ str) |
| bool | is_node (void * pType) |
| bool | is_node (IntPtr type) |
| T * | node_cast (void * pType) |
| T * | node_cast (IntPtr type) |
| T * | type_cast (void * pType) |
| T * | type_cast (IntPtr type) |
Public Types Documentation¶
enum ActionCommandStatus¶
enum SpinnakerNET::ActionCommandStatus {
ACTION_COMMAND_STATUS_OK = 0,
ACTION_COMMAND_STATUS_NO_REF_TIME = 0x8013,
ACTION_COMMAND_STATUS_OVERFLOW = 0x8015,
ACTION_COMMAND_STATUS_ACTION_LATE = 0x8016,
ACTION_COMMAND_STATUS_ERROR = 0x8FFF
};
Possible Status Codes Returned from Action Command
enum BufferOwnership¶
enum CCMApplication¶
enum CCMColorSpace¶
enum CCMColorTemperature¶
enum SpinnakerNET::CCMColorTemperature {
INCANDESCENT_2765K,
TUNGSTEN_2800K,
WARM_FLUORESCENT_3000K,
HALOGEN_3188K,
COOL_FLUORESCENT_4000K,
LED_4649K,
LED_H_AND_E_4649K,
FLUORESCENT_4665K,
SUNNY_5000K,
DAYLIGHT_5034K,
DAYLIGHT_H_AND_E_5034K,
CLOUDY_6500K,
SHADE_8000K,
GENERAL,
NUM_CCM_COLOR_TEMPERATURE
};
enum CCMSensor¶
enum SpinnakerNET::CCMSensor {
IMX226,
IMX249,
IMX250,
IMX252,
IMX253,
IMX255,
IMX264,
IMX265,
IMX267,
IMX273,
IMX287,
IMX296,
IMX297,
IMX304,
IMX327,
IMX334,
IMX342,
IMX367,
IMX387,
IMX392,
IMX420,
IMX421,
IMX422,
IMX425,
IMX428,
IMX429,
IMX430,
AR0521,
NUM_CCM_SENSOR
};
enum CCMType¶
enum ColorProcessingAlgorithm¶
enum SpinnakerNET::ColorProcessingAlgorithm {
NONE,
NEAREST_NEIGHBOR,
NEAREST_NEIGHBOR_AVG,
BILINEAR,
EDGE_SENSING,
HQ_LINEAR,
IPP,
DIRECTIONAL_FILTER,
RIGOROUS,
WEIGHTED_DIRECTIONAL_FILTER
};
Color processing algorithms. Please refer to our knowledge base at article at https://www.teledynevisionsolutions.com/support/support-center/technical-guidance/iis/different-color-processing-algorithms-in-flycapture2/ for complete details for each algorithm.
enum DisparityProcessingMethod¶
Strategies for post-processing disparity maps to fill missing or invalid regions using weighted interpolation, joint bilateral filtering, domain transfer, and speckle filtering. Each strategy balances accuracy, density, and computational cost differently.
enum Error¶
enum SpinnakerNET::Error {
SPINNAKER_ERR_SUCCESS = 0,
SPINNAKER_ERR_ERROR = -1001,
SPINNAKER_ERR_NOT_INITIALIZED = -1002,
SPINNAKER_ERR_NOT_IMPLEMENTED = -1003,
SPINNAKER_ERR_RESOURCE_IN_USE = -1004,
SPINNAKER_ERR_ACCESS_DENIED = -1005,
SPINNAKER_ERR_INVALID_HANDLE = -1006,
SPINNAKER_ERR_INVALID_ID = -1007,
SPINNAKER_ERR_NO_DATA = -1008,
SPINNAKER_ERR_INVALID_PARAMETER = -1009,
SPINNAKER_ERR_IO = -1010,
SPINNAKER_ERR_TIMEOUT = -1011,
SPINNAKER_ERR_ABORT = -1012,
SPINNAKER_ERR_INVALID_BUFFER = -1013,
SPINNAKER_ERR_NOT_AVAILABLE = -1014,
SPINNAKER_ERR_INVALID_ADDRESS = -1015,
SPINNAKER_ERR_BUFFER_TOO_SMALL = -1016,
SPINNAKER_ERR_INVALID_INDEX = -1017,
SPINNAKER_ERR_PARSING_CHUNK_DATA = -1018,
SPINNAKER_ERR_INVALID_VALUE = -1019,
SPINNAKER_ERR_RESOURCE_EXHAUSTED = -1020,
SPINNAKER_ERR_OUT_OF_MEMORY = -1021,
SPINNAKER_ERR_BUSY = -1022,
SPINNAKER_ERR_IP_CONFLICT = -1023,
SPINNAKER_ERR_INVALID_CAMERA = -1024,
SPINNAKER_ERR_GENICAM_INVALID_ARGUMENT = -2001,
SPINNAKER_ERR_GENICAM_OUT_OF_RANGE = -2002,
SPINNAKER_ERR_GENICAM_PROPERTY = -2003,
SPINNAKER_ERR_GENICAM_RUN_TIME = -2004,
SPINNAKER_ERR_GENICAM_LOGICAL = -2005,
SPINNAKER_ERR_GENICAM_ACCESS = -2006,
SPINNAKER_ERR_GENICAM_TIMEOUT = -2007,
SPINNAKER_ERR_GENICAM_DYNAMIC_CAST = -2008,
SPINNAKER_ERR_GENICAM_GENERIC = -2009,
SPINNAKER_ERR_IM_CONVERT = -3001,
SPINNAKER_ERR_IM_COPY = -3002,
SPINNAKER_ERR_IM_MALLOC = -3003,
SPINNAKER_ERR_IM_NOT_SUPPORTED = -3004,
SPINNAKER_ERR_IM_HISTOGRAM_RANGE = -3005,
SPINNAKER_ERR_IM_HISTOGRAM_MEAN = -3006,
SPINNAKER_ERR_IM_MIN_MAX = -3007,
SPINNAKER_ERR_IM_COLOR_CONVERSION = -3008,
SPINNAKER_ERR_IM_DECOMPRESSION = -3009,
SPINNAKER_ERR_IM_INVALID_IMAGE_TYPE = -3010,
SPINNAKER_ERR_GPU_DECOMPRESSION = -3100,
SPINNAKER_ERR_GPU_NOT_SUPPORTED = -3101,
SPINNAKER_ERR_STEREO_INVALID_PIXEL_FORMAT = -3200,
SPINNAKER_ERR_STEREO_RESOLUTION_MISMATCH = -3201,
SPINNAKER_ERR_STEREO_INVALID_FILENAME = -3202,
SPINNAKER_ERR_STEREO_INVALID_PLY_FILE = -3203,
SPINNAKER_ERR_STEREO_MALLOC = -3204,
SPINNAKER_ERR_STEREO_SPECKLE_FILTER = -3205,
SPINNAKER_ERR_CUSTOM_ID = -10000
};
The error codes used in SpinnakerNet. These codes are returned as part of SpinnakerNet::ManagedException. The error codes in the range of -1000 to -1999 are reserved for exceptions that map directly to GenTL values. The error codes in the range of -2000 to -2999 are reserved for GenICam related errors.
enum HeatmapColor¶
enum SpinnakerNET::HeatmapColor {
HEATMAP_BLACK = 1,
HEATMAP_BLUE = 2,
HEATMAP_CYAN = 3,
HEATMAP_GREEN = 4,
HEATMAP_YELLOW = 5,
HEATMAP_RED = 6,
HEATMAP_WHITE = 7
};
enum ImageFileFormat¶
enum SpinnakerNET::ImageFileFormat {
FromFileExtension = -1,
Pgm,
Ppm,
Bmp,
Jpeg,
Jpeg2000,
Tiff,
Png,
Raw
};
File formats to be used for saving images to disk.
enum ImagePayloadType¶
enum SpinnakerNET::ImagePayloadType {
IMAGE_PAYLOAD_TYPE_UNKNOWN = -1,
IMAGE_PAYLOAD_TYPE_IMAGE,
IMAGE_PAYLOAD_TYPE_EXTENDED_CHUNK,
IMAGE_PAYLOAD_TYPE_JPEG,
IMAGE_PAYLOAD_TYPE_LOSSLESS_COMPRESSED,
IMAGE_PAYLOAD_TYPE_LOSSY_COMPRESSED,
IMAGE_PAYLOAD_TYPE_JPEG_LOSSLESS_COMPRESSED,
IMAGE_PAYLOAD_TYPE_RAW_SENSOR1,
IMAGE_PAYLOAD_TYPE_RAW_SENSOR2,
IMAGE_PAYLOAD_TYPE_RECTIFIED_SENSOR1,
IMAGE_PAYLOAD_TYPE_RECTIFIED_SENSOR2,
IMAGE_PAYLOAD_TYPE_DISPARITY_SENSOR1,
IMAGE_PAYLOAD_TYPE_GENDC_GENERIC,
IMAGE_PAYLOAD_TYPE_RANGE_SENSOR1,
IMAGE_PAYLOAD_TYPE_RANGE_SENSOR2
};
enum ImageStatus¶
enum SpinnakerNET::ImageStatus {
IMAGE_UNKNOWN_ERROR = -1,
IMAGE_NO_ERROR = 0,
IMAGE_CRC_CHECK_FAILED = 1,
IMAGE_DATA_OVERFLOW = 2,
IMAGE_MISSING_PACKETS = 3,
IMAGE_LEADER_BUFFER_SIZE_INCONSISTENT = 4,
IMAGE_TRAILER_BUFFER_SIZE_INCONSISTENT = 5,
IMAGE_PACKETID_INCONSISTENT = 6,
IMAGE_MISSING_LEADER = 7,
IMAGE_MISSING_TRAILER = 8,
IMAGE_DATA_INCOMPLETE = 9,
IMAGE_INFO_INCONSISTENT = 10,
IMAGE_CHUNK_DATA_INVALID = 11,
IMAGE_NO_SYSTEM_RESOURCES = 12,
IMAGE_GENDC_DATA_INVALID = 13,
IMAGE_GENDC_PART_DATA_INVALID = 14
};
Status of images returned from GetNextImage() call.
enum InferenceBoundingBoxType¶
Inference Bounding Box Type
enum ManagedLogType¶
enum ManagedLoggingLevel¶
enum SpinnakerNET::ManagedLoggingLevel {
LOG_LEVEL_OFF = -1,
LOG_LEVEL_FATAL = 0,
LOG_LEVEL_ALERT = 100,
LOG_LEVEL_CRIT = 200,
LOG_LEVEL_ERROR = 300,
LOG_LEVEL_WARN = 400,
LOG_LEVEL_NOTICE = 500,
LOG_LEVEL_INFO = 600,
LOG_LEVEL_DEBUG = 700,
LOG_LEVEL_NOTSET = 800
};
typedef OnDeviceArrivalNative¶
typedef OnDeviceEventNative¶
typedef void(__stdcall * SpinnakerNET::OnDeviceEventNative) (Spinnaker::GenICam::gcstring eventName);
typedef OnDeviceRemovalNative¶
typedef OnImageEventNative¶
typedef OnInterfaceArrivalNative¶
typedef OnInterfaceRemovalNative¶
typedef OnLoggingEventNative¶
typedef void(__stdcall * SpinnakerNET::OnLoggingEventNative) (Spinnaker::LoggingEventDataPtr loggingEvent);
enum PolarizationQuadrant¶
enum StatisticsChannel¶
enum SpinnakerNET::StatisticsChannel {
Grey,
Red,
Green,
Blue,
Hue,
Saturation,
Lightness,
NumberOfStatisticsChannels
};
Channels that allow statistics to be calculated.
enum TIFFCompressionMethod¶
enum SpinnakerNET::TIFFCompressionMethod {
None = 1,
PackBits,
Deflate,
AdobeDeflate,
CcittFax3,
CcittFax4,
Lzw,
Jpeg
};
Compression method to use for encoding TIFF images.
enum TLPayloadType¶
enum SpinnakerNET::TLPayloadType {
TLPAYLOAD_TYPE_UNKNOWN = 0,
TLPAYLOAD_TYPE_IMAGE = 1,
TLPAYLOAD_TYPE_RAW_DATA = 2,
TLPAYLOAD_TYPE_FILE = 3,
TLPAYLOAD_TYPE_CHUNK_DATA = 4,
TLPAYLOAD_TYPE_JPEG = 5,
TLPAYLOAD_TYPE_JPEG2000 = 6,
TLPAYLOAD_TYPE_H264 = 7,
TLPAYLOAD_TYPE_CHUNK_ONLY = 8,
TLPAYLOAD_TYPE_DEVICE_SPECIFIC = 9,
TLPAYLOAD_TYPE_MULTI_PART = 10,
TLPAYLOAD_TYPE_CUSTOM_ID = 1000,
TLPAYLOAD_TYPE_LOSSLESS_COMPRESSED = TLPAYLOAD_TYPE_CUSTOM_ID + 1,
TLPAYLOAD_TYPE_LOSSY_COMPRESSED = TLPAYLOAD_TYPE_CUSTOM_ID + 2,
TLPAYLOAD_TYPE_JPEG_LOSSLESS_COMPRESSED = TLPAYLOAD_TYPE_CUSTOM_ID + 3
};
Enumeration of TLType dependent payload types. Introduced in GenTL v1.2
enum TLPixelFormatNamespace¶
enum SpinnakerNET::TLPixelFormatNamespace {
TLPIXELFORMAT_NAMESPACE_UNKNOWN = 0,
TLPIXELFORMAT_NAMESPACE_GEV = 1,
TLPIXELFORMAT_NAMESPACE_IIDC = 2,
TLPIXELFORMAT_NAMESPACE_PFNC_16BIT = 3,
TLPIXELFORMAT_NAMESPACE_PFNC_32BIT = 4,
TLPIXELFORMAT_NAMESPACE_CUSTOM_ID = 1000
};
Public Functions Documentation¶
function ManagedLogEventCallback¶
delegate void SpinnakerNET::ManagedLogEventCallback (
SpinnakerNET::ManagedLoggingEventData ^ logEvent
)
function OnDeviceArrivalDelegate¶
function OnDeviceEventDelegate¶
function OnDeviceRemovalDelegate¶
function OnImageEventDelegate¶
function OnInterfaceArrivalDelegate¶
function OnInterfaceRemovalDelegate¶
function OnLoggingEventDelegate¶
function ToManaged¶
function ToManaged¶
function ToManaged¶
function ToNative¶
function is_node¶
function is_node¶
function node_cast¶
function node_cast¶
function type_cast¶
function type_cast¶
The documentation for this class was generated from the following file /workspace/src/SpinnakerNET/IManagedCamera.h