Functions | |
| virtual GenICam::gcstring | GetSymbolic () const =0 |
| Get symbolic enum value. | |
| virtual double | GetNumericValue ()=0 |
| Get double number associated with the entry. | |
| virtual bool | IsSelfClearing ()=0 |
| Indicates if the corresponding EnumEntry is self clearing. | |
Variables | |
| interface SPINNAKER_API_ABSTRACT | IEnumEntry |
| Interface of single enum value. | |
|
pure virtual |
Get double number associated with the entry.
|
pure virtual |
Get symbolic enum value.
|
pure virtual |
Indicates if the corresponding EnumEntry is self clearing.
| interface SPINNAKER_API_ABSTRACT IEnumEntry |
Interface of single enum value.
Maps of Enum Values to symbolic values