Spinnaker SDK C++
4.2.0.83
 
 

 
Loading...
Searching...
No Matches
INodeMapDyn Interface

Functions

virtual void LoadXMLFromFile (const GenICam::gcstring &FileName)=0
 Loads an XML from a file.
 
virtual void LoadXMLFromFileInject (const GenICam::gcstring &TargetFileName, const GenICam::gcstring &InjectFileName)=0
 Loads an XML from a file with injection.
 
virtual void LoadXMLFromString (const GenICam::gcstring &XMLData)=0
 Loads an XML from a string.
 
virtual void LoadXMLFromStringInject (const GenICam::gcstring &TargetXMLData, const GenICam::gcstring &InjectXMLData)=0
 Loads an XML from a string with injection.
 
virtual void PreprocessXMLFromFile (const GenICam::gcstring &XMLFileName, const GenICam::gcstring &StyleSheetFileName, const GenICam::gcstring &OutputFileName, const uint32_t XMLValidation=xvDefault)=0
 Loads an XML, checks it for correctness, pre-processes it, caches it, and optionally applies a style sheet, and optionally writes it to a file.
 
virtual void MergeXMLFiles (const GenICam::gcstring &TargetFileName, const GenICam::gcstring &InjectedFileName, const GenICam::gcstring &OutputFileName)=0
 Injects an XML file into a target file.
 
virtual void ExtractIndependentSubtree (const GenICam::gcstring &XMLData, const GenICam::gcstring &InjectXMLData, const GenICam::gcstring &SubTreeRootNodeName, GenICam::gcstring &ExtractedSubtree)=0
 Extract independent subtree.
 
virtual void GetSupportedSchemaVersions (GenICam::gcstring_vector &SchemaVersions)=0
 Gets a list of supported schema versions.
 
virtual void LoadXMLFromZIPFile (const GenICam::gcstring &ZipFileName)=0
 Loads an XML from a ZIP file.
 
virtual void LoadXMLFromZIPData (const void *zipData, size_t zipSize)=0
 Loads an XML from a ZIP data buffer.
 
virtual void PreprocessXMLFromZIPFile (const GenICam::gcstring &XMLFileName, const GenICam::gcstring &StyleSheetFileName, const GenICam::gcstring &OutputFileName, const uint32_t XMLValidation=xvDefault)=0
 Loads a Zipped XML, checks it for correctness, pre-processes it, caches it, and optionally applies a style sheet, and optionally writes it to a file.
 

Variables

interface SPINNAKER_API_ABSTRACT INodeMapDyn
 Interface to access the node map.
 

Detailed Description

Function Documentation

◆ ExtractIndependentSubtree()

virtual void ExtractIndependentSubtree ( const GenICam::gcstring XMLData,
const GenICam::gcstring InjectXMLData,
const GenICam::gcstring SubTreeRootNodeName,
GenICam::gcstring ExtractedSubtree 
)
pure virtual

Extract independent subtree.

Parameters
InjectXMLData

‍The XML data the subtree is extracted from.

SubTreeRootNodeName

‍Optional XML data that is injected before extracting the subtree. No effect if an empty string is passed.

ExtractedSubtree

‍The name of the node that represents the root of the subtree that shall be extracted.> The returned extracted subtree as string.

◆ GetSupportedSchemaVersions()

virtual void GetSupportedSchemaVersions ( GenICam::gcstring_vector &  SchemaVersions)
pure virtual

Gets a list of supported schema versions.

Each list entry is a string with the format "Major.Minor" were Major and Minor are integers Example: {"1.1", "1.2"} indicates that the schema v1.1 and v1.2 are supported. The SubMinor version number is not given since it is for fully compatible bug fixes only

◆ LoadXMLFromFile()

virtual void LoadXMLFromFile ( const GenICam::gcstring FileName)
pure virtual

Loads an XML from a file.

◆ LoadXMLFromFileInject()

virtual void LoadXMLFromFileInject ( const GenICam::gcstring TargetFileName,
const GenICam::gcstring InjectFileName 
)
pure virtual

Loads an XML from a file with injection.

◆ LoadXMLFromString()

virtual void LoadXMLFromString ( const GenICam::gcstring XMLData)
pure virtual

Loads an XML from a string.

◆ LoadXMLFromStringInject()

virtual void LoadXMLFromStringInject ( const GenICam::gcstring TargetXMLData,
const GenICam::gcstring InjectXMLData 
)
pure virtual

Loads an XML from a string with injection.

◆ LoadXMLFromZIPData()

virtual void LoadXMLFromZIPData ( const void *  zipData,
size_t  zipSize 
)
pure virtual

Loads an XML from a ZIP data buffer.

◆ LoadXMLFromZIPFile()

virtual void LoadXMLFromZIPFile ( const GenICam::gcstring ZipFileName)
pure virtual

Loads an XML from a ZIP file.

◆ MergeXMLFiles()

virtual void MergeXMLFiles ( const GenICam::gcstring TargetFileName,
const GenICam::gcstring InjectedFileName,
const GenICam::gcstring OutputFileName 
)
pure virtual

Injects an XML file into a target file.

Parameters
InjectedFileName

‍Name of the target XML file to process

OutputFileName

‍Name of the Injected XML file to process> Name of the oputput file

◆ PreprocessXMLFromFile()

virtual void PreprocessXMLFromFile ( const GenICam::gcstring XMLFileName,
const GenICam::gcstring StyleSheetFileName,
const GenICam::gcstring OutputFileName,
const uint32_t  XMLValidation = xvDefault 
)
pure virtual

Loads an XML, checks it for correctness, pre-processes it, caches it, and optionally applies a style sheet, and optionally writes it to a file.

Parameters
StyleSheetFileName

‍The name of the XML file to process

OutputFileName

‍Optional name of a style sheet which is applied after the pre-processor (can be empty string)> This has no effect if the OutputFileName is an empty string

XMLValidation

‍Optional name of an output file into which the processed data is written (can be empty string)> Optional bit mask formed from EXMLValidation enumeration indicating which tests should be performed on the XML file

◆ PreprocessXMLFromZIPFile()

virtual void PreprocessXMLFromZIPFile ( const GenICam::gcstring XMLFileName,
const GenICam::gcstring StyleSheetFileName,
const GenICam::gcstring OutputFileName,
const uint32_t  XMLValidation = xvDefault 
)
pure virtual

Loads a Zipped XML, checks it for correctness, pre-processes it, caches it, and optionally applies a style sheet, and optionally writes it to a file.

Parameters
StyleSheetFileName

‍The name of the XML file to process

OutputFileName

‍Optional name of a style sheet which is applied after the pre-processor (can be empty string)> This has no effect if the OutputFileName is an empty string

XMLValidation

‍Optional name of an output file into which the processed data is written (can be empty string)> Optional bit mask formed from EXMLValidation enumeration indicating which tests should be performed on the XML file

Variable Documentation

◆ INodeMapDyn

Interface to access the node map.