Functions | |
virtual void | Write (const void *pBuffer, int64_t Address, int64_t Length)=0 |
Writes a chunk of bytes to the port. More... | |
Variables | |
interface SPINNAKER_API_ABSTRACT | IPort |
Interface for ports. More... | |
interface SPINNAKER_API_ABSTRACT int64_t | Address |
interface SPINNAKER_API_ABSTRACT int64_t int64_t | Length = 0 |
|
pure virtual |
Writes a chunk of bytes to the port.
interface SPINNAKER_API_ABSTRACT int64_t Address |
Interface for ports.
interface SPINNAKER_API_ABSTRACT int64_t Length = 0 |
Contact Support | Spinnaker® SDK Programmer's Guide and API Reference | Thu Dec 16 2021 © FLIR Integrated Imaging Solutions Inc. All rights reserved. |