Functions | |
| virtual GenICam::gcstring | ToString (bool Verify=false, bool IgnoreCache=false)=0 |
| Get content of the node as string. | |
| virtual void | FromString (const GenICam::gcstring &ValueStr, bool Verify=true)=0 |
| Set content of the node as string. | |
| virtual bool | IsValueCacheValid () const =0 |
| Checks if the value comes from cache or is requested from another node. | |
Variables | |
| interface SPINNAKER_API_ABSTRACT | IValue |
| Interface for value properties. | |
|
pure virtual |
Set content of the node as string.
| ValueStr | The value to set |
| Verify | Enables AccessMode and Range verification (default = true) |
|
pure virtual |
Checks if the value comes from cache or is requested from another node.
|
pure virtual |
Get content of the node as string.
| Verify | Enables Range verification (default = false). The AccessMode is always checked |
| IgnoreCache | If true the value is read ignoring any caches (default = false) |
| interface SPINNAKER_API_ABSTRACT IValue |
Interface for value properties.