Spinnaker SDK C++
4.2.0.83
 
 

 
Loading...
Searching...
No Matches
StereoAcquisitionParams Struct Reference

#include <StereoAcquisition_QuickSpin.h>

Public Attributes

unsigned int numImageSets = 3
 
bool doEnableRawSensor1Transmit = false
 
bool doEnableRawSensor2Transmit = false
 
bool doEnableRectSensor1Transmit = false
 
bool doEnableRectSensor2Transmit = false
 
bool doEnableDisparityTransmit = false
 
bool doEnablePointCloudOutput = false
 
bool doEnableSpeckleFilter = false
 

Friends

std::ostream & operator<< (std::ostream &os, const StereoAcquisitionParams &stereoAcquisitionParams)
 
std::ostream & operator<< (std::ostream &os, const StereoAcquisitionParams &stereoAcquisitionParams)
 

Detailed Description

Friends And Related Symbol Documentation

◆ operator<< [1/2]

std::ostream & operator<< ( std::ostream &  os,
const StereoAcquisitionParams stereoAcquisitionParams 
)
friend

◆ operator<< [2/2]

std::ostream & operator<< ( std::ostream &  os,
const StereoAcquisitionParams stereoAcquisitionParams 
)
friend

Member Data Documentation

◆ doEnableDisparityTransmit

bool doEnableDisparityTransmit = false

◆ doEnablePointCloudOutput

bool doEnablePointCloudOutput = false

◆ doEnableRawSensor1Transmit

bool doEnableRawSensor1Transmit = false

◆ doEnableRawSensor2Transmit

bool doEnableRawSensor2Transmit = false

◆ doEnableRectSensor1Transmit

bool doEnableRectSensor1Transmit = false

◆ doEnableRectSensor2Transmit

bool doEnableRectSensor2Transmit = false

◆ doEnableSpeckleFilter

bool doEnableSpeckleFilter = false

◆ numImageSets

unsigned int numImageSets = 3

The documentation for this struct was generated from the following files: