Functions | |
| virtual void | Get (uint8_t *pBuffer, int64_t Length, bool Verify=false, bool IgnoreCache=false)=0 |
| Fills a buffer with the register's contents. | |
| virtual int64_t | GetLength ()=0 |
| Retrieves the Length of the register [Bytes]. | |
| virtual int64_t | GetAddress ()=0 |
| Retrieves the Address of the register. | |
Variables | |
| interface SPINNAKER_API_ABSTRACT | IRegister |
| Interface for registers. | |
|
pure virtual |
Fills a buffer with the register's contents.
| pBuffer | The buffer receiving the data to read |
| Length | The number of bytes to retrieve |
| Verify | Enables Range verification (default = false). The AccessMode is always checked |
| IgnoreCache | If true the value is read ignoring any caches (default = false) |
|
pure virtual |
Retrieves the Address of the register.
|
pure virtual |
Retrieves the Length of the register [Bytes].
| interface SPINNAKER_API_ABSTRACT IRegister |
Interface for registers.