ChunkData¶
ChunkData.cpp shows how to get chunk data on an image, either from the nodemap or from the image itself. It relies on information provided in the Enumeration, Acquisition, and NodeMapInfo examples.
//=============================================================================
// Copyright (c) 2026 FLIR Integrated Imaging Solutions, Inc. All Rights Reserved.
//
// This software is the confidential and proprietary information of FLIR
// Integrated Imaging Solutions, Inc. ("Confidential Information"). You
// shall not disclose such Confidential Information and shall use it only in
// accordance with the terms of the license agreement you entered into
// with FLIR Integrated Imaging Solutions, Inc. (FLIR).
//
// FLIR MAKES NO REPRESENTATIONS OR WARRANTIES ABOUT THE SUITABILITY OF THE
// SOFTWARE, EITHER EXPRESSED OR IMPLIED, INCLUDING, BUT NOT LIMITED TO, THE
// IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR
// PURPOSE, OR NON-INFRINGEMENT. FLIR SHALL NOT BE LIABLE FOR ANY DAMAGES
// SUFFERED BY LICENSEE AS A RESULT OF USING, MODIFYING OR DISTRIBUTING
// THIS SOFTWARE OR ITS DERIVATIVES.
//=============================================================================
/**
* @example ChunkData.cpp
*
* @brief ChunkData.cpp shows how to get chunk data on an image, either from
* the nodemap or from the image itself. It relies on information provided in
* the Enumeration, Acquisition, and NodeMapInfo examples.
*
* It can also be helpful to familiarize yourself with the ImageFormatControl
* and Exposure examples. As they are somewhat shorter and simpler, either
* provides a strong introduction to camera customization.
*
* Chunk data provides information on various traits of an image. This includes
* identifiers such as frame ID, properties such as black level, and more. This
* information can be acquired from either the nodemap or the image itself.
*
* It may be preferable to grab chunk data from each individual image, as it
* can be hard to verify whether data is coming from the correct image when
* using the nodemap. This is because chunk data retrieved from the nodemap is
* only valid for the current image; when GetNextImage() is called, chunk data
* will be updated to that of the new current image.
*
* Please leave us feedback at: https://www.surveymonkey.com/r/TDYMVAPI
* More source code examples at: https://github.com/Teledyne-MV/Spinnaker-Examples
* Need help? Check out our forum at: https://teledynevisionsolutions.zendesk.com/hc/en-us/community/topics
*/
#include "Spinnaker.h"
#include "SpinGenApi/SpinnakerGenApi.h"
#include <iostream>
#include <sstream>
#include <cstdint>
#include <iomanip>
#include <cctype>
using namespace Spinnaker;
using namespace Spinnaker::GenApi;
using namespace Spinnaker::GenICam;
using namespace std;
// Use the following enum and global constant to select whether chunk data is
// displayed from the image or the nodemap.
enum chunkDataType
{
IMAGE,
NODEMAP
};
const chunkDataType chosenChunkData = IMAGE;
// This function configures the camera to add chunk data to each image. It does
// this by enabling each type of chunk data after enabling chunk data mode.
// When chunk data mode is turned on, the data is made available in both the nodemap
// and each image.
int ConfigureChunkData(INodeMap& nodeMap)
{
int result = 0;
cout << endl << endl << "*** CONFIGURING CHUNK DATA ***" << endl << endl;
try
{
//
// Activate chunk mode
//
// *** NOTES ***
// Once enabled, chunk data will be available at the end of the payload
// of every image captured until it is disabled. Chunk data can also be
// retrieved from the nodemap.
//
CBooleanPtr ptrChunkModeActive = nodeMap.GetNode("ChunkModeActive");
if (!IsWritable(ptrChunkModeActive))
{
cout << "Unable to activate chunk mode. Aborting..." << endl << endl;
return -1;
}
ptrChunkModeActive->SetValue(true);
cout << "Chunk mode activated..." << endl;
//
// Enable all types of chunk data
//
// *** NOTES ***
// Enabling chunk data requires working with nodes: "ChunkSelector"
// is an enumeration selector node and "ChunkEnable" is a boolean. It
// requires retrieving the selector node (which is of enumeration node
// type), selecting the entry of the chunk data to be enabled, retrieving
// the corresponding boolean, and setting it to true.
//
// In this example, all chunk data is enabled, so these steps are
// performed in a loop. Once this is complete, chunk mode still needs to
// be activated.
//
NodeList_t entries;
// Retrieve the selector node
CEnumerationPtr ptrChunkSelector = nodeMap.GetNode("ChunkSelector");
if (!IsReadable(ptrChunkSelector))
{
cout << "Unable to retrieve chunk selector. Aborting..." << endl << endl;
return -1;
}
// Retrieve entries
ptrChunkSelector->GetEntries(entries);
cout << "Enabling entries..." << endl;
for (size_t i = 0; i < entries.size(); i++)
{
// Select entry to be enabled
CEnumEntryPtr ptrChunkSelectorEntry = entries.at(i);
// Go to next node if problem occurs
if (!IsReadable(ptrChunkSelectorEntry))
{
continue;
}
ptrChunkSelector->SetIntValue(ptrChunkSelectorEntry->GetValue());
cout << "\t" << ptrChunkSelectorEntry->GetSymbolic() << ": ";
// Retrieve corresponding boolean
CBooleanPtr ptrChunkEnable = nodeMap.GetNode("ChunkEnable");
// Enable the boolean, thus enabling the corresponding chunk data
if (!IsAvailable(ptrChunkEnable))
{
cout << "not available" << endl;
result = -1;
}
else if (ptrChunkEnable->GetValue())
{
cout << "enabled" << endl;
}
else if (IsWritable(ptrChunkEnable))
{
ptrChunkEnable->SetValue(true);
cout << "enabled" << endl;
}
else
{
cout << "not writable" << endl;
result = -1;
}
}
}
catch (Spinnaker::Exception& e)
{
cout << "Error: " << e.what() << endl;
result = -1;
}
return result;
}
void printBytesAsHex(uint8_t* array, int64_t length)
{
cout << "\t As Hex: ";
for (int64_t i = 0; i < length - 1; ++i)
{
if (i != 0 && i % 8 == 0)
{
cout << endl << "\t ";
}
cout << "0x" << hex << setw(2) << setfill('0') << static_cast<int>(array[i]) << " ";
}
cout << endl;
}
// This function displays a select amount of chunk data from the image. Unlike
// accessing chunk data via the nodemap, there is no way to loop through all
// available data.
int DisplayChunkData(ImagePtr pImage)
{
int result = 0;
cout << "Printing chunk data from image..." << endl;
try
{
//
// Retrieve chunk data from image
//
// *** NOTES ***
// When retrieving chunk data from an image, the data is stored in a
// a ChunkData object and accessed with getter functions.
//
ChunkData chunkData = pImage->GetChunkData();
//
// Retrieve exposure time; exposure time recorded in microseconds
//
// *** NOTES ***
// Floating point numbers are returned as a float64_t. This can safely
// and easily be statically cast to a double.
//
double exposureTime = static_cast<double>(chunkData.GetExposureTime());
std::cout << "\tExposure time: " << exposureTime << endl;
//
// Retrieve frame ID
//
// *** NOTES ***
// Integers are returned as an int64_t. As this is the typical integer
// data type used in the Spinnaker SDK, there is no need to cast it.
//
int64_t frameID = chunkData.GetFrameID();
cout << "\tFrame ID: " << frameID << endl;
// Retrieve gain; gain recorded in decibels
double gain = chunkData.GetGain();
cout << "\tGain: " << gain << endl;
// Retrieve height; height recorded in pixels
int64_t height = chunkData.GetHeight();
cout << "\tHeight: " << height << endl;
// Retrieve offset X; offset X recorded in pixels
int64_t offsetX = chunkData.GetOffsetX();
cout << "\tOffset X: " << offsetX << endl;
// Retrieve offset Y; offset Y recorded in pixels
int64_t offsetY = chunkData.GetOffsetY();
cout << "\tOffset Y: " << offsetY << endl;
// Retrieve sequencer set active
int64_t sequencerSetActive = chunkData.GetSequencerSetActive();
cout << "\tSequencer set active: " << sequencerSetActive << endl;
// Retrieve timestamp
uint64_t timestamp = chunkData.GetTimestamp();
cout << "\tTimestamp: " << timestamp << endl;
// Retrieve width; width recorded in pixels
int64_t width = chunkData.GetWidth();
cout << "\tWidth: " << width << endl;
// Retrieve Serial Data:
int64_t serialDataLength = chunkData.GetSerialDataLength();
if (serialDataLength > 0)
{
cout << "\tSerial Data (" << serialDataLength << ") Bytes):" << endl;
if (chunkData.GetSerialReceiveOverflow())
{
cout << "\t Warning: Device serial data buffer overflow" << endl;
}
uint8_t* pSerialData = chunkData.GetSerialData();
printBytesAsHex(pSerialData, chunkData.GetSerialDataLength());
}
else
{
cout << "\tSerialData: N/A" << endl;
}
}
catch (Spinnaker::Exception& e)
{
cout << "Error: " << e.what() << endl;
result = -1;
}
return result;
}
// This function displays all available chunk data by looping through the chunk
// data category node on the nodemap.
int DisplayChunkData(INodeMap& nodeMap)
{
int result = 0;
cout << "Printing chunk data from nodemap..." << endl;
try
{
//
// Retrieve chunk data information nodes
//
// *** NOTES ***
// As well as being written into the payload of the image, chunk data is
// accessible on the GenICam nodemap. Insofar as chunk data is enabled,
// it is available from both sources.
//
CCategoryPtr ptrChunkDataControl = nodeMap.GetNode("ChunkDataControl");
if (!IsReadable(ptrChunkDataControl))
{
cout << "Unable to retrieve chunk data control. Aborting..." << endl << endl;
return -1;
}
FeatureList_t features;
ptrChunkDataControl->GetFeatures(features);
// Iterate through children
FeatureList_t::const_iterator it;
for (it = features.begin(); it != features.end(); ++it)
{
CNodePtr pFeature = (CNodePtr)*it;
if (!IsReadable(pFeature))
{
cout << "node not readable" << endl;
result = result | -1;
continue;
}
//
// Print boolean node type value
//
// *** NOTES ***
// Boolean information is manipulated to output the more-easily
// identifiable 'true' and 'false' as opposed to '1' and '0'.
//
cout << "\t" << pFeature->GetDisplayName() << ": ";
if (pFeature->GetPrincipalInterfaceType() == intfIBoolean)
{
CBooleanPtr pBool = (CBooleanPtr)pFeature;
bool value = pBool->GetValue();
cout << (value ? "true" : "false") << endl;
}
//
// Print non-boolean node type value
//
// *** NOTES ***
// All nodes can be cast as value nodes and have their information
// retrieved as a string using the ToString() method. This is much
// easier than dealing with each node type individually.
//
else
{
CValuePtr pValue = (CValuePtr)pFeature;
cout << pValue->ToString() << endl;
}
}
}
catch (Spinnaker::Exception& e)
{
cout << "Error: " << e.what() << endl;
result = -1;
}
return result;
}
// This function prints the device information of the camera from the transport
// layer; please see NodeMapInfo example for more in-depth comments on printing
// device information from the nodemap.
int PrintDeviceInfo(INodeMap& nodeMap)
{
int result = 0;
cout << endl << "*** DEVICE INFORMATION ***" << endl << endl;
try
{
FeatureList_t features;
CCategoryPtr category = nodeMap.GetNode("DeviceInformation");
if (IsReadable(category))
{
category->GetFeatures(features);
FeatureList_t::const_iterator it;
for (it = features.begin(); it != features.end(); ++it)
{
try
{
CNodePtr pfeatureNode = *it;
cout << pfeatureNode->GetName() << " : ";
CValuePtr pValue = (CValuePtr)pfeatureNode;
cout << (IsReadable(pValue) ? pValue->ToString() : gcstring("Node not readable"));
cout << endl;
}
catch (Spinnaker::Exception)
{
cout << "Node not readable" << endl;
}
}
}
else
{
cout << "Device control information not readable." << endl;
}
}
catch (Spinnaker::Exception& e)
{
cout << "Error: " << e.what() << endl;
result = -1;
}
return result;
}
// This function acquires and saves 10 images from a device; please see
// Acquisition example for more in-depth comments on acquiring images.
int AcquireImages(CameraPtr pCam, INodeMap& nodeMap, INodeMap& nodeMapTLDevice)
{
int result = 0;
cout << endl << endl << "*** IMAGE ACQUISITION ***" << endl << endl;
try
{
// Set acquisition mode to continuous
CEnumerationPtr ptrAcquisitionMode = nodeMap.GetNode("AcquisitionMode");
if (!IsReadable(ptrAcquisitionMode) || !IsWritable(ptrAcquisitionMode))
{
cout << "Unable to set acquisition mode to continuous (node retrieval). Aborting..." << endl << endl;
return -1;
}
CEnumEntryPtr ptrAcquisitionModeContinuous = ptrAcquisitionMode->GetEntryByName("Continuous");
if (!IsReadable(ptrAcquisitionModeContinuous))
{
cout << "Unable to set acquisition mode to continuous (entry 'continuous' retrieval). Aborting..." << endl
<< endl;
return -1;
}
int64_t acquisitionModeContinuous = ptrAcquisitionModeContinuous->GetValue();
ptrAcquisitionMode->SetIntValue(acquisitionModeContinuous);
cout << "Acquisition mode set to continuous..." << endl;
// Begin acquiring images
pCam->BeginAcquisition();
cout << "Acquiring images..." << endl;
// Retrieve device serial number for filename
gcstring deviceSerialNumber("");
CStringPtr ptrStringSerial = nodeMapTLDevice.GetNode("DeviceSerialNumber");
if (IsReadable(ptrStringSerial))
{
deviceSerialNumber = ptrStringSerial->GetValue();
cout << "Device serial number retrieved as " << deviceSerialNumber << "..." << endl;
}
cout << endl;
// Retrieve, convert, and save images
const unsigned int k_numImages = 10;
//
// Create ImageProcessor instance for post processing images
//
ImageProcessor processor;
//
// Set default image processor color processing method
//
// *** NOTES ***
// By default, if no specific color processing algorithm is set, the image
// processor will default to NEAREST_NEIGHBOR method.
//
processor.SetColorProcessing(SPINNAKER_COLOR_PROCESSING_ALGORITHM_HQ_LINEAR);
for (unsigned int imageCnt = 0; imageCnt < k_numImages; imageCnt++)
{
try
{
// Retrieve next received image and ensure image completion
ImagePtr pResultImage = pCam->GetNextImage(1000);
if (pResultImage->IsIncomplete())
{
cout << "Image incomplete with image status " << pResultImage->GetImageStatus() << "..." << endl
<< endl;
}
else
{
// Print image information
cout << "Grabbed image " << imageCnt << ", width = " << pResultImage->GetWidth()
<< ", height = " << pResultImage->GetHeight() << endl;
// Convert image to mono 8
ImagePtr convertedImage = processor.Convert(pResultImage, PixelFormat_Mono8);
// Create a unique filename
ostringstream filename;
filename << "ChunkData-";
if (deviceSerialNumber != "")
{
filename << deviceSerialNumber.c_str() << "-";
}
filename << imageCnt << ".jpg";
// Save image
convertedImage->Save(filename.str().c_str());
cout << "Image saved at " << filename.str() << endl;
// Display chunk data
if (chosenChunkData == IMAGE)
{
result = DisplayChunkData(pResultImage);
}
else if (chosenChunkData == NODEMAP)
{
result = DisplayChunkData(nodeMap);
}
}
// Release image
pResultImage->Release();
cout << endl;
}
catch (Spinnaker::Exception& e)
{
cout << "Error: " << e.what() << endl;
result = -1;
}
}
// End acquisition
pCam->EndAcquisition();
}
catch (Spinnaker::Exception& e)
{
cout << "Error: " << e.what() << endl;
result = -1;
}
return result;
}
// This function disables each type of chunk data before disabling chunk data mode.
int DisableChunkData(INodeMap& nodeMap)
{
int result = 0;
try
{
NodeList_t entries;
// Retrieve the selector node
CEnumerationPtr ptrChunkSelector = nodeMap.GetNode("ChunkSelector");
if (!IsReadable(ptrChunkSelector))
{
cout << "Unable to retrieve chunk selector. Aborting..." << endl << endl;
return -1;
}
// Retrieve entries
ptrChunkSelector->GetEntries(entries);
cout << "Disabling entries..." << endl;
for (size_t i = 0; i < entries.size(); i++)
{
// Select entry to be disabled
CEnumEntryPtr ptrChunkSelectorEntry = entries.at(i);
// Go to next node if problem occurs
if (!IsReadable(ptrChunkSelectorEntry))
{
continue;
}
ptrChunkSelector->SetIntValue(ptrChunkSelectorEntry->GetValue());
cout << "\t" << ptrChunkSelectorEntry->GetSymbolic() << ": ";
// Retrieve corresponding boolean
CBooleanPtr ptrChunkEnable = nodeMap.GetNode("ChunkEnable");
// Disable the boolean, thus disabling the corresponding chunk data
if (!IsAvailable(ptrChunkEnable))
{
cout << "not available" << endl;
result = -1;
}
else if (!ptrChunkEnable->GetValue())
{
cout << "disabled" << endl;
}
else if (IsWritable(ptrChunkEnable))
{
ptrChunkEnable->SetValue(false);
cout << "disabled" << endl;
}
else
{
cout << "not writable" << endl;
}
}
cout << endl;
// Deactivate ChunkMode
CBooleanPtr ptrChunkModeActive = nodeMap.GetNode("ChunkModeActive");
if (!IsWritable(ptrChunkModeActive))
{
cout << "Unable to deactivate chunk mode. Aborting..." << endl << endl;
return -1;
}
ptrChunkModeActive->SetValue(false);
cout << "Chunk mode deactivated..." << endl;
}
catch (Spinnaker::Exception& e)
{
cout << "Error: " << e.what() << endl;
result = -1;
}
return result;
}
// This function acts as the body of the example; please see NodeMapInfo example
// for more in-depth comments on setting up cameras.
int RunSingleCamera(CameraPtr pCam)
{
int result = 0;
int err = 0;
try
{
// Retrieve TL device nodemap and print device information
INodeMap& nodeMapTLDevice = pCam->GetTLDeviceNodeMap();
result = PrintDeviceInfo(nodeMapTLDevice);
// This example is not compatible with BX (Bumblebee) stereo cameras, see StereoAcquisiton for this camera.
CStringPtr ptrDeviceModelName = nodeMapTLDevice.GetNode("DeviceModelName");
if (IsReadable(ptrDeviceModelName))
{
string deviceModelName = ptrDeviceModelName->GetValue().c_str();
if (deviceModelName.find("BX") != std::string::npos)
{
cout << "This example is not compatible with BX (Bumblebee) stereo cameras. Please see "
"StereoAcquisition Example for ChunkData usage with this camera."
<< endl;
return -1;
}
}
// Initialize camera
pCam->Init();
// Retrieve GenICam nodemap
INodeMap& nodeMap = pCam->GetNodeMap();
// Configure chunk data
err = ConfigureChunkData(nodeMap);
if (err < 0)
{
return err;
}
// Acquire images and display chunk data
result = result | AcquireImages(pCam, nodeMap, nodeMapTLDevice);
// Disable chunk data
err = DisableChunkData(nodeMap);
if (err < 0)
{
return err;
}
// Deinitialize camera
pCam->DeInit();
}
catch (Spinnaker::Exception& e)
{
cout << "Error: " << e.what() << endl;
result = -1;
}
return result;
}
// Example entry point; please see Enumeration example for more in-depth
// comments on preparing and cleaning up the system.
int main(int /*argc*/, char** /*argv*/)
{
// Since this application saves images in the current folder
// we must ensure that we have permission to write to this folder.
// If we do not have permission, fail right away.
FILE* tempFile = fopen("test.txt", "w+");
if (tempFile == nullptr)
{
cout << "Failed to create file in current folder. Please check "
"permissions."
<< endl;
cout << "Press Enter to exit..." << endl;
getchar();
return -1;
}
fclose(tempFile);
remove("test.txt");
int result = 0;
// Print application build information
cout << "Application build date: " << __DATE__ << " " << __TIME__ << endl << endl;
// Retrieve singleton reference to system object
SystemPtr system = System::GetInstance();
// Print out current library version
const LibraryVersion spinnakerLibraryVersion = system->GetLibraryVersion();
cout << "Spinnaker library version: " << spinnakerLibraryVersion.major << "." << spinnakerLibraryVersion.minor
<< "." << spinnakerLibraryVersion.type << "." << spinnakerLibraryVersion.build << endl
<< endl;
// Retrieve list of cameras from the system
CameraList camList = system->GetCameras();
unsigned int numCameras = camList.GetSize();
cout << "Number of cameras detected: " << numCameras << endl << endl;
// Finish if there are no cameras
if (numCameras == 0)
{
// Clear camera list before releasing system
camList.Clear();
// Release system
system->ReleaseInstance();
cout << "Not enough cameras!" << endl;
cout << "Done! Press Enter to exit..." << endl;
getchar();
return -1;
}
// Run example on each camera
for (unsigned int i = 0; i < numCameras; i++)
{
cout << endl << "Running example for camera " << i << "..." << endl;
result = result | RunSingleCamera(camList.GetByIndex(i));
cout << "Camera " << i << " example complete..." << endl << endl;
}
// Clear camera list before releasing system
camList.Clear();
// Release system
system->ReleaseInstance();
cout << endl << "Done! Press Enter to exit..." << endl;
getchar();
return result;
}