Trigger¶
Trigger.cpp shows how to trigger the camera. It relies on information provided in the Enumeration, Acquisition, and NodeMapInfo examples.
//=============================================================================
// Copyright (c) 2026 FLIR Integrated Imaging Solutions, Inc. All Rights Reserved.
//
// This software is the confidential and proprietary information of FLIR
// Integrated Imaging Solutions, Inc. ("Confidential Information"). You
// shall not disclose such Confidential Information and shall use it only in
// accordance with the terms of the license agreement you entered into
// with FLIR Integrated Imaging Solutions, Inc. (FLIR).
//
// FLIR MAKES NO REPRESENTATIONS OR WARRANTIES ABOUT THE SUITABILITY OF THE
// SOFTWARE, EITHER EXPRESSED OR IMPLIED, INCLUDING, BUT NOT LIMITED TO, THE
// IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR
// PURPOSE, OR NON-INFRINGEMENT. FLIR SHALL NOT BE LIABLE FOR ANY DAMAGES
// SUFFERED BY LICENSEE AS A RESULT OF USING, MODIFYING OR DISTRIBUTING
// THIS SOFTWARE OR ITS DERIVATIVES.
//=============================================================================
/**
* @example Trigger.cpp
*
* @brief Trigger.cpp shows how to trigger the camera. It relies on information
* provided in the Enumeration, Acquisition, and NodeMapInfo examples.
*
* It can also be helpful to familiarize yourself with the ImageFormatControl
* and Exposure examples. As they are somewhat shorter and simpler, either
* provides a strong introduction to camera customization.
*
* This example shows the process of configuring, using, and cleaning up a
* camera for use with both a software and a hardware trigger.
*
* Please leave us feedback at: https://www.surveymonkey.com/r/TDYMVAPI
* More source code examples at: https://github.com/Teledyne-MV/Spinnaker-Examples
* Need help? Check out our forum at: https://teledynevisionsolutions.zendesk.com/hc/en-us/community/topics
*/
#include "Spinnaker.h"
#include "SpinGenApi/SpinnakerGenApi.h"
#include <iostream>
#include <sstream>
using namespace Spinnaker;
using namespace Spinnaker::GenApi;
using namespace Spinnaker::GenICam;
using namespace std;
// Use the following enum and global constant to select whether a software or
// hardware trigger is used.
enum triggerType
{
SOFTWARE,
HARDWARE
};
const triggerType chosenTrigger = SOFTWARE;
// This function configures the camera to use a trigger. First, trigger mode is
// set to off in order to select the trigger source. Once the trigger source
// has been selected, trigger mode is then enabled, which has the camera
// capture only a single image upon the execution of the chosen trigger.
int ConfigureTrigger(INodeMap& nodeMap)
{
int result = 0;
cout << endl << endl << "*** CONFIGURING TRIGGER ***" << endl << endl;
cout << "Note that if the application / user software triggers faster than frame time, the trigger may be dropped "
"/ skipped by the camera."
<< endl
<< "If several frames are needed per trigger, a more reliable alternative for such case, is to use the "
"multi-frame mode."
<< endl
<< endl;
if (chosenTrigger == SOFTWARE)
{
cout << "Software trigger chosen..." << endl;
}
else if (chosenTrigger == HARDWARE)
{
cout << "Hardware trigger chosen..." << endl;
}
try
{
//
// Ensure trigger mode off
//
// *** NOTES ***
// The trigger must be disabled in order to configure whether the source
// is software or hardware.
//
CEnumerationPtr ptrTriggerMode = nodeMap.GetNode("TriggerMode");
if (!IsReadable(ptrTriggerMode))
{
cout << "Unable to disable trigger mode (node retrieval). Aborting..." << endl;
return -1;
}
CEnumEntryPtr ptrTriggerModeOff = ptrTriggerMode->GetEntryByName("Off");
if (!IsReadable(ptrTriggerModeOff))
{
cout << "Unable to disable trigger mode (enum entry retrieval). Aborting..." << endl;
return -1;
}
ptrTriggerMode->SetIntValue(ptrTriggerModeOff->GetValue());
cout << "Trigger mode disabled..." << endl;
//
// Set TriggerSelector to FrameStart
//
// *** NOTES ***
// For this example, the trigger selector should be set to frame start.
// This is the default for most cameras.
//
CEnumerationPtr ptrTriggerSelector = nodeMap.GetNode("TriggerSelector");
if (!IsReadable(ptrTriggerSelector) || !IsWritable(ptrTriggerSelector))
{
cout << "Unable to get or set trigger selector (node retrieval). Aborting..." << endl;
return -1;
}
CEnumEntryPtr ptrTriggerSelectorFrameStart = ptrTriggerSelector->GetEntryByName("FrameStart");
if (!IsReadable(ptrTriggerSelectorFrameStart))
{
cout << "Unable to get trigger selector (enum entry retrieval). Aborting..." << endl;
return -1;
}
ptrTriggerSelector->SetIntValue(ptrTriggerSelectorFrameStart->GetValue());
cout << "Trigger selector set to frame start..." << endl;
//
// Select trigger source
//
// *** NOTES ***
// The trigger source must be set to hardware or software while trigger
// mode is off.
//
CEnumerationPtr ptrTriggerSource = nodeMap.GetNode("TriggerSource");
if (!IsReadable(ptrTriggerSource) || !IsWritable(ptrTriggerSource))
{
cout << "Unable to get or set trigger mode (node retrieval). Aborting..." << endl;
return -1;
}
if (chosenTrigger == SOFTWARE)
{
// Set trigger mode to software
CEnumEntryPtr ptrTriggerSourceSoftware = ptrTriggerSource->GetEntryByName("Software");
if (!IsReadable(ptrTriggerSourceSoftware))
{
cout << "Unable to set trigger mode (enum entry retrieval). Aborting..." << endl;
return -1;
}
ptrTriggerSource->SetIntValue(ptrTriggerSourceSoftware->GetValue());
cout << "Trigger source set to software..." << endl;
}
else if (chosenTrigger == HARDWARE)
{
// Set trigger mode to hardware ('Line0')
CEnumEntryPtr ptrTriggerSourceHardware = ptrTriggerSource->GetEntryByName("Line0");
if (!IsReadable(ptrTriggerSourceHardware))
{
cout << "Unable to set trigger mode (enum entry retrieval). Aborting..." << endl;
return -1;
}
ptrTriggerSource->SetIntValue(ptrTriggerSourceHardware->GetValue());
cout << "Trigger source set to hardware..." << endl;
}
//
// Turn trigger mode on
//
// *** LATER ***
// Once the appropriate trigger source has been set, turn trigger mode
// on in order to retrieve images using the trigger.
//
CEnumEntryPtr ptrTriggerModeOn = ptrTriggerMode->GetEntryByName("On");
if (!IsReadable(ptrTriggerModeOn))
{
cout << "Unable to enable trigger mode (enum entry retrieval). Aborting..." << endl;
return -1;
}
ptrTriggerMode->SetIntValue(ptrTriggerModeOn->GetValue());
// NOTE: Blackfly and Flea3 GEV cameras need 1 second delay after trigger mode is turned on
cout << "Trigger mode turned back on..." << endl << endl;
}
catch (Spinnaker::Exception& e)
{
cout << "Error: " << e.what() << endl;
result = -1;
}
return result;
}
// This function retrieves a single image using the trigger. In this example,
// only a single image is captured and made available for acquisition - as such,
// attempting to acquire two images for a single trigger execution would cause
// the example to hang. This is different from other examples, whereby a
// constant stream of images are being captured and made available for image
// acquisition.
int GrabNextImageByTrigger(INodeMap& nodeMap, CameraPtr pCam)
{
int result = 0;
try
{
//
// Use trigger to capture image
//
// *** NOTES ***
// The software trigger only feigns being executed by the Enter key;
// what might not be immediately apparent is that there is not a
// continuous stream of images being captured; in other examples that
// acquire images, the camera captures a continuous stream of images.
// When an image is retrieved, it is plucked from the stream.
//
if (chosenTrigger == SOFTWARE)
{
// Get user input
cout << "Press the Enter key to initiate software trigger." << endl;
getchar();
// Execute software trigger
CCommandPtr ptrSoftwareTriggerCommand = nodeMap.GetNode("TriggerSoftware");
if (!IsWritable(ptrSoftwareTriggerCommand))
{
cout << "Unable to execute trigger. Aborting..." << endl;
return -1;
}
ptrSoftwareTriggerCommand->Execute();
// NOTE: Blackfly and Flea3 GEV cameras need 2 second delay after software trigger
}
else if (chosenTrigger == HARDWARE)
{
// Execute hardware trigger
cout << "Use the hardware to trigger image acquisition." << endl;
}
}
catch (Spinnaker::Exception& e)
{
cout << "Error: " << e.what() << endl;
result = -1;
}
return result;
}
// This function returns the camera to a normal state by turning off trigger
// mode.
int ResetTrigger(INodeMap& nodeMap)
{
int result = 0;
try
{
//
// Turn trigger mode back off
//
// *** NOTES ***
// Once all images have been captured, turn trigger mode back off to
// restore the camera to a clean state.
//
CEnumerationPtr ptrTriggerMode = nodeMap.GetNode("TriggerMode");
if (!IsReadable(ptrTriggerMode))
{
cout << "Unable to disable trigger mode (node retrieval). Non-fatal error..." << endl;
return -1;
}
CEnumEntryPtr ptrTriggerModeOff = ptrTriggerMode->GetEntryByName("Off");
if (!IsReadable(ptrTriggerModeOff))
{
cout << "Unable to disable trigger mode (enum entry retrieval). Non-fatal error..." << endl;
return -1;
}
ptrTriggerMode->SetIntValue(ptrTriggerModeOff->GetValue());
cout << "Trigger mode disabled..." << endl << endl;
}
catch (Spinnaker::Exception& e)
{
cout << "Error: " << e.what() << endl;
result = -1;
}
return result;
}
// This function prints the device information of the camera from the transport
// layer; please see NodeMapInfo example for more in-depth comments on printing
// device information from the nodemap.
int PrintDeviceInfo(INodeMap& nodeMap)
{
int result = 0;
cout << endl << "*** DEVICE INFORMATION ***" << endl << endl;
try
{
FeatureList_t features;
CCategoryPtr category = nodeMap.GetNode("DeviceInformation");
if (IsReadable(category))
{
category->GetFeatures(features);
FeatureList_t::const_iterator it;
for (it = features.begin(); it != features.end(); ++it)
{
try
{
CNodePtr pfeatureNode = *it;
cout << pfeatureNode->GetName() << " : ";
CValuePtr pValue = (CValuePtr)pfeatureNode;
cout << (IsReadable(pValue) ? pValue->ToString() : gcstring("Node not readable"));
cout << endl;
}
catch (Spinnaker::Exception)
{
cout << "Node not readable" << endl;
}
}
}
else
{
cout << "Device control information not readable." << endl;
}
}
catch (Spinnaker::Exception& e)
{
cout << "Error: " << e.what() << endl;
result = -1;
}
return result;
}
// This function acquires and saves 10 images from a device; please see
// Acquisition example for more in-depth comments on acquiring images.
int AcquireImages(CameraPtr pCam, INodeMap& nodeMap, INodeMap& nodeMapTLDevice)
{
int result = 0;
cout << endl << "*** IMAGE ACQUISITION ***" << endl << endl;
try
{
// Set acquisition mode to continuous
CEnumerationPtr ptrAcquisitionMode = nodeMap.GetNode("AcquisitionMode");
if (!IsReadable(ptrAcquisitionMode) || !IsWritable(ptrAcquisitionMode))
{
cout << "Unable to get or set acquisition mode to continuous (node retrieval). Aborting..." << endl << endl;
return -1;
}
CEnumEntryPtr ptrAcquisitionModeContinuous = ptrAcquisitionMode->GetEntryByName("Continuous");
if (!IsReadable(ptrAcquisitionModeContinuous))
{
cout << "Unable to get acquisition mode to continuous (entry 'continuous' retrieval). Aborting..." << endl
<< endl;
return -1;
}
int64_t acquisitionModeContinuous = ptrAcquisitionModeContinuous->GetValue();
ptrAcquisitionMode->SetIntValue(acquisitionModeContinuous);
cout << "Acquisition mode set to continuous..." << endl;
// Begin acquiring images
pCam->BeginAcquisition();
cout << "Acquiring images..." << endl;
// Retrieve device serial number for filename
gcstring deviceSerialNumber("");
CStringPtr ptrStringSerial = nodeMapTLDevice.GetNode("DeviceSerialNumber");
if (IsReadable(ptrStringSerial))
{
deviceSerialNumber = ptrStringSerial->GetValue();
cout << "Device serial number retrieved as " << deviceSerialNumber << "..." << endl;
}
cout << endl;
// Retrieve, convert, and save images
const int unsigned k_numImages = 10;
//
// Create ImageProcessor instance for post processing images
//
ImageProcessor processor;
//
// Set default image processor color processing method
//
// *** NOTES ***
// By default, if no specific color processing algorithm is set, the image
// processor will default to NEAREST_NEIGHBOR method.
//
processor.SetColorProcessing(SPINNAKER_COLOR_PROCESSING_ALGORITHM_HQ_LINEAR);
for (unsigned int imageCnt = 0; imageCnt < k_numImages; imageCnt++)
{
try
{
// Retrieve the next image from the trigger
result = result | GrabNextImageByTrigger(nodeMap, pCam);
// Retrieve the next received image
ImagePtr pResultImage = pCam->GetNextImage(1000);
if (pResultImage->IsIncomplete())
{
cout << "Image incomplete with image status " << pResultImage->GetImageStatus() << "..." << endl
<< endl;
}
else
{
// Print image information
cout << "Grabbed image " << imageCnt << ", width = " << pResultImage->GetWidth()
<< ", height = " << pResultImage->GetHeight() << endl;
// Convert image to mono 8
ImagePtr convertedImage = processor.Convert(pResultImage, PixelFormat_Mono8);
// Create a unique filename
ostringstream filename;
filename << "Trigger-";
if (deviceSerialNumber != "")
{
filename << deviceSerialNumber.c_str() << "-";
}
filename << imageCnt << ".jpg";
// Save image
convertedImage->Save(filename.str().c_str());
cout << "Image saved at " << filename.str() << endl;
}
// Release image
pResultImage->Release();
cout << endl;
}
catch (Spinnaker::Exception& e)
{
cout << "Error: " << e.what() << endl;
result = -1;
}
}
// End acquisition
pCam->EndAcquisition();
}
catch (Spinnaker::Exception& e)
{
cout << "Error: " << e.what() << endl;
result = -1;
}
return result;
}
// This function acts as the body of the example; please see NodeMapInfo example
// for more in-depth comments on setting up cameras.
int RunSingleCamera(CameraPtr pCam)
{
int result = 0;
int err = 0;
try
{
// Retrieve TL device nodemap and print device information
INodeMap& nodeMapTLDevice = pCam->GetTLDeviceNodeMap();
result = PrintDeviceInfo(nodeMapTLDevice);
// Initialize camera
pCam->Init();
// Retrieve GenICam nodemap
INodeMap& nodeMap = pCam->GetNodeMap();
// Configure trigger
err = ConfigureTrigger(nodeMap);
if (err < 0)
{
return err;
}
// Acquire images
result = result | AcquireImages(pCam, nodeMap, nodeMapTLDevice);
// Reset trigger
result = result | ResetTrigger(nodeMap);
// Deinitialize camera
pCam->DeInit();
}
catch (Spinnaker::Exception& e)
{
cout << "Error: " << e.what() << endl;
result = -1;
}
return result;
}
// Example entry point; please see Enumeration example for more in-depth
// comments on preparing and cleaning up the system.
int main(int /*argc*/, char** /*argv*/)
{
// Since this application saves images in the current folder
// we must ensure that we have permission to write to this folder.
// If we do not have permission, fail right away.
FILE* tempFile = fopen("test.txt", "w+");
if (tempFile == nullptr)
{
cout << "Failed to create file in current folder. Please check "
"permissions."
<< endl;
cout << "Press Enter to exit..." << endl;
getchar();
return -1;
}
fclose(tempFile);
remove("test.txt");
int result = 0;
// Print application build information
cout << "Application build date: " << __DATE__ << " " << __TIME__ << endl << endl;
// Retrieve singleton reference to system object
SystemPtr system = System::GetInstance();
// Print out current library version
const LibraryVersion spinnakerLibraryVersion = system->GetLibraryVersion();
cout << "Spinnaker library version: " << spinnakerLibraryVersion.major << "." << spinnakerLibraryVersion.minor
<< "." << spinnakerLibraryVersion.type << "." << spinnakerLibraryVersion.build << endl
<< endl;
// Retrieve list of cameras from the system
CameraList camList = system->GetCameras();
unsigned int numCameras = camList.GetSize();
cout << "Number of cameras detected: " << numCameras << endl << endl;
// Finish if there are no cameras
if (numCameras == 0)
{
// Clear camera list before releasing system
camList.Clear();
// Release system
system->ReleaseInstance();
cout << "Not enough cameras!" << endl;
cout << "Done! Press Enter to exit..." << endl;
getchar();
return -1;
}
// Run example on each camera
for (unsigned int i = 0; i < numCameras; i++)
{
cout << endl << "Running example for camera " << i << "..." << endl;
result = result | RunSingleCamera(camList.GetByIndex(i));
cout << "Camera " << i << " example complete..." << endl << endl;
}
// Clear camera list before releasing system
camList.Clear();
// Release system
system->ReleaseInstance();
cout << endl << "Done! Press Enter to exit..." << endl;
getchar();
return result;
}