Namespace Spinnaker¶
Namespaces¶
| Type | Name |
|---|---|
| namespace | GUI |
| namespace | GUI_WPF |
| namespace | GenApi |
| namespace | GenICam |
| namespace | Relay |
| namespace | Video |
Classes¶
| Type | Name |
|---|---|
| struct | ActionCommandResult |
| struct | BMPOption |
| class | BasePtr <class T, class B> The base class of the SystemPtr ,CameraPtr ,InterfacePtr ,ProducerPtr ,ImagePtr andLoggingEventDataPtr objects. |
| struct | CCMSettings |
| class | Camera The camera object class. |
| class | CameraBase The base class for the camera object. |
| class | CameraList Used to hold a list of camera objects. |
| class | CameraPtr A reference tracked pointer to a camera object. |
| class | ChunkData The chunk data which contains additional information about an image. |
| struct | CoordinateDependentParams Container for 3D scan calibration parameters used in stereo processing. |
| class | DeviceArrivalEventHandler An event handler for capturing the device arrival event. |
| struct | DeviceEventExposureEndData |
| class | DeviceEventHandler A handler to device events. |
| struct | DeviceEventInferenceData |
| class | DeviceEventUtility Static helper functions for the device event object class. |
| class | DeviceRemovalEventHandler An event handler for capturing the device removal event. |
| class | EventHandler The base class for all event handler types. |
| class | Exception The Exception object represents an error that is returned from the library. Overloaded operators allow comparisons against otherException objects. |
| struct | GenDCOption |
| class | ICameraBase The interface file for base class for the camera object. |
| class | ICameraList Used to hold a list of camera objects. |
| class | IChunkData The Interface file forChunkData . |
| class | IDataStream |
| class | IDeviceArrivalEventHandler |
| class | IDeviceEventHandler |
| class | IDeviceRemovalEventHandler |
| class | IImage The interface file for Image . |
| class | IImageEventHandler |
| class | IImageList The interface file for ImageList class. |
| class | IImageListEventHandler |
| class | IImageProcessor The interface file for ImageProcessor class. |
| class | IImageStatistics The interface file for image statistics. |
| class | IInterface The interface file for Interface . |
| class | IInterfaceArrivalEventHandler |
| class | IInterfaceEventHandler |
| class | IInterfaceList The interface file for InterfaceList class. |
| class | IInterfaceRemovalEventHandler |
| class | ILoggingEventHandler |
| class | IPointCloud The interface file for PointCloud class. |
| class | IProducer The interface file for Producer . |
| class | IProducerList The interface file for ProducerList class. |
| class | IScan3DParameters The Interface file forScan3DParameters data. |
| class | ISpinnakerGPU The interface file for SpinnakerGPU class. |
| class | ISystem The interface file for System . |
| class | ISystemEventHandler |
| class | Image The image object class. |
| class | ImageEventHandler A handler for capturing image arrival events. |
| class | ImageList Used to hold a list of image objects. |
| class | ImageListEventHandler A handler for capturing image list arrival events. |
| struct | ImagePixel |
| class | ImageProcessor Image post processing class for converting a source image to another pixel format. |
| class | ImagePtr A reference tracked pointer to an image object. When the ImagePtr goes out of scope, it will trigger an auto release of the image from the stream. |
| class | ImageStatistics Represents image statistics for an image. |
| class | ImageUtility Static helper functions for the image object class. |
| class | ImageUtilityCCM Static function to create color corrected images from an image object. |
| class | ImageUtilityHeatmap Static functions to create heatmap images from image objects of pixel format Mono8 and Mono16. |
| class | ImageUtilityPolarization Static functions to create polarization images from image objects of pixel format Polarized8 and BayerRGPolarized8. |
| class | ImageUtilityStereo Static helper functions for stereo related computations. |
| struct | InferenceBoundingBox |
| class | InferenceBoundingBoxResult An inference bounding boxes object which holds information about the detected bounding boxes. |
| struct | InferenceBoxCircle |
| struct | InferenceBoxRect |
| struct | InferenceBoxRotatedRect |
| class | Interface An interface object which holds a list of cameras. |
| class | InterfaceArrivalEventHandler An event handler for capturing the interface arrival event. Note that only GEV interface arrivals are currently handled. |
| class | InterfaceEventHandler A handler to device arrival and removal events on all interfaces. |
| class | InterfaceList A list of the available interfaces on the system. |
| class | InterfacePtr A reference tracked pointer to the interface object. |
| class | InterfaceRemovalEventHandler An event handler for capturing the interface removal event. Note that only GEV interface removals are currently handled. |
| struct | JPEGOption |
| struct | JPG2Option |
| struct | LibraryVersion |
| class | LoggingEventData The LoggingEventData object. |
| class | LoggingEventDataPtr A reference tracked pointer to the LoggingEvent object. |
| class | LoggingEventHandler An event handler for capturing the device logging event. |
| struct | PGMOption |
| struct | PNGOption |
| struct | PPMOption |
| class | PointCloud The PointCloud object class. |
| struct | PointCloudParameters |
| class | Producer The producer object is used to retrieve the list of interfaces and cameras available. |
| class | ProducerList A list of the available producers on the system. |
| class | ProducerPtr A reference tracked pointer to the producer object. |
| struct | SIOption |
| class | Scan3DParameters |
| class | SpinnakerGPU Provides the functionality for the user to post process images on an NVIDIA GPU device. |
| struct | Stereo3DPoint |
| struct | StereoCameraParameters |
| class | System The system object is used to retrieve the list of interfaces and cameras available. |
| class | SystemEventHandler A handler to interface arrival and removal events on the system. Note that only GEV interface arrivals and removals are currently handled. |
| class | SystemPtr A reference tracked pointer to a system object. |
| struct | TIFFOption |
| class | TransportLayerDevice Part of the QuickSpin API to provide access to camera information without having to first initialize the camera. |
| class | TransportLayerInterface Part of the QuickSpin API to provide access to camera information without having to first initialize the camera. |
| class | TransportLayerStream Part of the QuickSpin API to provide access to camera information without having to first initialize the camera. |
| class | TransportLayerSystem Part of the QuickSpin API to provide access to camera information without having to first initialize the camera. |
Public Types¶
| Type | Name |
|---|---|
| enum | StreamPriority |
Public Types Documentation¶
enum StreamPriority¶
The documentation for this class was generated from the following file /workspace/include/BasePtr.h