Struct _spinChunkData
ClassList > _spinChunkData
The type of information that can be obtained from image chunk data.
#include <ChunkDataDefC.h>
Public Attributes
Public Attributes Documentation
variable m_blackLevel
double _spinChunkData::m_blackLevel;
variable m_cRC
int64_t _spinChunkData::m_cRC;
variable m_compressionMode
int64_t _spinChunkData::m_compressionMode;
variable m_compressionRatio
double _spinChunkData::m_compressionRatio;
variable m_counterValue
int64_t _spinChunkData::m_counterValue;
variable m_currentDatarate
int64_t _spinChunkData::m_currentDatarate;
variable m_encoderValue
int64_t _spinChunkData::m_encoderValue;
variable m_exposureEndLineStatusAll
int64_t _spinChunkData::m_exposureEndLineStatusAll;
variable m_exposureTime
double _spinChunkData::m_exposureTime;
variable m_frameID
int64_t _spinChunkData::m_frameID;
variable m_gain
double _spinChunkData::m_gain;
variable m_height
int64_t _spinChunkData::m_height;
variable m_image
int64_t _spinChunkData::m_image;
variable m_inferenceConfidence
double _spinChunkData::m_inferenceConfidence;
variable m_inferenceFrameId
int64_t _spinChunkData::m_inferenceFrameId;
variable m_inferenceResult
int64_t _spinChunkData::m_inferenceResult;
variable m_largePenalty
int64_t _spinChunkData::m_largePenalty;
variable m_linePitch
int64_t _spinChunkData::m_linePitch;
variable m_lineStatusAll
int64_t _spinChunkData::m_lineStatusAll;
variable m_maxZ
double _spinChunkData::m_maxZ;
variable m_minZ
double _spinChunkData::m_minZ;
variable m_offsetX
int64_t _spinChunkData::m_offsetX;
variable m_offsetY
int64_t _spinChunkData::m_offsetY;
variable m_partSelector
int64_t _spinChunkData::m_partSelector;
variable m_pixelDynamicRangeMax
int64_t _spinChunkData::m_pixelDynamicRangeMax;
variable m_pixelDynamicRangeMin
int64_t _spinChunkData::m_pixelDynamicRangeMin;
variable m_scan3dAxisMax
double _spinChunkData::m_scan3dAxisMax;
variable m_scan3dAxisMin
double _spinChunkData::m_scan3dAxisMin;
variable m_scan3dBaseline
double _spinChunkData::m_scan3dBaseline;
variable m_scan3dCoordinateOffset
double _spinChunkData::m_scan3dCoordinateOffset;
variable m_scan3dCoordinateReferenceValue
double _spinChunkData::m_scan3dCoordinateReferenceValue;
variable m_scan3dCoordinateScale
double _spinChunkData::m_scan3dCoordinateScale;
variable m_scan3dFocalLength
double _spinChunkData::m_scan3dFocalLength;
variable m_scan3dInvalidDataValue
double _spinChunkData::m_scan3dInvalidDataValue;
variable m_scan3dPrincipalPointU
double _spinChunkData::m_scan3dPrincipalPointU;
variable m_scan3dPrincipalPointV
double _spinChunkData::m_scan3dPrincipalPointV;
double _spinChunkData::m_scan3dTransformValue;
variable m_scanLineSelector
int64_t _spinChunkData::m_scanLineSelector;
variable m_sequencerSetActive
int64_t _spinChunkData::m_sequencerSetActive;
variable m_serialDataLength
int64_t _spinChunkData::m_serialDataLength;
variable m_smallPenalty
int64_t _spinChunkData::m_smallPenalty;
variable m_stereoHeight
int64_t _spinChunkData::m_stereoHeight;
variable m_stereoWidth
int64_t _spinChunkData::m_stereoWidth;
variable m_streamChannelID
int64_t _spinChunkData::m_streamChannelID;
variable m_timerValue
double _spinChunkData::m_timerValue;
variable m_timestamp
int64_t _spinChunkData::m_timestamp;
variable m_timestampLatchValue
int64_t _spinChunkData::m_timestampLatchValue;
variable m_transferBlockID
int64_t _spinChunkData::m_transferBlockID;
variable m_transferQueueCurrentBlockCount
int64_t _spinChunkData::m_transferQueueCurrentBlockCount;
variable m_uniquenessRatio
int64_t _spinChunkData::m_uniquenessRatio;
variable m_width
int64_t _spinChunkData::m_width;
The documentation for this class was generated from the following file C:/workspace/include/spinc/ChunkDataDefC.h