Group IEnumeration_h¶
Public Attributes¶
| Type | Name |
|---|---|
| interface SPINNAKER_API_ABSTRACT | IEnumeration Interface for enumeration properties. |
Public Functions¶
| Type | Name |
|---|---|
| virtual IEnumEntry * | GetCurrentEntry (bool Verify=false, bool IgnoreCache=false) = 0 |
| virtual void | GetEntries (NodeList_t & Entries) = 0 |
| virtual IEnumEntry * | GetEntry (const int64_t IntValue) = 0 |
| virtual IEnumEntry * | GetEntryByName (const GenICam::gcstring & Symbolic) = 0 |
| virtual int64_t | GetIntValue (bool Verify=false, bool IgnoreCache=false) = 0 |
| virtual void | SetIntValue (int64_t Value, bool Verify=true) = 0 |
| virtual GenICam::gcstring | operator* () = 0 |
| virtual IEnumeration & | operator= (const GenICam::gcstring & ValueStr) = 0 |
Public Attributes Documentation¶
variable IEnumeration¶
Interface for enumeration properties.
Public Functions Documentation¶
function GetCurrentEntry¶
Get the current entry
function GetEntries¶
Get list of entry nodes
function GetEntry¶
Get an entry node by its IntValue
function GetEntryByName¶
Get an entry node by name
function GetIntValue¶
Get integer node value
Parameters:
VerifyEnables Range verification (default = false). The AccessMode is always checkedIgnoreCacheIf true the value is read ignoring any caches (default = false)
Returns:
The value read
function SetIntValue¶
Set integer node value
Parameters:
ValueThe value to setVerifyEnables AccessMode and Range verification (default = true)
function operator*¶
Get string node value
Get node value
function operator=¶
Set string node value
Set node value
Note : the operator= is not inherited thus the operator= versions from IEnumeration must be implemented again
Set node value