|
FLIR
Blackfly®S BFS-U3-63S4-BD |
Handling Precautions and Camera Care
Your FLIR machine vision camera is a precisely manufactured device and should be handled with care. Here are some tips on how to care for the device.
- Avoid electrostatic charging.
- If you have purchased a board-level camera you should take the following additional protective measures:
- Either handle bare handed or use non-chargeable gloves, clothes or material. Also, use conductive shoes.
- Install a conductive mat on the floor or working table to prevent the generation of static electricity.
- When handling the camera unit, avoid touching the lenses. Fingerprints will affect the quality of the image produced by the device.
- To clean the lenses, use a standard camera lens cleaning kit or a clean dry cotton cloth. Do not apply excessive force.
- Extended exposure to bright sunlight, rain, dusty environments, etc. may cause problems with the electronics and the optics of the system.
- Avoid excessive shaking, dropping or any kind of mishandling of the device.
| Cleaning the imaging surface of your camera |
| 12/9/2019
© 2015-2019 FLIR® Integrated Imaging Solutions Inc. All rights reserved. Legal | Contact Support | Cookie Policy |
|