PySpin.BooleanNode

class BooleanNode(*args, **kwargs)

Interface for string properties.

GetValue(self, Verify=False, IgnoreCache=False) bool

Parameters

Verify: bool IgnoreCache: bool

Get node value

param Verify:

Enables Range verification (default = false). The AccessMode is always checked.

param IgnoreCache:

If true the value is read ignoring any caches (default = false).

The value read.

IsValueUpdated(self) bool

Checks if the content of the node has changed since the value was last cached by IsValueUpdated() or GetValue().

true if the node value has changed, false otherwise.

SetReference(self, pBase)

Parameters

pBase: Spinnaker::GenApi::INode *

overload SetReference for Value

SetValue(self, Value, Verify=True)

Parameters

Value: bool Verify: bool

Set node value

param Value:

The value to set.

param Verify:

Enables AccessMode and Range verification (default = true).