PySpin.StringNode

class StringNode(*args, **kwargs)

Interface for string properties.

GetMaxLength(self) int64_t

Retrieves the maximum length of the string in bytes

GetValue(self, Verify=False, IgnoreCache=False) gcstring

Parameters

Verify: bool IgnoreCache: bool

Get node value

param Verify:

Enables Range verification (default = false). The AccessMode is always checked

param IgnoreCache:

If true the value is read ignoring any caches (default = false)

The value read

IsValueUpdated(self) bool

Checks if the content of the node has changed since the value was last cached by IsValueUpdated() or GetValue().

true if the node value has changed, false otherwise.

SetReference(self, pBase)

Parameters

pBase: Spinnaker::GenApi::INode *

overload SetReference for Value

SetValue(self, Value, Verify=True)

Parameters

Value: Spinnaker::GenICam::gcstring const & Verify: bool

Set node value

param Value:

The value to set

param Verify:

Enables AccessMode and Range verification (default = true)