PySpin.ChannelStatistics¶
- class ChannelStatistics(image, channel)¶
Class used to store statistics (as properties) for one channel of an image. Properties:
channel: The image channel that the statistics are based on (as an int).
range_min: The smallest possible pixel value.
range_max: The largest possible pixel value.
pixel_value_min: The smallest pixel value in the current channel.
pixel_value_max: The largest pixel value in the current channel.
num_pixel_values: The total number of pixel values in the current channel.
pixel_value_mean: The average pixel value in the current channel.
histogram: NumPy array representing the histogram of the current channel.
- property channel¶
- property histogram¶
- property num_pixel_values¶
- property pixel_value_max¶
- property pixel_value_mean¶
- property pixel_value_min¶
- property range_max¶
- property range_min¶