PySpin.CFeatureBag¶
- class CFeatureBag¶
Bag holding streamable features of a nodetree.
- GetFeatureBagHandle(self) void *¶
- LoadFromBag(self, pNodeMap, Verify=True, pErrorList=None) bool¶
Parameters¶
pNodeMap: Spinnaker::GenApi::INodeMap * Verify: bool pErrorList: Spinnaker::GenICam::gcstring_vector *
Loads the features from the bag to the node tree
- param pNodeMap:
The node map
- param Verify:
If true, all streamable features are read back
- param pErrorList:
If an error occurs during loading the error message is stored in the list and the loading continues For Verify=true the list of names in the feature bag is replayed
again. If a node is a selector it’s value is set to the value from the feature bag If not the value is read from the camera and compared with the value from the feature bag.
- SetInfo(self, Info)¶
Parameters¶
Info: Spinnaker::GenICam::gcstring &
sets information about the node map
- StoreToBag(self, pNodeMap, MaxNumPersistSkriptEntries=-1) int64_t¶
Parameters¶
pNodeMap: Spinnaker::GenApi::INodeMap * MaxNumPersistSkriptEntries: int const
Stores the streamable nodes to this feature bag.
- param pNodeMap:
The node map to persist
- param MaxNumPersistSkriptEntries:
The max number of entries in the container; -1 means unlimited
number of entries in the bag