PySpin.InferenceBoundingBoxResult¶
- class InferenceBoundingBoxResult(*args)¶
An inference bounding boxes object which holds information about the detected bounding boxes.
- GetBoxAt(self, index) InferenceBoundingBox¶
Parameters¶
index: uint16_t const
Returns the bounding box at specified index.
- param index:
Index of the bounding box to return.
- GetBoxCount(self) int16_t¶
Returns the number of bounding boxes.
- GetBoxSize(self) int8_t¶
Returns the number of bytes allocated for one bounding box.
- GetVersion(self) int8_t¶
Returns the bounding box format version number.