PySpin Class Reference¶

Every public class exported by the PySpin module is listed below. Click a class name to see its full method and property documentation.

PySpin.AVIOption

Options for saving AVI files.

PySpin.ActionCommandResult

Action Command Result

PySpin.BMPOption

Options for saving Bitmap image.

PySpin.BooleanNode

Interface for string properties.

PySpin.CBasePtr

Encapsulates a GenApi pointer dealing with the dynamic_cast automatically.

PySpin.CBooleanPtr

Encapsulates a GenApi pointer dealing with the dynamic_cast automatically.

PySpin.CCMSettings

PySpin.CCategoryPtr

Encapsulates a GenApi pointer dealing with the dynamic_cast automatically.

PySpin.CCommandPtr

Encapsulates a GenApi pointer dealing with the dynamic_cast automatically.

PySpin.CDeviceInfoPtr

Encapsulates a GenApi pointer dealing with the dynamic_cast automatically.

PySpin.CEnumEntryPtr

Encapsulates a GenApi pointer dealing with the dynamic_cast automatically.

PySpin.CEnumerationPtr

Encapsulates a GenApi pointer dealing with the dynamic_cast automatically.

PySpin.CFeatureBag

Bag holding streamable features of a nodetree.

PySpin.CFloatPtr

SmartPointer for IFloat interface pointer

PySpin.CIntegerPtr

Encapsulates a GenApi pointer dealing with the dynamic_cast automatically.

PySpin.CNodeMapDynPtr

Encapsulates a GenApi pointer dealing with the dynamic_cast automatically.

PySpin.CNodeMapPtr

Encapsulates a GenApi pointer dealing with the dynamic_cast automatically.

PySpin.CNodePtr

Encapsulates a GenApi pointer dealing with the dynamic_cast automatically.

PySpin.CRegisterPtr

Encapsulates a GenApi pointer dealing with the dynamic_cast automatically.

PySpin.CSelectorPtr

Encapsulates a GenApi pointer dealing with the dynamic_cast automatically.

PySpin.CSelectorSet

The set of selectors selecting a given node

PySpin.CStringPtr

Encapsulates a GenApi pointer dealing with the dynamic_cast automatically.

PySpin.CValuePtr

Encapsulates a GenApi pointer dealing with the dynamic_cast automatically.

PySpin.Camera

The camera object class.

PySpin.CameraBase

The base class for the camera object.

PySpin.CameraList

Used to hold a list of camera objects.

PySpin.CameraPtr

A reference tracked pointer to a camera object.

PySpin.CategoryNode

Interface for string properties.

PySpin.ChannelStatistics

Class used to store statistics (as properties) for one channel of an image.

PySpin.ChunkData

The chunk data which contains additional information about an image.

PySpin.CommandNode

Interface for string properties.

PySpin.CoordinateDependentParams

Container for 3D scan calibration parameters used in stereo processing.

PySpin.DeviceArrivalEventHandler

An event handler for capturing the device arrival event.

PySpin.DeviceEventExposureEndData

Data Fields for Device Event payload for EventExposureEnd

PySpin.DeviceEventHandler

Proxy of C++ Spinnaker::DeviceEventHandler class.

PySpin.DeviceEventInferenceData

Data fields for Device Event payload for EventInference

PySpin.DeviceRemovalEventHandler

An event handler for capturing the device removal event.

PySpin.EAccessModeClass

Holds conversion methods for the access mode enumeration.

PySpin.ECachingModeClass

Holds conversion methods for the caching mode enumeration.

PySpin.EDisplayNotationClass

Holds conversion methods for the notation type of floats.

PySpin.EEndianessClass

Holds conversion methods for the endianess enumeration.

PySpin.EGenApiSchemaVersionClass

helper class converting EGenApiSchemaVersion from and to string

PySpin.EInputDirectionClass

Holds conversion methods for the notation type of floats.

PySpin.ENameSpaceClass

Holds conversion methods for the namespace enumeration.

PySpin.ERepresentationClass

Holds conversion methods for the representation enumeration.

PySpin.ESignClass

Holds conversion methods for the sign enumeration.

PySpin.ESlopeClass

Holds conversion methods for the converter formulas.

PySpin.EStandardNameSpaceClass

Holds conversion methods for the standard namespace enumeration.

PySpin.EVisibilityClass

Holds conversion methods for the visibility enumeration.

PySpin.EYesNoClass

Holds conversion methods for the standard namespace enumeration.

PySpin.EnumEntryNode

Interface for string properties.

PySpin.EnumNode

Interface for string properties.

PySpin.EventHandler

The base class for all event handler types.

PySpin.FloatNode

Interface for string properties.

PySpin.FloatRegNode

Interface for string properties.

PySpin.GenDCOption

Options for saving GenDC image.

PySpin.H264Option

Options for saving H264 files.

PySpin.IBase

Proxy of C++ Spinnaker::GenApi::IBase class.

PySpin.IBoolean

Proxy of C++ Spinnaker::GenApi::IBoolean class.

PySpin.ICameraBase

The interface file for base class for the camera object.

PySpin.ICameraList

Used to hold a list of camera objects.

PySpin.ICategory

Proxy of C++ Spinnaker::GenApi::ICategory class.

PySpin.IChunkData

The Interface file for ChunkData.

PySpin.ICommand

Proxy of C++ Spinnaker::GenApi::ICommand class.

PySpin.IDestroy

Proxy of C++ Spinnaker::GenApi::IDestroy class.

PySpin.IDeviceArrivalEventHandler

PySpin.IDeviceEventHandler

PySpin.IDeviceInfo

Proxy of C++ Spinnaker::GenApi::IDeviceInfo class.

PySpin.IDeviceRemovalEventHandler

PySpin.IEnumEntry

Proxy of C++ Spinnaker::GenApi::IEnumEntry class.

PySpin.IEnumReference

Proxy of C++ Spinnaker::GenApi::IEnumReference class.

PySpin.IEnumeration

Proxy of C++ Spinnaker::GenApi::IEnumeration class.

PySpin.IEnumerationT_AcquisitionModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< AcquisitionModeEnums > class.

PySpin.IEnumerationT_AcquisitionStatusSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< AcquisitionStatusSelectorEnums > class.

PySpin.IEnumerationT_ActionSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ActionSelectorEnums > class.

PySpin.IEnumerationT_ActionUnconditionalModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ActionUnconditionalModeEnums > class.

PySpin.IEnumerationT_AdcBitDepthEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< AdcBitDepthEnums > class.

PySpin.IEnumerationT_AutoAlgorithmSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< AutoAlgorithmSelectorEnums > class.

PySpin.IEnumerationT_AutoExposureControlPriorityEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< AutoExposureControlPriorityEnums > class.

PySpin.IEnumerationT_AutoExposureLightingModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< AutoExposureLightingModeEnums > class.

PySpin.IEnumerationT_AutoExposureMeteringModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< AutoExposureMeteringModeEnums > class.

PySpin.IEnumerationT_AutoExposureTargetGreyValueAutoEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< AutoExposureTargetGreyValueAutoEnums > class.

PySpin.IEnumerationT_BalanceRatioSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< BalanceRatioSelectorEnums > class.

PySpin.IEnumerationT_BalanceWhiteAutoEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< BalanceWhiteAutoEnums > class.

PySpin.IEnumerationT_BalanceWhiteAutoProfileEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< BalanceWhiteAutoProfileEnums > class.

PySpin.IEnumerationT_BinningHorizontalModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< BinningHorizontalModeEnums > class.

PySpin.IEnumerationT_BinningSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< BinningSelectorEnums > class.

PySpin.IEnumerationT_BinningVerticalModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< BinningVerticalModeEnums > class.

PySpin.IEnumerationT_BlackLevelAutoBalanceEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< BlackLevelAutoBalanceEnums > class.

PySpin.IEnumerationT_BlackLevelAutoEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< BlackLevelAutoEnums > class.

PySpin.IEnumerationT_BlackLevelSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< BlackLevelSelectorEnums > class.

PySpin.IEnumerationT_BsiFlatFieldCorrectionAutoEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< BsiFlatFieldCorrectionAutoEnums > class.

PySpin.IEnumerationT_BsiFlatFieldCorrectionGainSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< BsiFlatFieldCorrectionGainSelectorEnums > class.

PySpin.IEnumerationT_ChunkBlackLevelSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkBlackLevelSelectorEnums > class.

PySpin.IEnumerationT_ChunkCounterSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkCounterSelectorEnums > class.

PySpin.IEnumerationT_ChunkEncoderSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkEncoderSelectorEnums > class.

PySpin.IEnumerationT_ChunkEncoderStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkEncoderStatusEnums > class.

PySpin.IEnumerationT_ChunkExposureTimeSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkExposureTimeSelectorEnums > class.

PySpin.IEnumerationT_ChunkGainSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkGainSelectorEnums > class.

PySpin.IEnumerationT_ChunkImageComponentEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkImageComponentEnums > class.

PySpin.IEnumerationT_ChunkPixelFormatEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkPixelFormatEnums > class.

PySpin.IEnumerationT_ChunkRegionIDEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkRegionIDEnums > class.

PySpin.IEnumerationT_ChunkScan3dCoordinateReferenceSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkScan3dCoordinateReferenceSelectorEnums > class.

PySpin.IEnumerationT_ChunkScan3dCoordinateSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkScan3dCoordinateSelectorEnums > class.

PySpin.IEnumerationT_ChunkScan3dCoordinateSystemEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkScan3dCoordinateSystemEnums > class.

PySpin.IEnumerationT_ChunkScan3dCoordinateSystemReferenceEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkScan3dCoordinateSystemReferenceEnums > class.

PySpin.IEnumerationT_ChunkScan3dCoordinateTransformSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkScan3dCoordinateTransformSelectorEnums > class.

PySpin.IEnumerationT_ChunkScan3dDistanceUnitEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkScan3dDistanceUnitEnums > class.

PySpin.IEnumerationT_ChunkScan3dOutputModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkScan3dOutputModeEnums > class.

PySpin.IEnumerationT_ChunkSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkSelectorEnums > class.

PySpin.IEnumerationT_ChunkSourceIDEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkSourceIDEnums > class.

PySpin.IEnumerationT_ChunkTimerSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkTimerSelectorEnums > class.

PySpin.IEnumerationT_ChunkTransferStreamIDEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ChunkTransferStreamIDEnums > class.

PySpin.IEnumerationT_ClConfigurationEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ClConfigurationEnums > class.

PySpin.IEnumerationT_ClTimeSlotsCountEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ClTimeSlotsCountEnums > class.

PySpin.IEnumerationT_ColorTransformationSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ColorTransformationSelectorEnums > class.

PySpin.IEnumerationT_ColorTransformationValueSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ColorTransformationValueSelectorEnums > class.

PySpin.IEnumerationT_ComponentDestinationEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ComponentDestinationEnums > class.

PySpin.IEnumerationT_ComponentSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ComponentSelectorEnums > class.

PySpin.IEnumerationT_CompressionSaturationPriorityEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< CompressionSaturationPriorityEnums > class.

PySpin.IEnumerationT_ConnectionConfigDefaultEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ConnectionConfigDefaultEnums > class.

PySpin.IEnumerationT_ConnectionConfigEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ConnectionConfigEnums > class.

PySpin.IEnumerationT_CounterEventActivationEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< CounterEventActivationEnums > class.

PySpin.IEnumerationT_CounterEventSourceEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< CounterEventSourceEnums > class.

PySpin.IEnumerationT_CounterResetActivationEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< CounterResetActivationEnums > class.

PySpin.IEnumerationT_CounterResetSourceEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< CounterResetSourceEnums > class.

PySpin.IEnumerationT_CounterSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< CounterSelectorEnums > class.

PySpin.IEnumerationT_CounterStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< CounterStatusEnums > class.

PySpin.IEnumerationT_CounterTriggerActivationEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< CounterTriggerActivationEnums > class.

PySpin.IEnumerationT_CounterTriggerSourceEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< CounterTriggerSourceEnums > class.

PySpin.IEnumerationT_CpuAffinityPrivilegeEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< CpuAffinityPrivilegeEnum > class.

PySpin.IEnumerationT_CpuAffinityServiceStatusEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< CpuAffinityServiceStatusEnum > class.

PySpin.IEnumerationT_CxpConnectionTestModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< CxpConnectionTestModeEnums > class.

PySpin.IEnumerationT_CxpLinkConfigurationEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< CxpLinkConfigurationEnums > class.

PySpin.IEnumerationT_CxpLinkConfigurationPreferredEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< CxpLinkConfigurationPreferredEnums > class.

PySpin.IEnumerationT_CxpLinkConfigurationStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< CxpLinkConfigurationStatusEnums > class.

PySpin.IEnumerationT_CxpPoCxpStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< CxpPoCxpStatusEnums > class.

PySpin.IEnumerationT_DecimationHorizontalModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DecimationHorizontalModeEnums > class.

PySpin.IEnumerationT_DecimationSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DecimationSelectorEnums > class.

PySpin.IEnumerationT_DecimationVerticalModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DecimationVerticalModeEnums > class.

PySpin.IEnumerationT_DefectCorrectionModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DefectCorrectionModeEnums > class.

PySpin.IEnumerationT_DefectPixelStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DefectPixelStatusEnums > class.

PySpin.IEnumerationT_DefectPixelTestModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DefectPixelTestModeEnums > class.

PySpin.IEnumerationT_DeinterlacingEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeinterlacingEnums > class.

PySpin.IEnumerationT_DeviceAccessStatusEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceAccessStatusEnum > class.

PySpin.IEnumerationT_DeviceCharacterSetEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceCharacterSetEnums > class.

PySpin.IEnumerationT_DeviceClockSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceClockSelectorEnums > class.

PySpin.IEnumerationT_DeviceConnectionStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceConnectionStatusEnums > class.

PySpin.IEnumerationT_DeviceCurrentSpeedEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceCurrentSpeedEnum > class.

PySpin.IEnumerationT_DeviceDataRW_SelectEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceDataRW_SelectEnums > class.

PySpin.IEnumerationT_DeviceDataStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceDataStatusEnums > class.

PySpin.IEnumerationT_DeviceEndianessMechanismEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceEndianessMechanismEnum > class.

PySpin.IEnumerationT_DeviceIndicatorModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceIndicatorModeEnums > class.

PySpin.IEnumerationT_DeviceLinkHeartbeatModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceLinkHeartbeatModeEnums > class.

PySpin.IEnumerationT_DeviceLinkThroughputLimitModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceLinkThroughputLimitModeEnums > class.

PySpin.IEnumerationT_DevicePowerSupplySelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DevicePowerSupplySelectorEnums > class.

PySpin.IEnumerationT_DeviceRegistersEndiannessEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceRegistersEndiannessEnums > class.

PySpin.IEnumerationT_DeviceScanTypeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceScanTypeEnums > class.

PySpin.IEnumerationT_DeviceSensorChromaEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceSensorChromaEnums > class.

PySpin.IEnumerationT_DeviceSerialPortBaudRateEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceSerialPortBaudRateEnums > class.

PySpin.IEnumerationT_DeviceSerialPortSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceSerialPortSelectorEnums > class.

PySpin.IEnumerationT_DeviceStreamChannelEndiannessEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceStreamChannelEndiannessEnums > class.

PySpin.IEnumerationT_DeviceStreamChannelTypeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceStreamChannelTypeEnums > class.

PySpin.IEnumerationT_DeviceTLTypeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceTLTypeEnums > class.

PySpin.IEnumerationT_DeviceTapGeometryEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceTapGeometryEnums > class.

PySpin.IEnumerationT_DeviceTemperatureSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceTemperatureSelectorEnums > class.

PySpin.IEnumerationT_DeviceTypeEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceTypeEnum > class.

PySpin.IEnumerationT_DeviceTypeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< DeviceTypeEnums > class.

PySpin.IEnumerationT_ElectricalCompliancyTestEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ElectricalCompliancyTestEnums > class.

PySpin.IEnumerationT_EncoderModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< EncoderModeEnums > class.

PySpin.IEnumerationT_EncoderOutputModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< EncoderOutputModeEnums > class.

PySpin.IEnumerationT_EncoderResetActivationEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< EncoderResetActivationEnums > class.

PySpin.IEnumerationT_EncoderResetSourceEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< EncoderResetSourceEnums > class.

PySpin.IEnumerationT_EncoderSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< EncoderSelectorEnums > class.

PySpin.IEnumerationT_EncoderSourceAEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< EncoderSourceAEnums > class.

PySpin.IEnumerationT_EncoderSourceBEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< EncoderSourceBEnums > class.

PySpin.IEnumerationT_EncoderStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< EncoderStatusEnums > class.

PySpin.IEnumerationT_EventNotificationEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< EventNotificationEnums > class.

PySpin.IEnumerationT_EventSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< EventSelectorEnums > class.

PySpin.IEnumerationT_ExposureActiveModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ExposureActiveModeEnums > class.

PySpin.IEnumerationT_ExposureAutoEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ExposureAutoEnums > class.

PySpin.IEnumerationT_ExposureModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ExposureModeEnums > class.

PySpin.IEnumerationT_ExposureTimeModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ExposureTimeModeEnums > class.

PySpin.IEnumerationT_ExposureTimeSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ExposureTimeSelectorEnums > class.

PySpin.IEnumerationT_ExternalVoltageSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ExternalVoltageSelectorEnums > class.

PySpin.IEnumerationT_FLIRFilterDriverStatusEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< FLIRFilterDriverStatusEnum > class.

PySpin.IEnumerationT_FanTypeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< FanTypeEnums > class.

PySpin.IEnumerationT_FfcModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< FfcModeEnums > class.

PySpin.IEnumerationT_FileOpenModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< FileOpenModeEnums > class.

PySpin.IEnumerationT_FileOperationSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< FileOperationSelectorEnums > class.

PySpin.IEnumerationT_FileOperationStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< FileOperationStatusEnums > class.

PySpin.IEnumerationT_FileSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< FileSelectorEnums > class.

PySpin.IEnumerationT_FlashStrobeActiveStateEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< FlashStrobeActiveStateEnums > class.

PySpin.IEnumerationT_FlashStrobeModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< FlashStrobeModeEnums > class.

PySpin.IEnumerationT_GUIXMLLocationEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GUIXMLLocationEnum > class.

PySpin.IEnumerationT_GainAutoBalanceEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GainAutoBalanceEnums > class.

PySpin.IEnumerationT_GainAutoEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GainAutoEnums > class.

PySpin.IEnumerationT_GainConversionEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GainConversionEnums > class.

PySpin.IEnumerationT_GainModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GainModeEnums > class.

PySpin.IEnumerationT_GainSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GainSelectorEnums > class.

PySpin.IEnumerationT_GenICamXMLLocationEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GenICamXMLLocationEnum > class.

PySpin.IEnumerationT_GevCCPEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GevCCPEnum > class.

PySpin.IEnumerationT_GevCCPEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GevCCPEnums > class.

PySpin.IEnumerationT_GevCurrentPhysicalLinkConfigurationEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GevCurrentPhysicalLinkConfigurationEnums > class.

PySpin.IEnumerationT_GevGVCPExtendedStatusCodesSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GevGVCPExtendedStatusCodesSelectorEnums > class.

PySpin.IEnumerationT_GevGVSPExtendedIDModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GevGVSPExtendedIDModeEnums > class.

PySpin.IEnumerationT_GevIEEE1588ClockAccuracyEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GevIEEE1588ClockAccuracyEnums > class.

PySpin.IEnumerationT_GevIEEE1588ModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GevIEEE1588ModeEnums > class.

PySpin.IEnumerationT_GevIEEE1588StatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GevIEEE1588StatusEnums > class.

PySpin.IEnumerationT_GevIEEE1588StatusLatchedEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GevIEEE1588StatusLatchedEnums > class.

PySpin.IEnumerationT_GevIPConfigurationStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GevIPConfigurationStatusEnums > class.

PySpin.IEnumerationT_GevPhysicalLinkConfigurationEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GevPhysicalLinkConfigurationEnums > class.

PySpin.IEnumerationT_GevSCPDirectionEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GevSCPDirectionEnums > class.

PySpin.IEnumerationT_GevSupportedOptionSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< GevSupportedOptionSelectorEnums > class.

PySpin.IEnumerationT_ImageComponentSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ImageComponentSelectorEnums > class.

PySpin.IEnumerationT_ImageCompressionJPEGFormatOptionEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ImageCompressionJPEGFormatOptionEnums > class.

PySpin.IEnumerationT_ImageCompressionModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ImageCompressionModeEnums > class.

PySpin.IEnumerationT_ImageCompressionRateOptionEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< ImageCompressionRateOptionEnums > class.

PySpin.IEnumerationT_InterfaceTypeEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< InterfaceTypeEnum > class.

PySpin.IEnumerationT_LF_FF_CalibrationROIEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LF_FF_CalibrationROIEnums > class.

PySpin.IEnumerationT_LF_FF_CalibrationStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LF_FF_CalibrationStatusEnums > class.

PySpin.IEnumerationT_LF_FF_RawSetDataStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LF_FF_RawSetDataStatusEnums > class.

PySpin.IEnumerationT_LF_FF_ReferencePointEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LF_FF_ReferencePointEnums > class.

PySpin.IEnumerationT_LF_FF_SequenceStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LF_FF_SequenceStatusEnums > class.

PySpin.IEnumerationT_LF_FF_SetSelectionModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LF_FF_SetSelectionModeEnums > class.

PySpin.IEnumerationT_LUTSelectionEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LUTSelectionEnums > class.

PySpin.IEnumerationT_LUTSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LUTSelectorEnums > class.

PySpin.IEnumerationT_LUTStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LUTStatusEnums > class.

PySpin.IEnumerationT_LensShadingCoefficientActiveSetEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LensShadingCoefficientActiveSetEnums > class.

PySpin.IEnumerationT_LensShadingCorrectionModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LensShadingCorrectionModeEnums > class.

PySpin.IEnumerationT_LineFormatEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LineFormatEnums > class.

PySpin.IEnumerationT_LineInputFilterSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LineInputFilterSelectorEnums > class.

PySpin.IEnumerationT_LineModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LineModeEnums > class.

PySpin.IEnumerationT_LineSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LineSelectorEnums > class.

PySpin.IEnumerationT_LineSourceEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LineSourceEnums > class.

PySpin.IEnumerationT_LogicBlockLUTInputActivationEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LogicBlockLUTInputActivationEnums > class.

PySpin.IEnumerationT_LogicBlockLUTInputSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LogicBlockLUTInputSelectorEnums > class.

PySpin.IEnumerationT_LogicBlockLUTInputSourceEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LogicBlockLUTInputSourceEnums > class.

PySpin.IEnumerationT_LogicBlockLUTSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LogicBlockLUTSelectorEnums > class.

PySpin.IEnumerationT_LogicBlockSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< LogicBlockSelectorEnums > class.

PySpin.IEnumerationT_MediaOptimizationPrivilegeEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< MediaOptimizationPrivilegeEnum > class.

PySpin.IEnumerationT_MultiRoiConfigurationInvalidReasonEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< MultiRoiConfigurationInvalidReasonEnums > class.

PySpin.IEnumerationT_MultiRoiSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< MultiRoiSelectorEnums > class.

PySpin.IEnumerationT_POEStatusEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< POEStatusEnum > class.

PySpin.IEnumerationT_PixelColorFilterEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< PixelColorFilterEnums > class.

PySpin.IEnumerationT_PixelFormatEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< PixelFormatEnums > class.

PySpin.IEnumerationT_PixelFormatInfoSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< PixelFormatInfoSelectorEnums > class.

PySpin.IEnumerationT_PixelSizeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< PixelSizeEnums > class.

PySpin.IEnumerationT_RegionDestinationEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< RegionDestinationEnums > class.

PySpin.IEnumerationT_RegionModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< RegionModeEnums > class.

PySpin.IEnumerationT_RegionSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< RegionSelectorEnums > class.

PySpin.IEnumerationT_RgbTransformLightSourceEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< RgbTransformLightSourceEnums > class.

PySpin.IEnumerationT_Scan3dCoordinateReferenceSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< Scan3dCoordinateReferenceSelectorEnums > class.

PySpin.IEnumerationT_Scan3dCoordinateSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< Scan3dCoordinateSelectorEnums > class.

PySpin.IEnumerationT_Scan3dCoordinateSystemEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< Scan3dCoordinateSystemEnums > class.

PySpin.IEnumerationT_Scan3dCoordinateSystemReferenceEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< Scan3dCoordinateSystemReferenceEnums > class.

PySpin.IEnumerationT_Scan3dCoordinateTransformSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< Scan3dCoordinateTransformSelectorEnums > class.

PySpin.IEnumerationT_Scan3dDistanceUnitEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< Scan3dDistanceUnitEnums > class.

PySpin.IEnumerationT_Scan3dOutputModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< Scan3dOutputModeEnums > class.

PySpin.IEnumerationT_SensorBitDepthEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SensorBitDepthEnums > class.

PySpin.IEnumerationT_SensorDigitizationTapsEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SensorDigitizationTapsEnums > class.

PySpin.IEnumerationT_SensorRegisterReadWriteModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SensorRegisterReadWriteModeEnums > class.

PySpin.IEnumerationT_SensorShutterModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SensorShutterModeEnums > class.

PySpin.IEnumerationT_SensorTapsEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SensorTapsEnums > class.

PySpin.IEnumerationT_SequencerConfigurationModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SequencerConfigurationModeEnums > class.

PySpin.IEnumerationT_SequencerConfigurationValidEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SequencerConfigurationValidEnums > class.

PySpin.IEnumerationT_SequencerModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SequencerModeEnums > class.

PySpin.IEnumerationT_SequencerSetValidEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SequencerSetValidEnums > class.

PySpin.IEnumerationT_SequencerTriggerActivationEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SequencerTriggerActivationEnums > class.

PySpin.IEnumerationT_SequencerTriggerSourceEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SequencerTriggerSourceEnums > class.

PySpin.IEnumerationT_SerialPortBaudRateEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SerialPortBaudRateEnums > class.

PySpin.IEnumerationT_SerialPortParityEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SerialPortParityEnums > class.

PySpin.IEnumerationT_SerialPortSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SerialPortSelectorEnums > class.

PySpin.IEnumerationT_SerialPortSourceEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SerialPortSourceEnums > class.

PySpin.IEnumerationT_SerialPortStopBitsEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SerialPortStopBitsEnums > class.

PySpin.IEnumerationT_SoftwareSignalSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SoftwareSignalSelectorEnums > class.

PySpin.IEnumerationT_SoftwareUpdateStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SoftwareUpdateStatusEnums > class.

PySpin.IEnumerationT_SourceSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< SourceSelectorEnums > class.

PySpin.IEnumerationT_StereoResolutionEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< StereoResolutionEnums > class.

PySpin.IEnumerationT_StreamBufferCountModeEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< StreamBufferCountModeEnum > class.

PySpin.IEnumerationT_StreamBufferHandlingModeEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< StreamBufferHandlingModeEnum > class.

PySpin.IEnumerationT_StreamModeEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< StreamModeEnum > class.

PySpin.IEnumerationT_StreamTypeEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< StreamTypeEnum > class.

PySpin.IEnumerationT_TLTypeEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TLTypeEnum > class.

PySpin.IEnumerationT_TeledyneGigeVisionFilterDriverStatusEnum

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TeledyneGigeVisionFilterDriverStatusEnum > class.

PySpin.IEnumerationT_TestImageSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TestImageSelectorEnums > class.

PySpin.IEnumerationT_TestModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TestModeEnums > class.

PySpin.IEnumerationT_TestPatternEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TestPatternEnums > class.

PySpin.IEnumerationT_TestPatternGeneratorSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TestPatternGeneratorSelectorEnums > class.

PySpin.IEnumerationT_TimerSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TimerSelectorEnums > class.

PySpin.IEnumerationT_TimerStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TimerStatusEnums > class.

PySpin.IEnumerationT_TimerTriggerActivationEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TimerTriggerActivationEnums > class.

PySpin.IEnumerationT_TimerTriggerSourceEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TimerTriggerSourceEnums > class.

PySpin.IEnumerationT_TransferComponentSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TransferComponentSelectorEnums > class.

PySpin.IEnumerationT_TransferControlModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TransferControlModeEnums > class.

PySpin.IEnumerationT_TransferOperationModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TransferOperationModeEnums > class.

PySpin.IEnumerationT_TransferQueueModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TransferQueueModeEnums > class.

PySpin.IEnumerationT_TransferSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TransferSelectorEnums > class.

PySpin.IEnumerationT_TransferStatusSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TransferStatusSelectorEnums > class.

PySpin.IEnumerationT_TransferTriggerActivationEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TransferTriggerActivationEnums > class.

PySpin.IEnumerationT_TransferTriggerModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TransferTriggerModeEnums > class.

PySpin.IEnumerationT_TransferTriggerSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TransferTriggerSelectorEnums > class.

PySpin.IEnumerationT_TransferTriggerSourceEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TransferTriggerSourceEnums > class.

PySpin.IEnumerationT_TriggerActivationEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TriggerActivationEnums > class.

PySpin.IEnumerationT_TriggerModeEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TriggerModeEnums > class.

PySpin.IEnumerationT_TriggerOverlapEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TriggerOverlapEnums > class.

PySpin.IEnumerationT_TriggerSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TriggerSelectorEnums > class.

PySpin.IEnumerationT_TriggerSourceEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< TriggerSourceEnums > class.

PySpin.IEnumerationT_U3VCurrentSpeedEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< U3VCurrentSpeedEnums > class.

PySpin.IEnumerationT_UserOutputSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< UserOutputSelectorEnums > class.

PySpin.IEnumerationT_UserSetDefaultEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< UserSetDefaultEnums > class.

PySpin.IEnumerationT_UserSetSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< UserSetSelectorEnums > class.

PySpin.IEnumerationT_WhiteBalanceStatusEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< WhiteBalanceStatusEnums > class.

PySpin.IEnumerationT_WhiteClipSelectorEnums

Proxy of C++ Spinnaker::GenApi::IEnumerationT< WhiteClipSelectorEnums > class.

PySpin.IFloat

Proxy of C++ Spinnaker::GenApi::IFloat class.

PySpin.IImage

The interface file for Image.

PySpin.IImageEventHandler

PySpin.IImageList

The interface file for ImageList class.

PySpin.IImageListEventHandler

PySpin.IImageProcessor

The interface file for ImageProcessor class.

PySpin.IInteger

Proxy of C++ Spinnaker::GenApi::IInteger class.

PySpin.IInterface

The interface file for Interface.

PySpin.IInterfaceArrivalEventHandler

PySpin.IInterfaceEventHandler

PySpin.IInterfaceList

The interface file for InterfaceList class.

PySpin.IInterfaceRemovalEventHandler

PySpin.ILoggingEventHandler

PySpin.INode

Proxy of C++ Spinnaker::GenApi::INode class.

PySpin.INodeMap

Proxy of C++ Spinnaker::GenApi::INodeMap class.

PySpin.INodeMapDyn

Proxy of C++ Spinnaker::GenApi::INodeMapDyn class.

PySpin.IPersistScript

Proxy of C++ Spinnaker::GenApi::IPersistScript class.

PySpin.IPointCloud

The interface file for PointCloud class.

PySpin.IReference

Proxy of C++ Spinnaker::GenApi::IReference class.

PySpin.IRegister

Proxy of C++ Spinnaker::GenApi::IRegister class.

PySpin.IScan3DParameters

The Interface file for Scan3DParameters data.

PySpin.ISelector

Proxy of C++ Spinnaker::GenApi::ISelector class.

PySpin.ISelectorDigit

Proxy of C++ Spinnaker::GenApi::ISelectorDigit class.

PySpin.IString

Proxy of C++ Spinnaker::GenApi::IString class.

PySpin.ISystem

The interface file for System.

PySpin.ISystemEventHandler

PySpin.IValue

Proxy of C++ Spinnaker::GenApi::IValue class.

PySpin.Image

The image object class.

PySpin.ImageEventHandler

A handler for capturing image arrival events.

PySpin.ImageList

Used to hold a list of image objects.

PySpin.ImageListEventHandler

A handler for capturing image list arrival events.

PySpin.ImagePixel

Image Pixel Structure

PySpin.ImageProcessor

Image post processing class for converting a source image to another pixel format.

PySpin.ImagePtr

A reference tracked pointer to an image object.

PySpin.ImageUtility

Static helper functions for the image object class.

PySpin.ImageUtilityCCM

Static function to create color corrected images from an image object.

PySpin.ImageUtilityHeatmap

Static functions to create heatmap images from image objects of pixel format Mono8 and Mono16.

PySpin.ImageUtilityPolarization

Static functions to create polarization images from image objects of pixel format Polarized8 and BayerRGPolarized8.

PySpin.ImageUtilityStereo

Static helper functions for stereo related computations.

PySpin.InferenceBoundingBox

Inference Bounding Boxes data structure

PySpin.InferenceBoundingBoxResult

An inference bounding boxes object which holds information about the detected bounding boxes.

PySpin.InferenceBoxCircle

PySpin.InferenceBoxRect

Inference Bounding Box Type Data Structures

PySpin.InferenceBoxRotatedRect

PySpin.IntRegNode

Interface for string properties.

PySpin.IntegerNode

Interface for string properties.

PySpin.InterfaceArrivalEventHandler

An event handler for capturing the interface arrival event.

PySpin.InterfaceEventHandler

A handler to device arrival and removal events on all interfaces.

PySpin.InterfaceList

A list of the available interfaces on the system.

PySpin.InterfacePtr

A reference tracked pointer to the interface object.

PySpin.InterfaceRemovalEventHandler

An event handler for capturing the interface removal event.

PySpin.JPEGOption

Options for saving JPEG image.

PySpin.JPG2Option

Options for saving JPEG2000 image.

PySpin.LibraryVersion

Provides easier access to the current version of Spinnaker.

PySpin.LoggingEventData

The LoggingEventData object.

PySpin.LoggingEventDataPtr

A reference tracked pointer to the LoggingEvent object.

PySpin.LoggingEventHandler

An event handler for capturing the device logging event.

PySpin.MJPGOption

Options for saving MJPG files.

PySpin.Node

class common to all nodes

PySpin.NodeCallback

Proxy of C++ NodeCallback class.

PySpin.NodeMap

Smart pointer template for NodeMaps with create function.

PySpin.PGMOption

Options for saving PGM images.

PySpin.PNGOption

Options for saving PNG images.

PySpin.PPMOption

Options for saving PPM images.

PySpin.PointCloud

The PointCloud object class.

PySpin.PointCloudParameters

PySpin.RegisterNode

Interface for string properties.

PySpin.SIOption

Options for saving Spinnaker image.

PySpin.Scan3DParameters

PySpin.SpinVideo

Provides the functionality for the user to record images to an AVI/MP4 file.

PySpin.SpinnakerException

Exception class for the PySpin module.

PySpin.Stereo3DPoint

3D Point Structure

PySpin.StereoCameraParameters

PySpin.StringNode

Interface for string properties.

PySpin.StringRegNode

Interface for string properties.

PySpin.System

The system object is used to retrieve the list of interfaces and cameras available.

PySpin.SystemEventHandler

A handler to interface arrival and removal events on the system.

PySpin.SystemPtr

A reference tracked pointer to a system object.

PySpin.TIFFOption

Options for saving TIFF images.

PySpin.TransportLayerDevice

Part of the QuickSpin API to provide access to camera information without having to first initialize the camera.

PySpin.TransportLayerInterface

Part of the QuickSpin API to provide access to camera information without having to first initialize the camera.

PySpin.TransportLayerStream

Part of the QuickSpin API to provide access to camera information without having to first initialize the camera.

PySpin.TransportLayerSystem

Part of the QuickSpin API to provide access to camera information without having to first initialize the camera.

PySpin.ValueNode

Interface for value properties.

PySpin.Version_t

Version

PySpin.double_autovector_t

Vector of doubles with reference counting.

PySpin.gcstring

PySpin.int64_autovector_t

Vector of integers with reference counting.

PySpin.node_vector

Proxy of C++ Spinnaker::GenApi::node_vector class.

PySpin.updatormessage_callback_type

PySpin.updatorprogress_callback_type

PySpin.value_vector

Proxy of C++ Spinnaker::GenApi::value_vector class.