PySpin.InterfaceRemovalEventHandler

class InterfaceRemovalEventHandler

An event handler for capturing the interface removal event. Note that only GEV interface removals are currently handled.

OnInterfaceRemoval(self, pInterface)

Parameters

pInterface: Spinnaker::InterfacePtr

Spinnaker::InterfaceRemovalEventHandler::OnInterfaceRemoval

Interface removal event callback. Note that only GEV interface removals are

currently handled.

param pInterface:

Reference tracked pointer to Interface object of the adapter removed from the system