PySpin.SpinVideo

class SpinVideo

Provides the functionality for the user to record images to an AVI/MP4 file.

Append(self, pImage)

Parameters

pImage: Spinnaker::ImagePtr

Spinnaker::Video::SpinVideo::Append Append an image to the video file. When using the H264 encoder, several images are required to be appended before the encoder is able to output the first encoded frame.

param pImage:

The image to append.

Close(self)

Spinnaker::Video::SpinVideo::Close Close the video file. This function will throw an exception when the H264 encoder was unable to output any encoded frames, in which case the output video should be considered invalid.

See: Open()

See: Append(ImagePtr pImage)

Open(self, pFileName, pOption)

Parameters

pFileName: char const * pOption: Spinnaker::Video::AVIOption &

Open(self, pFileName, pOption)

Parameters

pFileName: char const * pOption: Spinnaker::Video::MJPGOption &

Open(self, pFileName, pOption)

Parameters

pFileName: char const * pOption: Spinnaker::Video::H264Option &

Spinnaker::Video::SpinVideo::Open Open an H264 MP4 video file in preparation for writing Images to disk. The size of MP4 files is limited to 2GB. The filenames are automatically generated using the filename specified.

param pFileName:

The filename of the MP4 video file.

param pOption:

H264 options to apply to the MP4 video file.

See:

Close()

See: H264Option

SetMaximumFileSize(self, size)

Parameters

size: unsigned int

Spinnaker::Video::SpinVideo::SetMaximumFileSize Set the maximum file size (in megabytes) of a AVI/MP4 file. A new video file is created automatically when file size limit is reached. Setting a maximum size of 0 indicates no limit on file size.

Note that this size serves only as a hint and can still be slightly exceeded in some cases after the video trailer is written.

param size:

The maximum video file size in MB.

See:

Append(ImagePtr pImage)