PySpin.StringNode¶
- class StringNode(*args, **kwargs)¶
Interface for string properties.
- GetMaxLength(self) int64_t¶
Spinnaker::GenApi::StringNode::GetMaxLength Retrieves the maximum length of the string in bytes
- GetValue(self, Verify=False, IgnoreCache=False) gcstring¶
Parameters¶
Verify: bool IgnoreCache: bool
Spinnaker::GenApi::StringNode::GetValue Get node value
- param Verify:
Enables Range verification (default = false). The AccessMode is always checked
- param IgnoreCache:
If true the value is read ignoring any caches (default = false)
The value read
- IsValueUpdated(self) bool¶
Spinnaker::GenApi::StringNode::IsValueUpdated Checks if the content of the node has changed since the value was last cached by IsValueUpdated() or GetValue().
true if the node value has changed, false otherwise.