PySpin.InterfaceList¶
- class InterfaceList(*args)¶
A list of the available interfaces on the system.
- Add(self, iface)¶
Parameters¶
iface: Spinnaker::InterfacePtr
Spinnaker::InterfaceList::Add Adds a copy of an interface object.
- param iface:
An interface object to be added to this list.
- Append(self, list)¶
Parameters¶
list: Spinnaker::InterfaceList const *
Spinnaker::InterfaceList::Append Appends a copy of the interfact list.
- param list:
Another InterfaceList object, whose elements are added to this list.
- Clear(self)¶
Spinnaker::InterfaceList::Clear Clears the list of interfaces and destroys their corresponding objects. It is important to first make sure there are no referenced cameras still in use before calling Clear(). If a camera on any of the interfaces is still in use this function will throw an exception.
- GetByIndex(self, index) InterfacePtr¶
Parameters¶
index: unsigned int
Spinnaker::InterfaceList::GetByIndex Returns a pointer to an Interface object at the “index”.
- param index:
The index at which to retrieve the Interface object
A pointer to an Interface object.
- GetByInterfaceID(self, interfaceID) InterfacePtr¶
Parameters¶
interfaceID: std::string
Spinnaker::InterfaceList::GetByInterfaceID Returns a pointer to a interface object with the specified interface identifier. This function will return a NULL InterfacePtr if no matching interface identifier is found.
- param interfaceID:
The unique interface identifier of the interface object to retrieve
A pointer to an Interface object.
- GetSize(self) unsigned int¶
Spinnaker::InterfaceList::GetSize Returns the size of the interface list. The size is the number of Interface objects stored in the list.
An integer that represents the list size.
- Remove(self, iface)¶
Parameters¶
iface: Spinnaker::InterfacePtr
Spinnaker::InterfaceList::Remove Removes all occurences of an interface that is pointed to by the input interface pointer and destroys its corresponding reference counted object. This function will throw a Spinnaker exception with SPINNAKER_ERR_NOT_AVAILABLEerror if no matching interface is found.
- param iface:
Pointer to the interface that is to be removed