PySpin.InterfaceArrivalEventHandler¶
- class InterfaceArrivalEventHandler¶
An event handler for capturing the interface arrival event. Note that only GEV interface arrivals are currently handled.
- OnInterfaceArrival(self, pInterface)¶
Parameters¶
pInterface: Spinnaker::InterfacePtr
- Spinnaker::InterfaceArrivalEventHandler::OnInterfaceArrival
Interface arrival event callback. Note that only GEV interface arrivals are
currently handled.
- param pInterface:
Reference tracked pointer to Interface object of the adapter attached to the system