PySpin.ImageList¶
- class ImageList(*args)¶
Used to hold a list of image objects.
- Add(self, image)¶
Parameters¶
image: Spinnaker::ImagePtr
Spinnaker::ImageList::Add Adds a copy of an image object.
- param image:
An image object to be added to this list.
- Append(self, list)¶
Parameters¶
list: Spinnaker::ImageList const &
Spinnaker::ImageList::Append Appends a copy of the image list.
- param list:
Another ImageList object, whose elements are added to this list.
- Clear(self)¶
Spinnaker::ImageList::Clear Clears the list of images and destroys their corresponding reference counted objects. This is necessary in order to clean up the parent interface. It is important that the camera list is destroyed or is cleared before calling system->ReleaseInstance() or else the call to system->ReleaseInstance() will result in an error message thrown that a reference to the camera is still held.
See: System::ReleaseInstance()
- GetByIndex(self, index) ImagePtr¶
Parameters¶
index: unsigned int
Spinnaker::ImageList::GetByIndex Returns a pointer to an image object at the “index”. This function will throw a Spinnaker exception with SPINNAKER_ERR_INVALID_PARAMETER error if the input index is out of range.
- param index:
The index at which to retrieve the Image object
A pointer to an image object.
- GetByPayloadType(self, payloadType) ImagePtr¶
Parameters¶
payloadType: enum Spinnaker::ImagePayloadType const
Spinnaker::ImageList::GetByPayloadType Returns a pointer to an image object with the specified image payload type. This function will return a null image pointer if no image with matching image payload type is found.
- param payloadType:
The stream index of the Image object to retrieve
A pointer to a image object.
- GetByPixelFormat(self, pixelFormat) ImagePtr¶
Parameters¶
pixelFormat: enum Spinnaker::PixelFormatEnums
Spinnaker::ImageList::GetByPixelFormat Returns a pointer to the first image object with the pixel format from the list. This function will return a null image pointer if no image with matching pixel format is found.
- param pixelFormat:
The pixel format of the Image object to retrieve
A pointer to an image object.
- GetByStreamIndex(self, streamIndex) ImagePtr¶
Parameters¶
streamIndex: uint64_t const
Spinnaker::ImageList::GetByStreamIndex Returns a pointer to an image object with the specified stream index. This function will return a NULL ImagePtr if no image with matching stream index is found.
- param streamIndex:
The stream index of the Image object to retrieve
A pointer to a image object.
- GetImagesByPayloadType(self, payloadType) ImageList¶
Parameters¶
payloadType: enum Spinnaker::ImagePayloadType const
Spinnaker::ImageList::GetImagesByPayloadType Returns an ImageList containing all the images matching the specified image payload type. This function will return an empty list if no image with matching image payload type is found.
- param payloadType:
The stream index of the Image object to retrieve
A pointer to a image object.
- GetImagesByPixelFormat(self, pixelFormat) ImageList¶
Parameters¶
pixelFormat: enum Spinnaker::PixelFormatEnums
Spinnaker::ImageList::GetImagesByPixelFormat Returns an ImageList containing all imageList objects that match the pixel format provided. This function will return an empty list if no image with matching pixel format is found.
- param pixelFormat:
The pixel format of the Image object to retrieve
An ImageList containing all matching image objects.
- GetSize(self) unsigned int¶
Spinnaker::ImageList::GetSize Returns the size of the image list. The size is the number of Image objects stored in the list.
An integer that represents the list size.
- Release(self)¶
Spinnaker::ImageList::Release
- RemoveByIndex(self, index)¶
Parameters¶
index: unsigned int
Spinnaker::ImageList::RemoveByIndex Removes an image at “index” and destroys its corresponding reference counted object. This function will throw a Spinnaker exception with SPINNAKER_ERR_INVALID_PARAMETER error if the input index is out of range.
- param index:
The index at which to remove the Image object
- RemoveByPayloadType(self, payloadType)¶
Parameters¶
payloadType: enum Spinnaker::ImagePayloadType const
Spinnaker::ImageList::RemoveByPayloadType Removes an image object with the specified payload type from the list. This function will throw a Spinnaker exception with SPINNAKER_ERR_INVALID_PARAMETER error if the list does not have any image with the specified payload type.
- param payloadType:
The payload type of the Image object to retrieve
- RemoveByPixelFormat(self, pixelFormat)¶
Parameters¶
pixelFormat: enum Spinnaker::PixelFormatEnums
Spinnaker::ImageList::RemoveByPixelFormat Removes an image object with the image pixel format from the list. This function will throw a Spinnaker exception with SPINNAKER_ERR_INVALID_PARAMETER error if the list does not have any image with the specified pixel format.
- param pixelFormat:
The pixel format of the image object to remove
- RemoveByStreamIndex(self, streamIndex)¶
Parameters¶
streamIndex: uint64_t const
Spinnaker::ImageList::RemoveByStreamIndex Removes an image object with the stream index from the list. This function will throw a Spinnaker exception with SPINNAKER_ERR_INVALID_PARAMETER error if the list does not have any image with the specified stream index.
- param streamIndex:
The stream index of the Image object to retrieve