PySpin.FloatNode¶
- class FloatNode(*args, **kwargs)¶
Interface for string properties.
- GetDisplayNotation(self) Spinnaker::GenApi::EDisplayNotation¶
Spinnaker::GenApi::FloatNode::GetDisplayNotation Get the way the float should be converted to a string
- GetDisplayPrecision(self) int64_t¶
Spinnaker::GenApi::FloatNode::GetDisplayPrecision Get the precision to be used when converting the float to a string
- GetEnumAlias(self) IEnumeration¶
Spinnaker::GenApi::FloatNode::GetEnumAlias gets the interface of an alias node.
- GetInc(self) double¶
Spinnaker::GenApi::FloatNode::GetInc Get the constant increment if there is any
- GetIncMode(self) Spinnaker::GenApi::EIncMode¶
Spinnaker::GenApi::FloatNode::GetIncMode Get increment mode
- GetIntAlias(self) IInteger¶
Spinnaker::GenApi::FloatNode::GetIntAlias gets the interface of an alias node.
- GetListOfValidValues(self, bounded=True) double_autovector_t¶
Parameters¶
bounded: bool
Spinnaker::GenApi::FloatNode::GetListOfValidValues Get list of valid value
- GetMax(self) double¶
Spinnaker::GenApi::FloatNode::GetMax Get maximum value allowed
- GetMin(self) double¶
Spinnaker::GenApi::FloatNode::GetMin Get minimum value allowed
- GetRepresentation(self) Spinnaker::GenApi::ERepresentation¶
Spinnaker::GenApi::FloatNode::GetRepresentation Get recommended representation
- GetValue(self, Verify=False, IgnoreCache=False) double¶
Parameters¶
Verify: bool IgnoreCache: bool
Spinnaker::GenApi::FloatNode::GetValue Get node value
- param Verify:
Enables Range verification (default = false). The AccessMode is always checked
- param IgnoreCache:
If true the value is read ignoring any caches (default = false)
The value read
- ImposeMax(self, Value)¶
Parameters¶
Value: double
Spinnaker::GenApi::FloatNode::ImposeMax Restrict maximum value
- ImposeMin(self, Value)¶
Parameters¶
Value: double
Spinnaker::GenApi::FloatNode::ImposeMin Restrict minimum value
- IsValueUpdated(self) bool¶
Spinnaker::GenApi::FloatNode::IsValueUpdated Checks if the content of the node has changed since the value was last cached by IsValueUpdated() or GetValue().
true if the node value has changed, false otherwise.