PySpin.ChunkData¶
- class ChunkData(*args)¶
The chunk data which contains additional information about an image.
- GetBlackLevel(self) float64_t¶
Spinnaker::ChunkData::GetBlackLevel Description: Returns the black level used to capture the image. Visibility:
- GetCRC(self) int64_t¶
Spinnaker::ChunkData::GetCRC Description: Returns the CRC of the image payload. Visibility:
- GetCompressionMode(self) int64_t¶
Spinnaker::ChunkData::GetCompressionMode Description: Visibility:
- GetCompressionRatio(self) float64_t¶
Spinnaker::ChunkData::GetCompressionRatio Description: Visibility:
- GetCounterValue(self) int64_t¶
Spinnaker::ChunkData::GetCounterValue Description: Returns the value of the selected Chunk counter at the time of the FrameStart event. Visibility: Expert
- GetCurrentDatarate(self) int64_t¶
Spinnaker::ChunkData::GetCurrentDatarate Description: Visibility:
- GetEnable(self) bool¶
Spinnaker::ChunkData::GetEnable Description: Enables the inclusion of the selected Chunk data in the payload of the image. Visibility:
- GetEncoderValue(self) int64_t¶
Spinnaker::ChunkData::GetEncoderValue Description: Returns the counter’s value of the selected Encoder at the time of the FrameStart in area scan mode or the counter’s value at the time of the LineStart selected by ChunkScanLineSelector in LineScan mode. Visibility: Expert
- GetExposureEndLineStatusAll(self) int64_t¶
Spinnaker::ChunkData::GetExposureEndLineStatusAll Description: Returns the status of all the I/O lines at the end of exposure event. Visibility:
- GetExposureTime(self) float64_t¶
Spinnaker::ChunkData::GetExposureTime Description: Returns the exposure time used to capture the image. Visibility:
- GetFrameID(self) int64_t¶
Spinnaker::ChunkData::GetFrameID Description: Returns the image frame ID. Visibility:
- GetGain(self) float64_t¶
Spinnaker::ChunkData::GetGain Description: Returns the gain used to capture the image. Visibility:
- GetHeight(self) int64_t¶
Spinnaker::ChunkData::GetHeight Description: Returns the height of the image included in the payload. Visibility:
- GetImage(self) int64_t¶
Spinnaker::ChunkData::GetImage Description: Returns the image payload. Visibility:
- GetInferenceBoundingBoxResult(self) InferenceBoundingBoxResult¶
Spinnaker::ChunkData::GetInferenceBoundingBoxResult Description: Returns the chunk inference bounding box result data. Visibility: Expert
- GetInferenceConfidence(self) float64_t¶
Spinnaker::ChunkData::GetInferenceConfidence Description: Returns the chunk data inference confidence percentage. Visibility: Expert
- GetInferenceFrameId(self) int64_t¶
Spinnaker::ChunkData::GetInferenceFrameId Description: Returns the frame ID associated with the most recent inference result. Visibility: Expert
- GetInferenceResult(self) int64_t¶
Spinnaker::ChunkData::GetInferenceResult Description: Returns the chunk data inference result. Visibility: Expert
- GetLargePenalty(self) int64_t¶
Spinnaker::ChunkData::GetLargePenalty Description: Returns the penalty when the change of Disparity Change is plus or minus 1. Visibility: Expert
- GetLinePitch(self) int64_t¶
Spinnaker::ChunkData::GetLinePitch Description: Returns the LinePitch of the image included in the payload. Visibility: Expert
- GetLineStatusAll(self) int64_t¶
Spinnaker::ChunkData::GetLineStatusAll Description: Returns the status of all the I/O lines at the start of exposure event. Visibility:
- GetMaxZ(self) float64_t¶
Spinnaker::ChunkData::GetMaxZ Description: Returns the maximum depth in meters for the point cloud range. Visibility: Expert
- GetMinZ(self) float64_t¶
Spinnaker::ChunkData::GetMinZ Description: Returns the minimum depth in meters for the point cloud range. Visibility: Expert
- GetModeActive(self) bool¶
Spinnaker::ChunkData::GetModeActive Description: Activates the inclusion of Chunk data in the payload of the image. Visibility:
- GetOffsetX(self) int64_t¶
Spinnaker::ChunkData::GetOffsetX Description: Returns the Offset X of the image included in the payload. Visibility:
- GetOffsetY(self) int64_t¶
Spinnaker::ChunkData::GetOffsetY Description: Returns the Offset Y of the image included in the payload. Visibility:
- GetPartSelector(self) int64_t¶
Spinnaker::ChunkData::GetPartSelector Description: Selects the part to access in chunk data in a multipart transmission. Visibility: Expert
- GetPixelDynamicRangeMax(self) int64_t¶
Spinnaker::ChunkData::GetPixelDynamicRangeMax Description: Returns the maximum value of dynamic range of the image included in the payload. Visibility: Expert
- GetPixelDynamicRangeMin(self) int64_t¶
Spinnaker::ChunkData::GetPixelDynamicRangeMin Description: Returns the minimum value of dynamic range of the image included in the payload. Visibility: Expert
- GetScan3dAxisMax(self) float64_t¶
Spinnaker::ChunkData::GetScan3dAxisMax Description: Returns the Maximum Axis value for the selected coordinate axis of the image included in the payload. Visibility: Expert
- GetScan3dAxisMin(self) float64_t¶
Spinnaker::ChunkData::GetScan3dAxisMin Description: Returns the Minimum Axis value for the selected coordinate axis of the image included in the payload. Visibility: Expert
- GetScan3dBaseline(self) float64_t¶
Spinnaker::ChunkData::GetScan3dBaseline Description: Returns the baseline as the physical distance of two cameras in a stereo camera setup. The value of this feature can be used for 3D reconstruction from disparity images. In this case, the unit of the 3D coordinates corresponds to the unit of the baseline. Visibility: Expert
- GetScan3dCoordinateOffset(self) float64_t¶
Spinnaker::ChunkData::GetScan3dCoordinateOffset Description: Returns the Offset for the selected coordinate axis of the image included in the payload. Visibility: Expert
- GetScan3dCoordinateReferenceValue(self) float64_t¶
Spinnaker::ChunkData::GetScan3dCoordinateReferenceValue Description: Reads the value of a position or pose coordinate for the anchor or transformed coordinate systems relative to the reference point. Visibility: Expert
- GetScan3dCoordinateScale(self) float64_t¶
Spinnaker::ChunkData::GetScan3dCoordinateScale Description: Returns the Scale for the selected coordinate axis of the image included in the payload. Visibility: Expert
- GetScan3dFocalLength(self) float64_t¶
Spinnaker::ChunkData::GetScan3dFocalLength Description: Returns the focal length of the camera in pixel. The focal length depends on the selected region. The value of this feature takes into account horizontal binning, decimation, or any other function changing the image resolution. Visibility: Expert
- GetScan3dInvalidDataFlag(self) bool¶
Spinnaker::ChunkData::GetScan3dInvalidDataFlag Description: Returns if a specific non-valid data flag is used in the data stream. Visibility: Expert
- GetScan3dInvalidDataValue(self) float64_t¶
Spinnaker::ChunkData::GetScan3dInvalidDataValue Description: Returns the Invalid Data Value used for the image included in the payload. Visibility: Expert
- GetScan3dPrincipalPointU(self) float64_t¶
Spinnaker::ChunkData::GetScan3dPrincipalPointU Description: Returns the value of this feature gives the horizontal position of the principal point, relative to the region origin, i.e. OffsetX. The value of this feature takes into account horizontal binning, decimation, or any other function changing the image resolution. Visibility: Expert
- GetScan3dPrincipalPointV(self) float64_t¶
Spinnaker::ChunkData::GetScan3dPrincipalPointV Description: Returns the value of this feature gives the vertical position of the principal point, relative to the region origin, i.e. OffsetY. The value of this feature takes into account vertical binning, decimation, or any other function changing the image resolution. Visibility: Expert
- GetScan3dTransformValue(self) float64_t¶
Spinnaker::ChunkData::GetScan3dTransformValue Description: Returns the transform value. Visibility: Expert
- GetScanLineSelector(self) int64_t¶
Spinnaker::ChunkData::GetScanLineSelector Description: Index for vector representation of one chunk value per line in an image. Visibility: Expert
- GetSequencerSetActive(self) int64_t¶
Spinnaker::ChunkData::GetSequencerSetActive Description: Returns the index of the active set of the running sequencer included in the payload. Visibility:
- GetSerialData(self) uint8_t *¶
Spinnaker::ChunkData::GetSerialData Description: Returns the serial data that was received. Visibility:
- GetSerialDataLength(self) int64_t¶
Spinnaker::ChunkData::GetSerialDataLength Description: Returns the length of the received serial data that was included in the payload. Visibility:
- GetSerialReceiveOverflow(self) bool¶
Spinnaker::ChunkData::GetSerialReceiveOverflow Description: Returns the status of the chunk serial receive overflow. Visibility:
- GetSmallPenalty(self) int64_t¶
Spinnaker::ChunkData::GetSmallPenalty Description: Returns the penalty when the change of Disparity Change is plus or minus 1. Visibility: Expert
- GetStereoHeight(self) int64_t¶
Spinnaker::ChunkData::GetStereoHeight Description: Returns the height of the image after stereo processing by the device (in pixels). Visibility: Expert
- GetStereoWidth(self) int64_t¶
Spinnaker::ChunkData::GetStereoWidth Description: Returns the width of the image after stereo processing by the device (in pixels). Visibility: Expert
- GetStreamChannelID(self) int64_t¶
Spinnaker::ChunkData::GetStreamChannelID Description: Returns identifier of the stream channel used to carry the block. Visibility: Expert
- GetTimerValue(self) float64_t¶
Spinnaker::ChunkData::GetTimerValue Description: Returns the value of the selected Timer at the time of the FrameStart internal event. Visibility: Expert
- GetTimestamp(self) int64_t¶
Spinnaker::ChunkData::GetTimestamp Description: Returns the Timestamp of the image. Visibility:
- GetTimestampLatchValue(self) int64_t¶
Spinnaker::ChunkData::GetTimestampLatchValue Description: Returns the last Timestamp latched with the TimestampLatch command. Visibility: Expert
- GetTransferBlockID(self) int64_t¶
Spinnaker::ChunkData::GetTransferBlockID Description: Returns the unique identifier of the transfer block used to transport the payload. Visibility: Expert
- GetTransferQueueCurrentBlockCount(self) int64_t¶
Spinnaker::ChunkData::GetTransferQueueCurrentBlockCount Description: Returns the current number of blocks in the transfer queue. Visibility: Expert
- GetUniquenessRatio(self) int64_t¶
Spinnaker::ChunkData::GetUniquenessRatio Description: Returns the difference between the best matching disparity and the second-best matching disparity. Visibility: Expert
- GetWidth(self) int64_t¶
Spinnaker::ChunkData::GetWidth Description: Returns the width of the image included in the payload. Visibility: