PySpin.ValueNode¶
- class ValueNode(*args, **kwargs)¶
Interface for value properties.
- FromString(self, ValueStr, Verify=True)¶
Parameters¶
ValueStr: Spinnaker::GenICam::gcstring const & Verify: bool
Spinnaker::GenApi::ValueNode::FromString Set content of the node as string
- param ValueStr:
The value to set
- param Verify:
Enables AccessMode and Range verification (default = true)
- IsValueCacheValid(self) bool¶
Spinnaker::GenApi::ValueNode::IsValueCacheValid Checks if the value comes from cache or is requested from another node
- IsValueUpdated(self) bool¶
Spinnaker::GenApi::ValueNode::IsValueUpdated Checks if the value has changed since the last GetValue(). Returns true if GetValue() is unavailable.
true if the node value has changed, false otherwise.
- SetReference(self, pBase)¶
Parameters¶
pBase: Spinnaker::GenApi::INode *
Spinnaker::GenApi::ValueNode::SetReference overload SetReference for Value
- ToString(self, Verify=False, IgnoreCache=False) gcstring¶
Parameters¶
Verify: bool IgnoreCache: bool
Spinnaker::GenApi::ValueNode::ToString Get content of the node as string
- param Verify:
Enables Range verification (default = false). The AccessMode is always checked
- param IgnoreCache:
If true the value is read ignoring any caches (default = false)
The value read