PySpin.RegisterNode¶
- class RegisterNode(*args, **kwargs)¶
Interface for string properties.
- Get(self, pBuffer, Length, Verify=False, IgnoreCache=False)¶
Parameters¶
pBuffer: uint8_t * Length: int64_t Verify: bool IgnoreCache: bool
Spinnaker::GenApi::RegisterNode::Get Fills a buffer with the register’s contents
- param pBuffer:
The buffer receiving the data to read
- param Length:
The number of bytes to retrieve
- param Verify:
Enables Range verification (default = false). The AccessMode is always checked
- param IgnoreCache:
If true the value is read ignoring any caches (default = false)
The value read
- GetAddress(self) int64_t¶
Spinnaker::GenApi::RegisterNode::GetAddress Retrieves the Address of the register
- GetLength(self) int64_t¶
Spinnaker::GenApi::RegisterNode::GetLength Retrieves the Length of the register [Bytes]
- Set(self, pBuffer, Verify=True)¶
Parameters¶
pBuffer: uint8_t const * Verify: bool
Spinnaker::GenApi::RegisterNode::Set Set the register’s contents
- param pBuffer:
The buffer containing the data to set
- param Length:
The number of bytes in pBuffer
- param Verify:
Enables AccessMode and Range verification (default = true)