PySpin.SystemEventHandler

class SystemEventHandler

A handler to interface arrival and removal events on the system. Note that only GEV interface arrivals and removals are currently handled.

OnInterfaceArrival(self, pInterface)

Parameters

pInterface: Spinnaker::InterfacePtr

Spinnaker::SystemEventHandler::OnInterfaceArrival

Interface arrival event callback. Note that only GEV interface arrivals are

currently handled.

param pInterface:

Reference tracked pointer to Interface object of the adapter attached to the system

OnInterfaceRemoval(self, pInterface)

Parameters

pInterface: Spinnaker::InterfacePtr

Spinnaker::SystemEventHandler::OnInterfaceRemoval

Interface removal event callback. Note that only GEV interface removals are

currently handled.

param pInterface:

Reference tracked pointer to Interface object of the adapter removed from the system