PySpin.ImageProcessor¶
- class ImageProcessor(*args)¶
Image post processing class for converting a source image to another pixel format.
All supported input image pixel formats can be converted to supported output image pixel formats. If the input pixel format is a compressed format, the decompression will occur before converting to the output pixel format.
List of supported input image pixel formats:
PixelFormat_Mono8
PixelFormat_Mono16
PixelFormat_BayerGR8
PixelFormat_BayerRG8
PixelFormat_BayerGB8
PixelFormat_BayerBG8
PixelFormat_BayerGR16
PixelFormat_BayerRG16
PixelFormat_BayerGB16
PixelFormat_BayerBG16
PixelFormat_Mono12Packed
PixelFormat_BayerGR12Packed
PixelFormat_BayerRG12Packed
PixelFormat_BayerGB12Packed
PixelFormat_BayerBG12Packed
PixelFormat_YUV411Packed
PixelFormat_YUV422Packed
PixelFormat_YUV444Packed
PixelFormat_Mono12p
PixelFormat_BayerGR12p
PixelFormat_BayerRG12p
PixelFormat_BayerGB12p
PixelFormat_BayerBG12p
PixelFormat_YCbCr8
PixelFormat_YCbCr422_8
PixelFormat_YCbCr411_8
PixelFormat_BGR8
PixelFormat_BGRa8
PixelFormat_Mono10Packed
PixelFormat_BayerGR10Packed
PixelFormat_BayerRG10Packed
PixelFormat_BayerGB10Packed
PixelFormat_BayerBG10Packed
PixelFormat_Mono10p
PixelFormat_BayerGR10p
PixelFormat_BayerRG10p
PixelFormat_BayerGB10p
PixelFormat_BayerBG10p
PixelFormat_Mono10
PixelFormat_Mono12
PixelFormat_Mono14
PixelFormat_BayerBG10
PixelFormat_BayerBG12
PixelFormat_BayerGB10
PixelFormat_BayerGB12
PixelFormat_BayerGR10
PixelFormat_BayerGR12
PixelFormat_BayerRG10
PixelFormat_BayerRG12
PixelFormat_RGBa8
PixelFormat_RGB8
PixelFormat_RGB12
PixelFormat_BGR16
PixelFormat_R12
PixelFormat_G12
PixelFormat_B12
PixelFormat_YUV8_UYV
PixelFormat_YUV411_8_UYYVYY
PixelFormat_YUV422_8
PixelFormat_Polarized8
PixelFormat_Polarized10p
PixelFormat_Polarized12p
PixelFormat_Polarized16
PixelFormat_BayerRGPolarized8
PixelFormat_BayerRGPolarized10p
PixelFormat_BayerRGPolarized12p
PixelFormat_BayerRGPolarized16
PixelFormat_LLCMono8
PixelFormat_LLCBayerRG8
PixelFormat_JPEGMono8
PixelFormat_JPEGColor8
PixelFormat_Raw16
PixelFormat_Raw8
PixelFormat_R12_Jpeg
PixelFormat_GR12_Jpeg
PixelFormat_GB12_Jpeg
PixelFormat_B12_Jpeg
List of supported output image pixel formats
PixelFormat_Mono8
PixelFormat_Mono16
PixelFormat_BayerBG8
PixelFormat_BayerGB8
PixelFormat_BayerRG8
PixelFormat_BayerGR8
PixelFormat_BayerBG16
PixelFormat_BayerGB16
PixelFormat_BayerRG16
PixelFormat_BayerGR16
PixelFormat_BGR8
PixelFormat_BGRa8
PixelFormat_RGB8
PixelFormat_RGBa8
PixelFormat_BGR16
PixelFormat_RGB16
PixelFormat_R12
PixelFormat_G12
PixelFormat_B12
- ApplyGamma(self, srcImage, gamma, applyGammaInverse=False) ImagePtr¶
Parameters¶
srcImage: Spinnaker::ImagePtr const & gamma: float applyGammaInverse: bool
ApplyGamma(self, srcImage, destImage, gamma, applyGammaInverse=False)
Parameters¶
srcImage: Spinnaker::ImagePtr const & destImage: Spinnaker::ImagePtr & gamma: float applyGammaInverse: bool
Spinnaker::ImageProcessor::ApplyGamma Applies gamma correction to the source image and stores the result in the destination image.
Note that the destination image buffer cannot point to the same memory location as the source image buffer. This ensures that the image processing operation does not result in undefined behavior or data corruption due to overlapping memory regions.
- param srcImage:
The source image from which to apply gamma on.
- param destImage:
The destination image in which the gamma applied image data will be stored.
- param gamma:
Gamma value to apply. A value between 0.5 and 4 is acceptable. (Default assuming image-to-screen)
- param applyGammaInverse:
Converts a gamma corrected source image back to the original image using the inverse of the gamma value (used for applying screen-to-image gamma)
- Convert(self, srcImage, destFormat) ImagePtr¶
Parameters¶
srcImage: Spinnaker::ImagePtr const & destFormat: enum Spinnaker::PixelFormatEnums
Convert(self, srcImage, destImage, destFormat)
Parameters¶
srcImage: Spinnaker::ImagePtr const & destImage: Spinnaker::ImagePtr & destFormat: enum Spinnaker::PixelFormatEnums
Convert(self, srcImageList, destFormat) -> ImagePtr
Parameters¶
srcImageList: Spinnaker::ImageList const & destFormat: enum Spinnaker::PixelFormatEnums
Convert(self, srcImageList, destImage, destFormat)
Parameters¶
srcImageList: Spinnaker::ImageList const & destImage: Spinnaker::ImagePtr & destFormat: enum Spinnaker::PixelFormatEnums
Spinnaker::ImageProcessor::Convert Converts the source list of image buffers to the specified output pixel format and stores the result in the destination image. The conversion could encompasses decompression, interleaving and conversion of image data depending on the source pixel format of images in the source image list. The destination image needs to be configured to have the correct buffer size before calling this function. See ResetImage() to setup the correct buffer size according to specified pixel format.
Note that compressed images are decompressed before any further color processing, interleaving or conversion is performed. Decompression is multi-threaded and defaults to utilizing one less than the number of concurrent threads supported by the system. The default number of decompression threads can be set with SetNumDecompressionThreads().
Note not all the supported image pixel formats described in the class description are supported in this function.
List of supported image pixel formats for the source image list:
PixelFormat_R12
PixelFormat_GR12
PixelFormat_GB12
PixelFormat_B12
PixelFormat_R12_Jpeg
PixelFormat_GR12_Jpeg
PixelFormat_GB12_Jpeg
PixelFormat_B12_Jpeg
See: PixelFormatEnums
See: ResetImage
See: SetNumDecompressionThreads
Args: srcImageList: List of images from which to convert the images from. destImage: The destination image in which the converted image data will be stored. destFormat: Output format of the converted image.
- GetColorProcessing(self) Spinnaker::ColorProcessingAlgorithm¶
Spinnaker::ImageProcessor::GetColorProcessing Gets the default color processing algorithm.
See: SetColorProcessing()
The default color processing algorithm.
- GetNumDecompressionThreads(self) unsigned int¶
Spinnaker::ImageProcessor::GetNumDecompressionThreads Gets the number of threads used for image decompression during Convert().
See: SetNumDecompressionThreads()
Number of parallel image decompression threads set to run.
- SetColorProcessing(self, colorAlgorithm)¶
Parameters¶
colorAlgorithm: enum Spinnaker::ColorProcessingAlgorithm
Spinnaker::ImageProcessor::SetColorProcessing Sets the color processing algorithm used at the time of the Convert() call, therefore the most recent execution of this function will take precedence. The DEFAULT algorithm is deprecated and should not be used in the ImageProcessor class.
- param colorAlgorithm:
The color processing algorithm to set.
- See:
GetColorProcessing()
- SetNumDecompressionThreads(self, numThreads)¶
Parameters¶
numThreads: unsigned int
Spinnaker::ImageProcessor::SetNumDecompressionThreads Sets the default number of threads used for image decompression during Convert(). The number of threads used is defaulted to be equal to one less than the number of concurrent threads supported by the system.
- param numThreads:
Number of parallel image decompression threads set to run
- See:
Convert()