| 
                                             FLIR 
                                            Blackfly®S BFS-U3-200S6  | 
                                    
Transport Layer Control
The Transport Layer control provides the following information:
Payload Size - the number of bytes transferred for each image (including chunk data).
USB3 Vision Tab - Message Channel - Channel ID used for the Message Channel.
U3v Version Major/Minor - USB3 Vision standard version.
U3V Capabilities - what the camera supports (SIRM, EIRM and IIDC2).
Max Command Transfer Length - the maximum supported commands that can be sent to the camera.
Max Ack Transfer Length - the maximum supported ack that can be sent to the camera.
Number of Stream Channels - the number of stream channels the camera supports.
Current Speed - the speed of the camera's interface (Super Speed, High Speed).
Link Error Count - the number of errors on the usb link.
Link Recovery Count - the number of times the USB link has recovered.
Summary Table
| Name | Interface | Access | Visibility | Description | 
|---|---|---|---|---|
| Payload Size | IInteger | Expert | Provides the number of bytes transferred for each image or chunk on the stream channel. | |
| USB3 Vision | ICategory | RO | Beginner | Category that contains the features pertaining to the USB3 Vision transport layer of the device. | 
| Link Error Count | IInteger | RO | Expert | Counts the number of error on the link. | 
| Link Recovery Count | IInteger | RO | Expert | Counts the number of times the USB link has recovered. | 
Transport Layer Control Features
Payload Size
Provides the number of bytes transferred for each image or chunk on the stream channel.
| Property | Value | 
|---|---|
| Name | PayloadSize | 
| Interface | IInteger | 
| Access | |
| Unit | |
| Visibility | Expert | 
USB3 Vision
Category that contains the features pertaining to the USB3 Vision transport layer of the device.
| Property | Value | 
|---|---|
| Name | USB3Vision | 
| Interface | ICategory | 
| Access | RO | 
| Visibility | Beginner | 
Link Error Count
Counts the number of error on the link.
| Property | Value | 
|---|---|
| Name | LinkErrorCount | 
| Interface | IInteger | 
| Access | RO | 
| Unit | |
| Visibility | Expert | 
Link Recovery Count
Counts the number of times the USB link has recovered.
| Property | Value | 
|---|---|
| Name | LinkRecoveryCount | 
| Interface | IInteger | 
| Access | RO | 
| Unit | |
| Visibility | Expert | 
| 8/31/2017
                                             © 2015-2017 FLIR® Integrated Imaging Solutions Inc. All rights reserved. Legal | Contact Support | Cookie Policy  | 
                                        
                                             Blackfly®S BFS-U3-200S6   | 
                                        
                                             
                                                  |