| 
                                             You are here: Installation Guide > Camera Installation > Installing Your Interface Card and Software
                                             
                                         | 
                                        
                                             FLIR 
                                            Blackfly®S BFS-GE-16S2-BD2  | 
                                    
Installing Your Interface Card and Software
1. Install your Interface Card
                                             
                                         | 
                                        
                                             Ensure the card is installed per the manufacturer's instructions. Connect the internal IDE or SATA power connector on the card to the computer power supply. Alternatively, use your PC's built-in host controller, if equipped.  | 
                                    
Open the Windows Device Manager. Ensure the card is properly installed. 
2. Install the Spinnaker® Software
- Login to the Downloads page.
 - Select your Product Family, Camera Model and Operating System from the drop-down lists.
 - Click on the Software search results to expand the list.
 - Click the appropriate link to begin the download and installation.
 
After the download is complete, the Spinnaker setup wizard begins. If the wizard does not start automatically, double-click the .exe file to open it. Follow the steps in each setup dialog.
3. Enable jumbo frames
- In Start->All Programs-> Point Grey Spinnaker SDK->SpinView, right click on the Network Adapter and select Adapter Configuration, then select IP Configuration.
 - Click Open Network Connections.
 - Click Change Settings.
 - Click on the Advanced tab and from the Settings list select Jumbo Packet.
 - Set the Value to 9014 Bytes and click OK.
 
| 8/13/2018
                                             © 2015-2018 FLIR® Integrated Imaging Solutions Inc. All rights reserved. Legal | Contact Support | Cookie Policy  | 
                                        
                                             Blackfly®S BFS-GE-16S2-BD2   |