You are here: Technical Reference > Flat Field Correction Control - BFS-GE-16S2-BD Version 1808.1.1.0
FLIR

Blackfly®S

BFS-GE-16S2-BD2

 

Flat Field Correction Control

Flat Field Correction (FFC) is used to suppress an image sensor Fixed Pattern Noise (FPN) which is a common image artifact for many CMOS sensors. FFC includes correction for both Dark Signal Non-Uniformity (DSNU) and Pixel Response Non-Uniformity (PRNU). The suppression for DSNU is achieved by black level correction and the suppression for PRNU is achieved by gain correction. A reference equation is given below:

Pn = ΔGn ⨯ ( Un + ΔOn )

Where:

  • n could be pixel, row or column index.
  • P is the corrected pixel value.
  • U is the uncorrected pixel value.
  • ΔG is the delta gain (gain correction), which is row/column/pixel dependent.
  • ΔO is the delta offset (black level correction), which is row/column/pixel dependent.

Note that our FFC is currently column dependent only since the column FPN is the dominant noise for all sensors we support.

Flat Field Correction Control

FFC can be enabled or disabled using Flat Field Correction Enable. It is enabled by default.

Use Flat Field Correction Mode to select a mode. There are three FFC modes: Factory, User, and Calibration.

Factory mode

This is the default mode. In this mode, the camera uses the factory delta gain/offset parameters calibrated by FLIR.

The FFC coefficients change with different camera gain levels.

User mode

In this mode, the camera uses fixed FFC coefficients across all camera gain levels. The default values for this mode apply no FFC and are the equivalent of disabling FFC. To modify the values, you must switch to Calibration mode.

Calibration mode

In this mode, the Flat Field User Table Control access (R/W) is available. At the same time, FFC will be automatically disabled and become unavailable. Therefore, values entered for delta gain/offset do not take effect until the mode is switched to User and FFC is enabled again.

Flat Field User Table Control

When in Calibration mode, you can access these controls.

Table x Coordinate specifies the horizontal coordinate of the FFC gain/offset. The FFC implementation supports only the x coordinate, for suppressing the column FPN.

Flat Field Gain specifies the delta gain for each table x coordinate.

Flat Field Offset (16-bit) specifies the delta offset for each table x coordinate. The step size should be queried before writing the value as it is normally much greater than 1 (e.g., 32). Entering a value that is not divisible by the step size results in an error.

User Table Reset sets all FFC parameters back to the last saved values loaded from the camera. If nothing has been previously saved, this resets to the default values which is the equivalent of disabling FFC.

User Table Save saves the FFC parameters into non-volatile memory which is preserved even when the camera is power cycled. This overwrites the existing saved user table.

Summary Table

Name Interface Access Visibility Description
Flat Field Correction Enable IBoolean Beginner Enable or disable flat field correction.
Flat Field Correction Mode IEnumeration Expert Selects flat field correction mode. Note that flat field correction parameters are accessible only in Calibration mode. When switching modes from Calibration to User or Factory, it is recommended to stop image streaming to give the camera enough time to load the corresponding table.
Flat Field User Table Control ICategory Expert Category that contains User flat field correction table control features.

Flat Field Correction Control Features


Flat Field Correction Enable

Enable or disable flat field correction.

Property Value
Name FfcEnable
Interface IBoolean
Access
Visibility Beginner

Flat Field Correction Mode

Selects flat field correction mode. Note that flat field correction parameters are accessible only in Calibration mode. When switching modes from Calibration to User or Factory, it is recommended to stop image streaming to give the camera enough time to load the corresponding table.

Property Value
Name FfcMode
Interface IEnumeration
Access
Visibility Expert

Enumeration Values
Factory
User
Calibration

Flat Field User Table Control

Category that contains User flat field correction table control features.

Property Value
Name FfcUserTableControl
Interface ICategory
Access
Visibility Expert

 

8/13/2018
© 2015-2018 FLIR® Integrated Imaging Solutions Inc.
All rights reserved.
Legal
| Contact Support

Blackfly®S BFS-GE-16S2-BD2
Camera Reference

FLIR Camera and API References