You are here: Technical Reference > Flat Field Correction Control > Flat Field User Table Control
FLIR

Blackfly®S

BFS-GE-16S2-BD2

 

Flat Field User Table Control

Category that contains User flat field correction table control features.

Summary Table

Name Interface Access Visibility Description
Table X Coordinate IInteger Expert Controls the pixel X coordinate of the user flat field correction coefficients.
Flat Field Gain [Table X Coordinate] IFloat Expert The value of user flat field gain correction for the current pixel.
Flat Field Offset (16-bit) [Table X Coordinate] IInteger Expert The value of user flat field offset correction for the current pixel.
User Table Reset ICommand WO Expert Resets the user flat field correction table to the last saved values loaded from the camera. If nothing has been previously saved, this resets to the default values which is the equivalent of disabling FFC.
User Table Save ICommand WO Expert Saves the current User flat field correction table into the camera, which means the table is still available after a power cycle. Note that this overwrites the existing saved User table.

Flat Field User Table Control Features


Table X Coordinate

Controls the pixel X coordinate of the user flat field correction coefficients.

Property Value
Name FfcUserTableXCoordinate
Interface IInteger
Access
Unit
Visibility Expert
Value 0

Flat Field Gain

The value of user flat field gain correction for the current pixel.

Property Value
Name FfcUserGain [Table X Coordinate]
Interface IFloat
Access
Unit
Visibility Expert

Flat Field Offset (16-bit)

The value of user flat field offset correction for the current pixel.

Property Value
Name FfcUserOffset [Table X Coordinate]
Interface IInteger
Access
Unit
Visibility Expert

User Table Reset

Resets the user flat field correction table to the last saved values loaded from the camera. If nothing has been previously saved, this resets to the default values which is the equivalent of disabling FFC.

Property Value
Name FfcUserTableReset
Interface ICommand
Access WO
Visibility Expert

User Table Save

Saves the current User flat field correction table into the camera, which means the table is still available after a power cycle. Note that this overwrites the existing saved User table.

Property Value
Name FfcUserTableSave
Interface ICommand
Access WO
Visibility Expert

 

8/13/2018
© 2015-2018 FLIR® Integrated Imaging Solutions Inc.
All rights reserved.
Legal
| Contact Support | Cookie Policy

Blackfly®S BFS-GE-16S2-BD2
Camera Reference

FLIR Camera and API References